OnPathDimWithValueBuilder Class¶
-
class
NXOpen.GeometricUtilities.
OnPathDimWithValueBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.INXObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.GeometricUtilities.OnPathDimWithValueBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Location | Returns the location on path |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Value | Returns the value expression |
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
InheritLocation | Inherits location data of a NXOpen.GeometricUtilities.OnPathDimWithValueBuilder object |
InheritValue | Inherits value of a NXOpen.GeometricUtilities.OnPathDimWithValueBuilder object |
Prints a representation of this object to the system log file. | |
SetName | Sets the custom name of the object. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
IsOccurrence¶
-
OnPathDimWithValueBuilder.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
OnPathDimWithValueBuilder.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Location¶
-
OnPathDimWithValueBuilder.
Location
¶ Returns the location on path
-------------------------------------
Getter Method
Signature
Location()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX5.0.0.
License requirements: None.
Name¶
-
OnPathDimWithValueBuilder.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
OnPathDimWithValueBuilder.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
OnPathDimWithValueBuilder.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
OnPathDimWithValueBuilder.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Value¶
-
OnPathDimWithValueBuilder.
Value
¶ Returns the value expression
-------------------------------------
Getter Method
Signature
Value()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
Method Detail¶
FindObject¶
-
OnPathDimWithValueBuilder.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
InheritLocation¶
-
OnPathDimWithValueBuilder.
InheritLocation
¶ Inherits location data of a
NXOpen.GeometricUtilities.OnPathDimWithValueBuilder
objectSignature
InheritLocation(sourceBuilder)
Parameters: sourceBuilder ( NXOpen.GeometricUtilities.OnPathDimWithValueBuilder
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
InheritValue¶
-
OnPathDimWithValueBuilder.
InheritValue
¶ Inherits value of a
NXOpen.GeometricUtilities.OnPathDimWithValueBuilder
objectSignature
InheritValue(sourceBuilder)
Parameters: sourceBuilder ( NXOpen.GeometricUtilities.OnPathDimWithValueBuilder
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR free_form_modeling (“FREE-FORM MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
Print¶
-
OnPathDimWithValueBuilder.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
OnPathDimWithValueBuilder.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
Validate¶
-
OnPathDimWithValueBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.