EnumTestCurves Enumeration

NXOpen.GeometricUtilities.EnumTest.Curves is an alias for NXOpen.GeometricUtilities.EnumTestCurves

class NXOpen.GeometricUtilities.EnumTestCurves

Bases: object

Curves are important

Enum Members

Enum Member Enum Member Description
Line
the granddaddy of all curves
Arc
arcs are always jealous of lines’ notoriety
Circle
where do they start? The answer blows in the wind
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.