BlendStopshortBuilderChoices Enumeration

NXOpen.GeometricUtilities.BlendStopshortBuilder.Choices is an alias for NXOpen.GeometricUtilities.BlendStopshortBuilderChoices

class NXOpen.GeometricUtilities.BlendStopshortBuilderChoices

Bases: object

This enum represents the choice for stopshort option.

The default choice is ‘At Distance’.

Enum Members

Enum Member Enum Member Description
AtDistance
Distance
AtIntersection
Intersection
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.