OrientXpressBuilderReference Enumeration

NXOpen.GeometricUtilities.OrientXpressBuilder.Reference is an alias for NXOpen.GeometricUtilities.OrientXpressBuilderReference

class NXOpen.GeometricUtilities.OrientXpressBuilderReference

Bases: object

the option for reference csys

Enum Members

Enum Member Enum Member Description
AcsWorkPart
Reference CSYS is absolute coordinate system in the work part
AcsDisplayPart
Reference CSYS is absolute coordinate system in the display part
WcsWorkPart
Reference CSYS is work coordinate system in the work part
WcsDisplayPart
Reference CSYS is work coordinate system in the display part
Csys
Reference CSYS is user specified coordinate system
Fixed
Reference CSYS is user defined coordinate system
ProgramDefined
Reference CSYS is application defined
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.