FlowDirection Class

class NXOpen.GeometricUtilities.FlowDirection

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.GeometricUtilities.FlowDirection Allows user to specify different flow direction to control output surface shape.

New in version NX5.0.0.

Properties

Property Description
FlowDirectionType Returns or sets the flow direction type.
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

FlowDirectionType Enumeration flow direction type.

Property Detail

FlowDirectionType

FlowDirection.FlowDirectionType

Returns or sets the flow direction type.

-------------------------------------

Getter Method

Signature FlowDirectionType()

Returns:
Return type:NXOpen.GeometricUtilities.FlowDirectionType

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature FlowDirectionType(flowDirectionType)

Parameters:flowDirectionType (NXOpen.GeometricUtilities.FlowDirectionType) –

New in version NX5.0.0.

License requirements: nx_freeform_1 (“basic freeform modeling”)

Method Detail

Validate

FlowDirection.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.