SpineDefinitionBuilder Class

class NXOpen.GeometricUtilities.SpineDefinitionBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Provides a spine definition for modeling operations

New in version NX8.5.0.

Properties

Property Description
Method Returns or sets the method
Section Returns the section
Tag Returns the Tag for this object.
Vector Returns or sets the vector

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

SpineDefinitionBuilderMethodOptions Enumeration Options to define a spine

Property Detail

Method

SpineDefinitionBuilder.Method

Returns or sets the method

-------------------------------------

Getter Method

Signature Method()

Returns:
Return type:NXOpen.GeometricUtilities.SpineDefinitionBuilderMethodOptions

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Method(method)

Parameters:method (NXOpen.GeometricUtilities.SpineDefinitionBuilderMethodOptions) –

New in version NX8.5.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

Section

SpineDefinitionBuilder.Section

Returns the section

-------------------------------------

Getter Method

Signature Section()

Returns:
Return type:NXOpen.Section

New in version NX8.5.0.

License requirements: None.

Vector

SpineDefinitionBuilder.Vector

Returns or sets the vector

-------------------------------------

Getter Method

Signature Vector()

Returns:
Return type:NXOpen.Direction

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Vector(vector)

Parameters:vector (NXOpen.Direction) –

New in version NX8.5.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

Method Detail

Validate

SpineDefinitionBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.