EndHoleDataThreadRotationOptions Enumeration

NXOpen.GeometricUtilities.EndHoleData.ThreadRotationOptions is an alias for NXOpen.GeometricUtilities.EndHoleDataThreadRotationOptions

class NXOpen.GeometricUtilities.EndHoleDataThreadRotationOptions

Bases: object

Represents thread rotation options.

Enum Members

Enum Member Enum Member Description
Right
Right rotation
Left
Left rotation
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.