ReduceSurfaceRadiusBuilderReduceValueTypeSpecification Enumeration

NXOpen.GeometricUtilities.ReduceSurfaceRadiusBuilder.ReduceValueTypeSpecification is an alias for NXOpen.GeometricUtilities.ReduceSurfaceRadiusBuilderReduceValueTypeSpecification

class NXOpen.GeometricUtilities.ReduceSurfaceRadiusBuilderReduceValueTypeSpecification

Bases: object

Specify the reduction method.

There are three types: percentage reduction, reduction value and target value.

Enum Members

Enum Member Enum Member Description
Percentage
Value
Delta
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.