OrientXpressTestBuilder Class

class NXOpen.GeometricUtilities.OrientXpressTestBuilder

Bases: NXOpen.Builder

Represents a ModlUtilsJA.OrientXpressTest builder

OrientXpressTest is not supported in KF.

New in version NX6.0.0.

Properties

Property Description
ActiveAxis Returns or sets the active axis
ActivePlane Returns or sets the active plane
DisplayAxisBlock Returns or sets the display axis block
DisplayPlaneBlock Returns or sets the display plane block
DisplayReferenceBlock Returns or sets the display reference block
DisplayXaxis Returns or sets the display x-axis
DisplayXyplane Returns or sets the display xy-plane
DisplayXzplane Returns or sets the display xz-plane
DisplayYaxis Returns or sets the display y-axis
DisplayYzplane Returns or sets the display yz-plane
DisplayZaxis Returns or sets the display z-axis
SelectFixedCsys Returns the select fixed csys
SelectProgramCsys Returns the select program defined csys
Tag Returns the Tag for this object.
Type Returns or sets the test type

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

OrientXpressTestBuilderAxis Enumeration the active axis options
OrientXpressTestBuilderAxisBlock Enumeration the options to show or hide the axis block
OrientXpressTestBuilderPlane Enumeration the active plane options
OrientXpressTestBuilderPlaneBlock Enumeration the options to show or hide the plane block
OrientXpressTestBuilderReferenceBlock Enumeration the options to show or hide the reference block
OrientXpressTestBuilderTypes Enumeration the test types

Property Detail

ActiveAxis

OrientXpressTestBuilder.ActiveAxis

Returns or sets the active axis

-------------------------------------

Getter Method

Signature ActiveAxis()

Returns:
Return type:NXOpen.GeometricUtilities.OrientXpressTestBuilderAxis

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ActiveAxis(activeAxis)

Parameters:activeAxis (NXOpen.GeometricUtilities.OrientXpressTestBuilderAxis) –

New in version NX6.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

ActivePlane

OrientXpressTestBuilder.ActivePlane

Returns or sets the active plane

-------------------------------------

Getter Method

Signature ActivePlane()

Returns:
Return type:NXOpen.GeometricUtilities.OrientXpressTestBuilderPlane

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ActivePlane(activePlane)

Parameters:activePlane (NXOpen.GeometricUtilities.OrientXpressTestBuilderPlane) –

New in version NX6.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

DisplayAxisBlock

OrientXpressTestBuilder.DisplayAxisBlock

Returns or sets the display axis block

-------------------------------------

Getter Method

Signature DisplayAxisBlock()

Returns:
Return type:NXOpen.GeometricUtilities.OrientXpressTestBuilderAxisBlock

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DisplayAxisBlock(displayAxisBlock)

Parameters:displayAxisBlock (NXOpen.GeometricUtilities.OrientXpressTestBuilderAxisBlock) –

New in version NX6.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

DisplayPlaneBlock

OrientXpressTestBuilder.DisplayPlaneBlock

Returns or sets the display plane block

-------------------------------------

Getter Method

Signature DisplayPlaneBlock()

Returns:
Return type:NXOpen.GeometricUtilities.OrientXpressTestBuilderPlaneBlock

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DisplayPlaneBlock(displayPlaneBlock)

Parameters:displayPlaneBlock (NXOpen.GeometricUtilities.OrientXpressTestBuilderPlaneBlock) –

New in version NX6.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

DisplayReferenceBlock

OrientXpressTestBuilder.DisplayReferenceBlock

Returns or sets the display reference block

-------------------------------------

Getter Method

Signature DisplayReferenceBlock()

Returns:
Return type:NXOpen.GeometricUtilities.OrientXpressTestBuilderReferenceBlock

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DisplayReferenceBlock(displayReferenceBlock)

Parameters:displayReferenceBlock (NXOpen.GeometricUtilities.OrientXpressTestBuilderReferenceBlock) –

New in version NX6.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

DisplayXaxis

OrientXpressTestBuilder.DisplayXaxis

Returns or sets the display x-axis

-------------------------------------

Getter Method

Signature DisplayXaxis()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DisplayXaxis(displayXaxis)

Parameters:displayXaxis (bool) –

New in version NX6.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

DisplayXyplane

OrientXpressTestBuilder.DisplayXyplane

Returns or sets the display xy-plane

-------------------------------------

Getter Method

Signature DisplayXyplane()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DisplayXyplane(displayXYplane)

Parameters:displayXYplane (bool) –

New in version NX6.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

DisplayXzplane

OrientXpressTestBuilder.DisplayXzplane

Returns or sets the display xz-plane

-------------------------------------

Getter Method

Signature DisplayXzplane()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DisplayXzplane(displayXZplane)

Parameters:displayXZplane (bool) –

New in version NX6.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

DisplayYaxis

OrientXpressTestBuilder.DisplayYaxis

Returns or sets the display y-axis

-------------------------------------

Getter Method

Signature DisplayYaxis()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DisplayYaxis(displayYaxis)

Parameters:displayYaxis (bool) –

New in version NX6.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

DisplayYzplane

OrientXpressTestBuilder.DisplayYzplane

Returns or sets the display yz-plane

-------------------------------------

Getter Method

Signature DisplayYzplane()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DisplayYzplane(displayYZplane)

Parameters:displayYZplane (bool) –

New in version NX6.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

DisplayZaxis

OrientXpressTestBuilder.DisplayZaxis

Returns or sets the display z-axis

-------------------------------------

Getter Method

Signature DisplayZaxis()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DisplayZaxis(displayZaxis)

Parameters:displayZaxis (bool) –

New in version NX6.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

SelectFixedCsys

OrientXpressTestBuilder.SelectFixedCsys

Returns the select fixed csys

-------------------------------------

Getter Method

Signature SelectFixedCsys()

Returns:
Return type:NXOpen.SelectNXObject

New in version NX6.0.0.

License requirements: None.

SelectProgramCsys

OrientXpressTestBuilder.SelectProgramCsys

Returns the select program defined csys

-------------------------------------

Getter Method

Signature SelectProgramCsys()

Returns:
Return type:NXOpen.SelectNXObject

New in version NX6.0.0.

License requirements: None.

Type

OrientXpressTestBuilder.Type

Returns or sets the test type

-------------------------------------

Getter Method

Signature Type()

Returns:
Return type:NXOpen.GeometricUtilities.OrientXpressTestBuilderTypes

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Type(type)

Parameters:type (NXOpen.GeometricUtilities.OrientXpressTestBuilderTypes) –

New in version NX6.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

Method Detail

Validate

OrientXpressTestBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.