OrientXpressTestBuilderPlaneBlock Enumeration

NXOpen.GeometricUtilities.OrientXpressTestBuilder.PlaneBlock is an alias for NXOpen.GeometricUtilities.OrientXpressTestBuilderPlaneBlock

class NXOpen.GeometricUtilities.OrientXpressTestBuilderPlaneBlock

Bases: object

the options to show or hide the plane block

Enum Members

Enum Member Enum Member Description
Show
Test show plane block
Hide
Test hide plane block
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.