ModlMotionDelta Enumeration¶
NXOpen.GeometricUtilities.ModlMotion.Delta is an alias for NXOpen.GeometricUtilities.ModlMotionDelta
-
class
NXOpen.GeometricUtilities.
ModlMotionDelta
¶ Bases:
object
Represents the options of Delta XYZ.
Enum Members
Enum Member Enum Member Description ReferenceAcsWorkPart Reference CSYS is absolute coordinate system in the work partReferenceAcsDisplayPart Reference CSYS is absolute coordinate system in the display partReferenceWcsWorkPart Reference CSYS is work coordinate system in the work partReferenceWcsDisplayPart Reference CSYS is work coordinate system in the display part-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-