MovePoleBuilder Class

class NXOpen.GeometricUtilities.MovePoleBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

This class manages the control poles movements for a surface or curve.

New in version NX8.5.0.

Properties

Property Description
ControlPoleManager Returns the control pole manager
DegreesAndPatches Returns the degrees and patches
Entity Returns or sets the entity
MoveMethod Returns or sets the control pole move method
Plane Returns or sets the plane
Tag Returns the Tag for this object.
Vector Returns or sets the vector
WCSDirection Returns or sets the fixed direction

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

ControlPoleManager

MovePoleBuilder.ControlPoleManager

Returns the control pole manager

-------------------------------------

Getter Method

Signature ControlPoleManager()

Returns:
Return type:NXOpen.GeometricUtilities.ControlPoleManagerData

New in version NX8.5.0.

License requirements: None.

DegreesAndPatches

MovePoleBuilder.DegreesAndPatches

Returns the degrees and patches

-------------------------------------

Getter Method

Signature DegreesAndPatches()

Returns:
Return type:NXOpen.GeometricUtilities.DegreesAndSegmentsOrPatchesBuilder

New in version NX8.5.0.

License requirements: None.

Entity

MovePoleBuilder.Entity

Returns or sets the entity

-------------------------------------

Getter Method

Signature Entity()

Returns:
Return type:NXOpen.NXObject

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Entity(entity)

Parameters:entity (NXOpen.NXObject) –

New in version NX8.5.0.

License requirements: None.

MoveMethod

MovePoleBuilder.MoveMethod

Returns or sets the control pole move method

-------------------------------------

Getter Method

Signature MoveMethod()

Returns:
Return type:NXOpen.GeometricUtilities.MovePoleBuilderMoveMethodType

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature MoveMethod(moveMethod)

Parameters:moveMethod (NXOpen.GeometricUtilities.MovePoleBuilderMoveMethodType) –

New in version NX8.5.0.

License requirements: None.

Plane

MovePoleBuilder.Plane

Returns or sets the plane

-------------------------------------

Getter Method

Signature Plane()

Returns:
Return type:NXOpen.Plane

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Plane(plane)

Parameters:plane (NXOpen.Plane) –

New in version NX8.5.0.

License requirements: None.

Vector

MovePoleBuilder.Vector

Returns or sets the vector

-------------------------------------

Getter Method

Signature Vector()

Returns:
Return type:NXOpen.Direction

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Vector(vector)

Parameters:vector (NXOpen.Direction) –

New in version NX8.5.0.

License requirements: None.

WCSDirection

MovePoleBuilder.WCSDirection

Returns or sets the fixed direction

-------------------------------------

Getter Method

Signature WCSDirection()

Returns:
Return type:NXOpen.GeometricUtilities.MovePoleBuilderWCSDirectionType

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature WCSDirection(wcsDirection)

Parameters:wcsDirection (NXOpen.GeometricUtilities.MovePoleBuilderWCSDirectionType) –

New in version NX8.5.0.

License requirements: None.

Method Detail

Validate

MovePoleBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.