DegreesAndSegmentsOrPatchesBuilder Class¶
-
class
NXOpen.GeometricUtilities.
DegreesAndSegmentsOrPatchesBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.INXObject
,NXOpen.GeometricUtilities.IComponentBuilder
the DegreesAndSegmentsOrPatches builder
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Degree | Returns or sets the degree |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
SegmentsOrPatches | Returns or sets the patches |
Tag | Returns the Tag for this object. |
UDegree | Returns or sets the u degree |
UPatches | Returns or sets the u patches |
VDegree | Returns or sets the v degree |
VPatches | Returns or sets the v patches |
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
Prints a representation of this object to the system log file. | |
SetName | Sets the custom name of the object. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Degree¶
-
DegreesAndSegmentsOrPatchesBuilder.
Degree
¶ Returns or sets the degree
-------------------------------------
Getter Method
Signature
Degree()
Returns: Return type: int New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
Degree(degree)
Parameters: degree (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
IsOccurrence¶
-
DegreesAndSegmentsOrPatchesBuilder.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
DegreesAndSegmentsOrPatchesBuilder.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
DegreesAndSegmentsOrPatchesBuilder.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
DegreesAndSegmentsOrPatchesBuilder.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
DegreesAndSegmentsOrPatchesBuilder.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
DegreesAndSegmentsOrPatchesBuilder.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
SegmentsOrPatches¶
-
DegreesAndSegmentsOrPatchesBuilder.
SegmentsOrPatches
¶ Returns or sets the patches
-------------------------------------
Getter Method
Signature
SegmentsOrPatches()
Returns: Return type: int New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
SegmentsOrPatches(segmentsOrPatches)
Parameters: segmentsOrPatches (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
UDegree¶
-
DegreesAndSegmentsOrPatchesBuilder.
UDegree
¶ Returns or sets the u degree
-------------------------------------
Getter Method
Signature
UDegree()
Returns: Return type: int New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
UDegree(uDegree)
Parameters: uDegree (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
UPatches¶
-
DegreesAndSegmentsOrPatchesBuilder.
UPatches
¶ Returns or sets the u patches
-------------------------------------
Getter Method
Signature
UPatches()
Returns: Return type: int New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
UPatches(uPatches)
Parameters: uPatches (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
VDegree¶
-
DegreesAndSegmentsOrPatchesBuilder.
VDegree
¶ Returns or sets the v degree
-------------------------------------
Getter Method
Signature
VDegree()
Returns: Return type: int New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
VDegree(vDegree)
Parameters: vDegree (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
VPatches¶
-
DegreesAndSegmentsOrPatchesBuilder.
VPatches
¶ Returns or sets the v patches
-------------------------------------
Getter Method
Signature
VPatches()
Returns: Return type: int New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
VPatches(vPatches)
Parameters: vPatches (int) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Method Detail¶
FindObject¶
-
DegreesAndSegmentsOrPatchesBuilder.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Print¶
-
DegreesAndSegmentsOrPatchesBuilder.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
DegreesAndSegmentsOrPatchesBuilder.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
Validate¶
-
DegreesAndSegmentsOrPatchesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.