PatternIncrementItemOperationEnum Enumeration

NXOpen.GeometricUtilities.PatternIncrementItem.OperationEnum is an alias for NXOpen.GeometricUtilities.PatternIncrementItemOperationEnum

class NXOpen.GeometricUtilities.PatternIncrementItemOperationEnum

Bases: object

increment operation option.

Enum Members

Enum Member Enum Member Description
Add
add the increment to the master value.
Multiply
multiply the increment to the master value.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.