PolygonPattern Class

class NXOpen.GeometricUtilities.PolygonPattern

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

the polygon pattern definition.

Allows specification along both the angular and radial directions. .. versionadded:: NX8.0.0

Properties

Property Description
Flip Returns or sets the flip object for 2D mode.
HorizontalRef Returns the horizontal reference
NumberOfSides Returns the number of sides for the polygon type pattern will generated in this direction
PolygonSizeOption Returns or sets the polygon size option
PolygonSpacing Returns the polygon spacing of the instances of the pattern
RadialSpacing Returns the radial spacing of the instances of the pattern
RotationAxis Returns or sets the rotation axis for the pattern.
RotationCenter Returns or sets the rotation center for the 2d pattern.
Tag Returns the Tag for this object.
UseRadialDirectionToggle Returns or sets the UseRadialDirection toggle attribute.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

PolygonPatternSizeOptions Enumeration defines polygon size options for polygon type pattern.

Property Detail

Flip

PolygonPattern.Flip

Returns or sets the flip object for 2D mode.

This function gets the flip attribute of the 2D pattern.

-------------------------------------

Getter Method

Signature Flip()

Returns:
Return type:bool

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Flip(enabled)

Parameters:enabled (bool) –

New in version NX8.0.0.

License requirements: None.

HorizontalRef

PolygonPattern.HorizontalRef

Returns the horizontal reference

-------------------------------------

Getter Method

Signature HorizontalRef()

Returns:
Return type:NXOpen.GeometricUtilities.HorizontalReference

New in version NX8.0.0.

License requirements: None.

NumberOfSides

PolygonPattern.NumberOfSides

Returns the number of sides for the polygon type pattern will generated in this direction

-------------------------------------

Getter Method

Signature NumberOfSides()

Returns:
Return type:NXOpen.Expression

New in version NX8.0.0.

License requirements: None.

PolygonSizeOption

PolygonPattern.PolygonSizeOption

Returns or sets the polygon size option

-------------------------------------

Getter Method

Signature PolygonSizeOption()

Returns:
Return type:NXOpen.GeometricUtilities.PolygonPatternSizeOptions

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature PolygonSizeOption(option)

Parameters:option (NXOpen.GeometricUtilities.PolygonPatternSizeOptions) –

New in version NX8.0.0.

License requirements: None.

PolygonSpacing

PolygonPattern.PolygonSpacing

Returns the polygon spacing of the instances of the pattern

-------------------------------------

Getter Method

Signature PolygonSpacing()

Returns:
Return type:NXOpen.GeometricUtilities.PolygonPatternSpacing

New in version NX8.0.0.

License requirements: None.

RadialSpacing

PolygonPattern.RadialSpacing

Returns the radial spacing of the instances of the pattern

-------------------------------------

Getter Method

Signature RadialSpacing()

Returns:
Return type:NXOpen.GeometricUtilities.DistancePatternSpacing

New in version NX8.0.0.

License requirements: None.

RotationAxis

PolygonPattern.RotationAxis

Returns or sets the rotation axis for the pattern.

-------------------------------------

Getter Method

Signature RotationAxis()

Returns:
Return type:NXOpen.Axis

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature RotationAxis(rotationAxis)

Parameters:rotationAxis (NXOpen.Axis) –

New in version NX8.0.0.

License requirements: None.

RotationCenter

PolygonPattern.RotationCenter

Returns or sets the rotation center for the 2d pattern.

-------------------------------------

Getter Method

Signature RotationCenter()

Returns:
Return type:NXOpen.Point

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature RotationCenter(rotationCenter)

Parameters:rotationCenter (NXOpen.Point) –

New in version NX8.0.0.

License requirements: None.

UseRadialDirectionToggle

PolygonPattern.UseRadialDirectionToggle

Returns or sets the UseRadialDirection toggle attribute.

This function gets the UseRadialDirection toggle value

-------------------------------------

Getter Method

Signature UseRadialDirectionToggle()

Returns:
Return type:bool

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature UseRadialDirectionToggle(toggle)

Parameters:toggle (bool) –

New in version NX8.0.0.

License requirements: None.

Method Detail

Validate

PolygonPattern.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.