CurveFitDataJoin Enumeration

NXOpen.GeometricUtilities.CurveFitData.Join is an alias for NXOpen.GeometricUtilities.CurveFitDataJoin

class NXOpen.GeometricUtilities.CurveFitDataJoin

Bases: object

Represents the curve join method

Enum Members

Enum Member Enum Member Description
No
No
Cubic
Cubic
General
General
Quintic
Quintic
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.