CurveOptionsInputCurve Enumeration

NXOpen.GeometricUtilities.CurveOptions.InputCurve is an alias for NXOpen.GeometricUtilities.CurveOptionsInputCurve

class NXOpen.GeometricUtilities.CurveOptionsInputCurve

Bases: object

Represents the input curve options

Enum Members

Enum Member Enum Member Description
Retain
Retains the original input curve and creates the new output curve
Blank
Blanks the original input curve and creates the new output curve
Delete
Deletes the original input curve and creates the new output curve
Replace
Replaces the original input curve with the new output curve
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.