CurveShapingBuilder Class

class NXOpen.GeometricUtilities.CurveShapingBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.GeometricUtilities.CurveShapingBuilder.

This class allows shaping of curves by identifying key points on them and modifying the location of those points. It also allows constraining curve ends. .. versionadded:: NX7.5.0

Properties

Property Description
CanMoveAlongCurve Returns or sets the value indicating if point should be moved along curve.
ConstraintManager Returns the constraint manager.
EndContinuity Returns or sets the continuity at end of the curve
HasLinearTransition Returns or sets the value indicating if transition type is linear
InsertionMethod Returns or sets the point insertion method
MovementMethod Returns or sets the movement method
MovementPlane Returns or sets the movement plane
MovementVector Returns or sets the movement vector
Number Returns or sets the number of points to be inserted
OrientExpress Returns the orient express object
SelectCurves Returns the curve selection for point insertion
SpecifyPoints Returns the specified points to define insertion point locations
StartContinuity Returns or sets the continuity at start of the curve
Tag Returns the Tag for this object.
WCSOption Returns or sets the WCS option

Methods

Method Description
AddCurve Adds a curve for shaping
ApplyParameterValue Applies parameter value from a key point to a group of key points without affecting curve shape
Deform Deforms curves based on active points
DeleteAllPoints Deletes all points on a curve.
RemoveCurve Removes a curve
SetActivePoints Sets key points that are selected or will be moved
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

CurveShapingBuilderInsertionMethodOptions Enumeration Point insertion option
CurveShapingBuilderMovementMethodType Enumeration Curve parameter points movement types
CurveShapingBuilderWCSOptionType Enumeration WCS principal axis or plane types

Property Detail

CanMoveAlongCurve

CurveShapingBuilder.CanMoveAlongCurve

Returns or sets the value indicating if point should be moved along curve.

A key point is moved along the curve in order to change its parametric location without affecting curve shape.

-------------------------------------

Getter Method

Signature CanMoveAlongCurve()

Returns:
Return type:bool

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CanMoveAlongCurve(canMoveAlongCurve)

Parameters:canMoveAlongCurve (bool) –

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

ConstraintManager

CurveShapingBuilder.ConstraintManager

Returns the constraint manager.

Allows definition of key points to be used to shape the curve.

-------------------------------------

Getter Method

Signature ConstraintManager()

Returns:
Return type:NXOpen.Features.GeometricConstraintDataManager

New in version NX7.5.0.

License requirements: None.

EndContinuity

CurveShapingBuilder.EndContinuity

Returns or sets the continuity at end of the curve

-------------------------------------

Getter Method

Signature EndContinuity()

Returns:
Return type:NXOpen.GeometricUtilities.ContinuityContinuityTypes

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature EndContinuity(endContinuity)

Parameters:endContinuity (NXOpen.GeometricUtilities.ContinuityContinuityTypes) –

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

HasLinearTransition

CurveShapingBuilder.HasLinearTransition

Returns or sets the value indicating if transition type is linear

-------------------------------------

Getter Method

Signature HasLinearTransition()

Returns:
Return type:bool

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature HasLinearTransition(hasLinear)

Parameters:hasLinear (bool) –

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

InsertionMethod

CurveShapingBuilder.InsertionMethod

Returns or sets the point insertion method

-------------------------------------

Getter Method

Signature InsertionMethod()

Returns:
Return type:NXOpen.GeometricUtilities.CurveShapingBuilderInsertionMethodOptions

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature InsertionMethod(insertionMethod)

Parameters:insertionMethod (NXOpen.GeometricUtilities.CurveShapingBuilderInsertionMethodOptions) –

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

MovementMethod

CurveShapingBuilder.MovementMethod

Returns or sets the movement method

-------------------------------------

Getter Method

Signature MovementMethod()

Returns:
Return type:NXOpen.GeometricUtilities.CurveShapingBuilderMovementMethodType

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature MovementMethod(movementMethod)

Parameters:movementMethod (NXOpen.GeometricUtilities.CurveShapingBuilderMovementMethodType) –

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

MovementPlane

CurveShapingBuilder.MovementPlane

Returns or sets the movement plane

-------------------------------------

Getter Method

Signature MovementPlane()

Returns:
Return type:NXOpen.Plane

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature MovementPlane(movementPlane)

Parameters:movementPlane (NXOpen.Plane) –

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

MovementVector

CurveShapingBuilder.MovementVector

Returns or sets the movement vector

-------------------------------------

Getter Method

Signature MovementVector()

Returns:
Return type:NXOpen.Direction

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature MovementVector(movementVector)

Parameters:movementVector (NXOpen.Direction) –

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

Number

CurveShapingBuilder.Number

Returns or sets the number of points to be inserted

-------------------------------------

Getter Method

Signature Number()

Returns:
Return type:int

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Number(number)

Parameters:number (int) –

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

OrientExpress

CurveShapingBuilder.OrientExpress

Returns the orient express object

-------------------------------------

Getter Method

Signature OrientExpress()

Returns:
Return type:NXOpen.GeometricUtilities.OrientXpressBuilder

New in version NX7.5.0.

License requirements: None.

SelectCurves

CurveShapingBuilder.SelectCurves

Returns the curve selection for point insertion

-------------------------------------

Getter Method

Signature SelectCurves()

Returns:
Return type:NXOpen.SelectSplineList

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

SpecifyPoints

CurveShapingBuilder.SpecifyPoints

Returns the specified points to define insertion point locations

-------------------------------------

Getter Method

Signature SpecifyPoints()

Returns:
Return type:NXOpen.SelectPointList

New in version NX7.5.0.

License requirements: None.

StartContinuity

CurveShapingBuilder.StartContinuity

Returns or sets the continuity at start of the curve

-------------------------------------

Getter Method

Signature StartContinuity()

Returns:
Return type:NXOpen.GeometricUtilities.ContinuityContinuityTypes

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature StartContinuity(startContinuity)

Parameters:startContinuity (NXOpen.GeometricUtilities.ContinuityContinuityTypes) –

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

WCSOption

CurveShapingBuilder.WCSOption

Returns or sets the WCS option

-------------------------------------

Getter Method

Signature WCSOption()

Returns:
Return type:NXOpen.GeometricUtilities.CurveShapingBuilderWCSOptionType

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature WCSOption(wcsOption)

Parameters:wcsOption (NXOpen.GeometricUtilities.CurveShapingBuilderWCSOptionType) –

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

Method Detail

AddCurve

CurveShapingBuilder.AddCurve

Adds a curve for shaping

Signature AddCurve(curve)

Parameters:curve (NXOpen.Curve) – Curve to be deformed

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

ApplyParameterValue

CurveShapingBuilder.ApplyParameterValue

Applies parameter value from a key point to a group of key points without affecting curve shape

Signature ApplyParameterValue(sourcePoint, destinationPoints)

Parameters:
  • sourcePoint (NXOpen.Point) – Point whose parameter value to be applied
  • destinationPoints (list of NXOpen.Point) – Points to be edited

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

Deform

CurveShapingBuilder.Deform

Deforms curves based on active points

Signature Deform()

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

DeleteAllPoints

CurveShapingBuilder.DeleteAllPoints

Deletes all points on a curve.

If no curve is specified, deletes all points on all curves.

Signature DeleteAllPoints(curve)

Parameters:curve (NXOpen.Spline) – Curve

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

RemoveCurve

CurveShapingBuilder.RemoveCurve

Removes a curve

Signature RemoveCurve(curve)

Parameters:curve (NXOpen.Curve) – Curve to be deleted

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

SetActivePoints

CurveShapingBuilder.SetActivePoints

Sets key points that are selected or will be moved

Signature SetActivePoints(points, masterPoint)

Parameters:
  • points (list of NXOpen.Point) – Key points
  • masterPoint (NXOpen.Point) – Point which user actually moves to move a group of selected points

New in version NX7.5.0.

License requirements: studio_free_form (“STUDIO FREE FORM”)

Validate

CurveShapingBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.