HelixPatternDirectionTypes Enumeration

NXOpen.GeometricUtilities.HelixPattern.DirectionTypes is an alias for NXOpen.GeometricUtilities.HelixPatternDirectionTypes

class NXOpen.GeometricUtilities.HelixPatternDirectionTypes

Bases: object

This defines helix direction method

Enum Members

Enum Member Enum Member Description
Righthand
Right hand orientation.
Lefthand
Left hand orientation.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.