FaceChangeOverflowBehaviorOption Enumeration

NXOpen.GeometricUtilities.FaceChangeOverflowBehavior.Option is an alias for NXOpen.GeometricUtilities.FaceChangeOverflowBehaviorOption

class NXOpen.GeometricUtilities.FaceChangeOverflowBehaviorOption

Bases: object

face change option.

Enum Members

Enum Member Enum Member Description
Automatic
Automatic
ExtendChangeFace
Extend Change Face
ExtendIncidentFace
Extend Incident Face
ExtendCapFace
Extend Cap Face
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.