HelixPatternSizeOptions Enumeration

NXOpen.GeometricUtilities.HelixPattern.SizeOptions is an alias for NXOpen.GeometricUtilities.HelixPatternSizeOptions

class NXOpen.GeometricUtilities.HelixPatternSizeOptions

Bases: object

defines Helix size options for Helix type pattern.

Enum Members

Enum Member Enum Member Description
CountAngleDistance
use Count, Angle, Distance to define a Helix
CountHelixPitchAndTurns
use Count, Helix Pitch, Turns to define a Helix
CountHelixPitchAndSpan
use Count, Helix Pitch, Span to define a Helix
AngleHelixPitchAndTurns
use Angle, Helix Pitch, Turns to define a Helix
AngleHelixPitchAndSpan
use Angle, Helix Pitch, Span to define a Helix
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.