FeatureOptionsBodyStyle Enumeration

NXOpen.GeometricUtilities.FeatureOptions.BodyStyle is an alias for NXOpen.GeometricUtilities.FeatureOptionsBodyStyle

class NXOpen.GeometricUtilities.FeatureOptionsBodyStyle

Bases: object

This enum represents the various body types

Enum Members

Enum Member Enum Member Description
Solid
Solid Body
Sheet
Sheet Body
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.