OrientXpressBuilderPlane Enumeration

NXOpen.GeometricUtilities.OrientXpressBuilder.Plane is an alias for NXOpen.GeometricUtilities.OrientXpressBuilderPlane

class NXOpen.GeometricUtilities.OrientXpressBuilderPlane

Bases: object

the active plane option

Enum Members

Enum Member Enum Member Description
Yz
Active plane is parallel to yz-plane
Xz
Active plane is parallel to xz-plane
Xy
Active plane is parallel to xy-plane
Passive
Passive plane input mode
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.