PartModuleOutputBuilder Class¶
-
class
NXOpen.GeometricUtilities.
PartModuleOutputBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.GeometricUtilities.PartModuleOutputBuilder
To create a new instance of this class, use
NXOpen.Features.PartModule.CreatePartModuleOutputBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Activate | Returns or sets the option indicating whether the part module is to be activated. |
Deactivate | Returns or sets the option indicating whether the part module is to be deactivated. |
OutputReferences | Returns the part module output data |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Activate¶
-
PartModuleOutputBuilder.
Activate
¶ Returns or sets the option indicating whether the part module is to be activated.
If true, the part module will be activated, else, no action is taken
This API is now deprecated. Please use
NXOpen.Features.PartModule.Activate()
instead.-------------------------------------
Getter Method
Signature
Activate()
Returns: Return type: bool New in version NX8.0.0.
Deprecated since version NX9.0.0: Please use
NXOpen.Features.PartModule.Activate()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Activate(activate)
Parameters: activate (bool) – New in version NX8.0.0.
Deprecated since version NX9.0.0: Please use
NXOpen.Features.PartModule.Activate()
instead.License requirements: solid_modeling (“SOLIDS MODELING”)
Deactivate¶
-
PartModuleOutputBuilder.
Deactivate
¶ Returns or sets the option indicating whether the part module is to be deactivated.
If true, the part module will be deactivated, else, no action is taken
This API is now deprecated. Please use
NXOpen.Features.PartModule.Activate()
instead.-------------------------------------
Getter Method
Signature
Deactivate()
Returns: Return type: bool New in version NX8.0.0.
Deprecated since version NX9.0.0: Please use
NXOpen.Features.PartModule.Activate()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Deactivate(deactivate)
Parameters: deactivate (bool) – New in version NX8.0.0.
Deprecated since version NX9.0.0: Please use
NXOpen.Features.PartModule.Activate()
instead.License requirements: solid_modeling (“SOLIDS MODELING”)
OutputReferences¶
-
PartModuleOutputBuilder.
OutputReferences
¶ Returns the part module output data
This API is now deprecated. Please use
NXOpen.GeometricUtilities.PartModuleOutputBuilder1.OutputReferences1()
instead.-------------------------------------
Getter Method
Signature
OutputReferences()
Returns: Return type: NXOpen.GeometricUtilities.PartModuleReferencesBuilder
New in version NX8.0.0.
Deprecated since version NX9.0.0: Please use
NXOpen.GeometricUtilities.PartModuleOutputBuilder1.OutputReferences1()
instead.License requirements: None.
Method Detail¶
Validate¶
-
PartModuleOutputBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.