BlendLimitsData Class

class NXOpen.GeometricUtilities.BlendLimitsData

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.GeometricUtilities.BlendLimitsData

New in version NX5.0.0.

Properties

Property Description
CapsList Returns the caps list
Tag Returns the Tag for this object.
UserSelectedObjects Returns or sets the use plane cap blend

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

CapsList

BlendLimitsData.CapsList

Returns the caps list

-------------------------------------

Getter Method

Signature CapsList()

Returns:
Return type:NXOpen.TaggedObjectList

New in version NX5.0.0.

License requirements: None.

UserSelectedObjects

BlendLimitsData.UserSelectedObjects

Returns or sets the use plane cap blend

-------------------------------------

Getter Method

Signature UserSelectedObjects()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature UserSelectedObjects(useSelectedObject)

Parameters:useSelectedObject (bool) –

New in version NX6.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”)

Method Detail

Validate

BlendLimitsData.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.