Type Enumeration

class NXOpen.GeometricUtilities.Type

Bases: object

This enum represents the kind of offset Enum Members

Enum Member Enum Member Description
NoOffset
No offset
NonsymmetricOffset
Offset with two different distances
SymmetricOffset
Offset with same distance in both directions
SingleOffset
Offset with single distance in one direction
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.