FrameOnPathBuilder Class

class NXOpen.GeometricUtilities.FrameOnPathBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Frame on path builder

New in version NX7.5.1.

Properties

Property Description
AnchorLocation Returns or sets the anchor location
AnchorPosition Returns the anchor position
Height Returns the height
IsApexReversed Returns or sets the value indicating if apex point is reversed
Length Returns the length
Offset Returns the offset
Tag Returns the Tag for this object.
WScale Returns or sets the width scale

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

FrameOnPathBuilderAnchorLocationType Enumeration Anchor location types

Property Detail

AnchorLocation

FrameOnPathBuilder.AnchorLocation

Returns or sets the anchor location

-------------------------------------

Getter Method

Signature AnchorLocation()

Returns:
Return type:NXOpen.GeometricUtilities.FrameOnPathBuilderAnchorLocationType

New in version NX7.5.1.

License requirements: None.

-------------------------------------

Setter Method

Signature AnchorLocation(anchorLocation)

Parameters:anchorLocation (NXOpen.GeometricUtilities.FrameOnPathBuilderAnchorLocationType) –

New in version NX7.5.1.

License requirements: solid_modeling (“SOLIDS MODELING”)

AnchorPosition

FrameOnPathBuilder.AnchorPosition

Returns the anchor position

-------------------------------------

Getter Method

Signature AnchorPosition()

Returns:
Return type:NXOpen.GeometricUtilities.OnPathDimensionBuilder

New in version NX7.5.1.

License requirements: None.

Height

FrameOnPathBuilder.Height

Returns the height

-------------------------------------

Getter Method

Signature Height()

Returns:
Return type:NXOpen.Expression

New in version NX7.5.1.

License requirements: None.

IsApexReversed

FrameOnPathBuilder.IsApexReversed

Returns or sets the value indicating if apex point is reversed

-------------------------------------

Getter Method

Signature IsApexReversed()

Returns:
Return type:bool

New in version NX7.5.1.

License requirements: None.

-------------------------------------

Setter Method

Signature IsApexReversed(isReversed)

Parameters:isReversed (bool) –

New in version NX7.5.1.

License requirements: solid_modeling (“SOLIDS MODELING”)

Length

FrameOnPathBuilder.Length

Returns the length

-------------------------------------

Getter Method

Signature Length()

Returns:
Return type:NXOpen.Expression

New in version NX7.5.1.

License requirements: None.

Offset

FrameOnPathBuilder.Offset

Returns the offset

-------------------------------------

Getter Method

Signature Offset()

Returns:
Return type:NXOpen.Expression

New in version NX7.5.1.

License requirements: None.

WScale

FrameOnPathBuilder.WScale

Returns or sets the width scale

-------------------------------------

Getter Method

Signature WScale()

Returns:
Return type:float

New in version NX7.5.1.

License requirements: None.

-------------------------------------

Setter Method

Signature WScale(wScale)

Parameters:wScale (float) –

New in version NX7.5.1.

License requirements: None.

Method Detail

Validate

FrameOnPathBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.