ReplAsstBuilder Class

class NXOpen.GeometricUtilities.ReplAsstBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.GeometricUtilities.ReplAsstBuilder.

This is the primary data container for Replacement Assistant mapping environment available on editing Linked Body, Linked Face, Extract Body, Extract Face and Mirror Body features. Execute Enter() before invoking any match creation or automatic matching APIs. Call Exit() to exit the mapping environment.

New in version NX6.0.0.

Properties

Property Description
Allowance Returns or sets the deviation allowance for geometric matching
MatchList Returns the list of all Parent Equivalency Map objects
MatchSheetBoundariesOnly Returns or sets the automatic matching preference to match sheet boundaries only
OneToOne Returns or sets the one to one auto matching preference
Tag Returns the Tag for this object.
UsageInfoList Returns the list of all Entity Usage Info objects

Methods

Method Description
CreateEmptyMatch This is the default creator for a parent equivalency map.
CreateGeometricMaps Perform geometric matching.
CreateInferredMaps Infer more matches from matches already ‘Accepted’.
CreateNameBasedMaps Perform automatic matching based on user-defined object names.
Enter Entry and re-entry to the Replacement Assistant mapping environment.
Exit Exit the Replacement Assistant mapping environment.
QueryFeatureOutputUsage Query the downstream usage of the current feature’s output entities and populate the usageInfoList.
SetNewParents Set the source entities for the Replacement Assistant.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

Allowance

ReplAsstBuilder.Allowance

Returns or sets the deviation allowance for geometric matching

-------------------------------------

Getter Method

Signature Allowance()

Returns:
Return type:float

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Allowance(allowance)

Parameters:allowance (float) –

New in version NX6.0.0.

License requirements: None.

MatchList

ReplAsstBuilder.MatchList

Returns the list of all Parent Equivalency Map objects

-------------------------------------

Getter Method

Signature MatchList()

Returns:
Return type:NXOpen.GeometricUtilities.ParentEquivalencyMapList

New in version NX6.0.0.

License requirements: None.

MatchSheetBoundariesOnly

ReplAsstBuilder.MatchSheetBoundariesOnly

Returns or sets the automatic matching preference to match sheet boundaries only

-------------------------------------

Getter Method

Signature MatchSheetBoundariesOnly()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature MatchSheetBoundariesOnly(sheetBoundariesOnly)

Parameters:sheetBoundariesOnly (bool) –

New in version NX6.0.0.

License requirements: None.

OneToOne

ReplAsstBuilder.OneToOne

Returns or sets the one to one auto matching preference

-------------------------------------

Getter Method

Signature OneToOne()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature OneToOne(oneToOne)

Parameters:oneToOne (bool) –

New in version NX6.0.0.

License requirements: None.

UsageInfoList

ReplAsstBuilder.UsageInfoList

Returns the list of all Entity Usage Info objects

-------------------------------------

Getter Method

Signature UsageInfoList()

Returns:
Return type:NXOpen.GeometricUtilities.EntityUsageInfoList

New in version NX6.0.0.

License requirements: None.

Method Detail

CreateEmptyMatch

ReplAsstBuilder.CreateEmptyMatch

This is the default creator for a parent equivalency map.

Signature CreateEmptyMatch()

Returns:
Return type:NXOpen.GeometricUtilities.ParentEquivalencyMap

New in version NX6.0.0.

License requirements: None.

CreateGeometricMaps

ReplAsstBuilder.CreateGeometricMaps

Perform geometric matching.

Signature CreateGeometricMaps()

Returns:new maps created by geometric matching
Return type:list of NXOpen.GeometricUtilities.ParentEquivalencyMap

New in version NX6.0.0.

License requirements: None.

CreateInferredMaps

ReplAsstBuilder.CreateInferredMaps

Infer more matches from matches already ‘Accepted’.

Add [array_order_guaranteed] annotation for output array when API wrap allows the same.

Signature CreateInferredMaps()

Returns:new maps created by inferring
Return type:list of NXOpen.GeometricUtilities.ParentEquivalencyMap

New in version NX6.0.0.

License requirements: None.

CreateNameBasedMaps

ReplAsstBuilder.CreateNameBasedMaps

Perform automatic matching based on user-defined object names.

Signature CreateNameBasedMaps()

Returns:new maps created by name-based matching
Return type:list of NXOpen.GeometricUtilities.ParentEquivalencyMap

New in version NX6.0.0.

License requirements: None.

Enter

ReplAsstBuilder.Enter

Entry and re-entry to the Replacement Assistant mapping environment.

This function needs to be executed before invoking any match creation or automatic matching APIs. The matches inferred internally (internal identifier reuse, inherited from parent and siblings) will be populated when this function is executed for the first time after selecting a replacement entity.

Signature Enter()

New in version NX6.0.0.

License requirements: None.

Exit

ReplAsstBuilder.Exit

Exit the Replacement Assistant mapping environment.

Any match creation or automatic matchping API cannot be executed after this function is called.

Signature Exit()

New in version NX6.0.0.

License requirements: None.

QueryFeatureOutputUsage

ReplAsstBuilder.QueryFeatureOutputUsage

Query the downstream usage of the current feature’s output entities and populate the usageInfoList.

This API need be called only ONCE per feature being reparented.

Signature QueryFeatureOutputUsage()

Returns:
Return type:int

New in version NX6.0.0.

License requirements: None.

SetNewParents

ReplAsstBuilder.SetNewParents

Set the source entities for the Replacement Assistant.

If there are matches already created and the body is changed, the matches will be deleted.

Signature SetNewParents(replacementObjects)

Parameters:replacementObjects (list of NXOpen.DisplayableObject) – replacement objects

New in version NX6.0.0.

License requirements: None.

Validate

ReplAsstBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.