EnumTestCars Enumeration

NXOpen.GeometricUtilities.EnumTest.Cars is an alias for NXOpen.GeometricUtilities.EnumTestCars

class NXOpen.GeometricUtilities.EnumTestCars

Bases: object

Cars are dangerous to eat and not very tasty

Enum Members

Enum Member Enum Member Description
Mustang
Mustangs might be good eating though
Edsel
Edsels look funny
Tucker
Tucker could run for president of the ‘guys who got screwed by corporate America’ club
Citroen
Citrons are edible but Citroens are strange
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.