FeatureOffset Class¶
-
class
NXOpen.GeometricUtilities.
FeatureOffset
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a Offset .
New in version NX3.0.1.
Properties¶
Property | Description |
---|---|
EndOffset | Returns the End Offset |
Option | Returns or sets the Offset option |
StartOffset | Returns the Start Offset |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
SetEndOffset | The End Offset |
SetStartOffset | The Start Offset |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
EndOffset¶
-
FeatureOffset.
EndOffset
¶ Returns the End Offset
-------------------------------------
Getter Method
Signature
EndOffset()
Returns: end offset Return type: NXOpen.Expression
New in version NX3.0.1.
License requirements: None.
Option¶
-
FeatureOffset.
Option
¶ Returns or sets the Offset option
-------------------------------------
Getter Method
Signature
Option()
Returns: offset type Return type: NXOpen.GeometricUtilities.Type
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Option(offsetType)
Parameters: offsetType ( NXOpen.GeometricUtilities.Type
) – offset typeNew in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
StartOffset¶
-
FeatureOffset.
StartOffset
¶ Returns the Start Offset
-------------------------------------
Getter Method
Signature
StartOffset()
Returns: end offset Return type: NXOpen.Expression
New in version NX3.0.1.
License requirements: None.
Method Detail¶
SetEndOffset¶
-
FeatureOffset.
SetEndOffset
¶ The End Offset
Signature
SetEndOffset(valueExpression)
Parameters: valueExpression (str) – value of end offset expression New in version NX3.0.1.
Deprecated since version NX8.5.0: To set the value of the expression modify the expression directly using
GeometricUtilities.FeatureOffset.EndOffset()
andExpression.RightHandSide()
.License requirements: solid_modeling (“SOLIDS MODELING”)
SetStartOffset¶
-
FeatureOffset.
SetStartOffset
¶ The Start Offset
Signature
SetStartOffset(valueExpression)
Parameters: valueExpression (str) – value of start offset expression New in version NX3.0.1.
Deprecated since version NX8.5.0: To set the value of the expression modify the expression directly using
GeometricUtilities.FeatureOffset.StartOffset()
andExpression.RightHandSide()
.License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
FeatureOffset.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.