RectangularPattern Class

class NXOpen.GeometricUtilities.RectangularPattern

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

the rectangular pattern definition.

Allows specification along two linear axes, which may or may not be orthogonal. .. versionadded:: NX7.5.0

Properties

Property Description
CreateLastStaggered Returns or sets the option to generate the last item in a staggered row.
HorizontalRef Returns the horizontal reference
SimplifiedLayoutType Returns or sets the simplified layout type to be used by the pattern
StaggerType Returns or sets the type of stagger to be used by the pattern
Tag Returns the Tag for this object.
UseYDirectionToggle Returns or sets the UseYDirection toggle attribute.
XDirection Returns or sets the x axis
XFlip Returns or sets the XSelection flip attribute.
XSelection Returns the direction object.
XSpacing Returns the instance spacing along the x axis
XSymmetryToggle Returns or sets the XSymmetry toggle attribute.
YDirection Returns or sets the y axis, which can be any vector not parallel to the x axis
YFlip Returns or sets the YSelection flip attribute.
YSelection Returns the direction object.
YSpacing Returns the instance spacing along the y axis
YSymmetryToggle Returns or sets the YSymmetry toggle attribute.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

RectangularPatternSimplifiedLayoutTypes Enumeration defines simplified layout type for linear pattern.
RectangularPatternStaggerOptions Enumeration defines any stagger to be defined on the pattern.

Property Detail

CreateLastStaggered

RectangularPattern.CreateLastStaggered

Returns or sets the option to generate the last item in a staggered row.

If ‘true’ the pattern will be narrower on rows that have been staggered.

-------------------------------------

Getter Method

Signature CreateLastStaggered()

Returns:
Return type:bool

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CreateLastStaggered(create)

Parameters:create (bool) –

New in version NX7.5.0.

License requirements: None.

HorizontalRef

RectangularPattern.HorizontalRef

Returns the horizontal reference

-------------------------------------

Getter Method

Signature HorizontalRef()

Returns:
Return type:NXOpen.GeometricUtilities.HorizontalReference

New in version NX8.0.0.

License requirements: None.

SimplifiedLayoutType

RectangularPattern.SimplifiedLayoutType

Returns or sets the simplified layout type to be used by the pattern

-------------------------------------

Getter Method

Signature SimplifiedLayoutType()

Returns:
Return type:NXOpen.GeometricUtilities.RectangularPatternSimplifiedLayoutTypes

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SimplifiedLayoutType(type)

Parameters:type (NXOpen.GeometricUtilities.RectangularPatternSimplifiedLayoutTypes) –

New in version NX8.0.0.

License requirements: None.

StaggerType

RectangularPattern.StaggerType

Returns or sets the type of stagger to be used by the pattern

-------------------------------------

Getter Method

Signature StaggerType()

Returns:
Return type:NXOpen.GeometricUtilities.RectangularPatternStaggerOptions

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature StaggerType(spaceType)

Parameters:spaceType (NXOpen.GeometricUtilities.RectangularPatternStaggerOptions) –

New in version NX7.5.0.

License requirements: None.

UseYDirectionToggle

RectangularPattern.UseYDirectionToggle

Returns or sets the UseYDirection toggle attribute.

This function gets the UseYDirection toggle value

-------------------------------------

Getter Method

Signature UseYDirectionToggle()

Returns:
Return type:bool

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature UseYDirectionToggle(toggle)

Parameters:toggle (bool) –

New in version NX7.5.0.

License requirements: None.

XDirection

RectangularPattern.XDirection

Returns or sets the x axis

-------------------------------------

Getter Method

Signature XDirection()

Returns:
Return type:NXOpen.Direction

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature XDirection(xDirection)

Parameters:xDirection (NXOpen.Direction) –

New in version NX7.5.0.

License requirements: None.

XFlip

RectangularPattern.XFlip

Returns or sets the XSelection flip attribute.

This function flips X selection object of the 2D pattern

-------------------------------------

Getter Method

Signature XFlip()

Returns:
Return type:bool

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature XFlip(flip)

Parameters:flip (bool) –

New in version NX7.5.0.

License requirements: None.

XSelection

RectangularPattern.XSelection

Returns the direction object.

This function gets X direction object of the 2D pattern. This call will result in an Exception if not called in 2D mode.

-------------------------------------

Getter Method

Signature XSelection()

Returns:
Return type:NXOpen.SelectNXObject

New in version NX7.5.0.

License requirements: None.

XSpacing

RectangularPattern.XSpacing

Returns the instance spacing along the x axis

-------------------------------------

Getter Method

Signature XSpacing()

Returns:
Return type:NXOpen.GeometricUtilities.DistancePatternSpacing

New in version NX7.5.0.

License requirements: None.

XSymmetryToggle

RectangularPattern.XSymmetryToggle

Returns or sets the XSymmetry toggle attribute.

This function gets the x Symmetry toggle value

-------------------------------------

Getter Method

Signature XSymmetryToggle()

Returns:
Return type:bool

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature XSymmetryToggle(toggle)

Parameters:toggle (bool) –

New in version NX7.5.0.

License requirements: None.

YDirection

RectangularPattern.YDirection

Returns or sets the y axis, which can be any vector not parallel to the x axis

-------------------------------------

Getter Method

Signature YDirection()

Returns:
Return type:NXOpen.Direction

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature YDirection(yDirection)

Parameters:yDirection (NXOpen.Direction) –

New in version NX7.5.0.

License requirements: None.

YFlip

RectangularPattern.YFlip

Returns or sets the YSelection flip attribute.

This function flips Y selection object of the 2D pattern

-------------------------------------

Getter Method

Signature YFlip()

Returns:
Return type:bool

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature YFlip(flip)

Parameters:flip (bool) –

New in version NX7.5.0.

License requirements: None.

YSelection

RectangularPattern.YSelection

Returns the direction object.

This function gets Y direction object of the 2D pattern. This call will result in an Exception if not called in 2D mode.

-------------------------------------

Getter Method

Signature YSelection()

Returns:
Return type:NXOpen.SelectNXObject

New in version NX7.5.0.

License requirements: None.

YSpacing

RectangularPattern.YSpacing

Returns the instance spacing along the y axis

-------------------------------------

Getter Method

Signature YSpacing()

Returns:
Return type:NXOpen.GeometricUtilities.DistancePatternSpacing

New in version NX7.5.0.

License requirements: None.

YSymmetryToggle

RectangularPattern.YSymmetryToggle

Returns or sets the YSymmetry toggle attribute.

This function gets the y Symmetry toggle value

-------------------------------------

Getter Method

Signature YSymmetryToggle()

Returns:
Return type:bool

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature YSymmetryToggle(toggle)

Parameters:toggle (bool) –

New in version NX7.5.0.

License requirements: None.

Method Detail

Validate

RectangularPattern.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.