BooleanToolBuilderBooleanToolType Enumeration

NXOpen.GeometricUtilities.BooleanToolBuilder.BooleanToolType is an alias for NXOpen.GeometricUtilities.BooleanToolBuilderBooleanToolType

class NXOpen.GeometricUtilities.BooleanToolBuilderBooleanToolType

Bases: object

the boolean tool created options

Enum Members

Enum Member Enum Member Description
FaceOrPlane
Tool consists of sets of faces or datum planes
NewPlane
Tool consists of plane created on the fly
Extrude
Tool consists of extrude created on the fly
Revolve
Tool consists of revolve created on the fly
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.