SurfaceRangeBuilderAnchorPositionType Enumeration

NXOpen.GeometricUtilities.SurfaceRangeBuilder.AnchorPositionType is an alias for NXOpen.GeometricUtilities.SurfaceRangeBuilderAnchorPositionType

class NXOpen.GeometricUtilities.SurfaceRangeBuilderAnchorPositionType

Bases: object

Represents the anchor position type

Enum Members

Enum Member Enum Member Description
Center
Anchor at the center of the surface
Vertex1
Anchor at the first corner of the surface
Vertex2
Anchor at the second corner of the surface
Vertex3
Anchor at the third corner of the surface
Vertex4
Anchor at the fourth corner of the surface
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.