EndHoleDataHoleDepthLimitOptions Enumeration¶
NXOpen.GeometricUtilities.EndHoleData.HoleDepthLimitOptions is an alias for NXOpen.GeometricUtilities.EndHoleDataHoleDepthLimitOptions
-
class
NXOpen.GeometricUtilities.
EndHoleDataHoleDepthLimitOptions
¶ Bases:
object
Represents hole depth limit options for threaded hole in end plate of hole series.
Enum Members
Enum Member Enum Member Description Value Value limit optionsUntilSelected Until selected limit optionsUntilNext Until next limit optionsThroughBody Through body limit options-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-