QuadrilateralFrameBuilder Class

class NXOpen.GeometricUtilities.QuadrilateralFrameBuilder

Bases: NXOpen.GeometricUtilities.ShapeFrameBuilder

Represents a NXOpen.GeometricUtilities.QuadrilateralFrameBuilder

New in version NX6.0.0.

Properties

Property Description
Anchor Returns the anchor of the frame
AnchorAttachment Returns or sets the anchor attachment
NumberVertices Returns the number of vertices of the frame
Subtype Returns or sets the subtype
Tag Returns the Tag for this object.

Methods

Method Description
GetMidpointCoords Gets the coordinates of the i-th midpoint of the frame with respect to the plane @return coordinates of midpoint relative with respect to plane
GetVertexCoords Gets the coordinates of the i-th vertex of the frame with respect to the plane @return coordinates of vertex relative with respect to plane
SetMidpointCoords Sets the coordinates of the i-th midpoint of the frame with respect to the plane
SetVertexCoords Sets the coordinates of the i-th vertex of the frame with respect to the plane
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

QuadrilateralFrameBuilderSubtypes Enumeration Represents the quadrialteral frame subtypes

Property Detail

Subtype

QuadrilateralFrameBuilder.Subtype

Returns or sets the subtype

-------------------------------------

Getter Method

Signature Subtype()

Returns:
Return type:NXOpen.GeometricUtilities.QuadrilateralFrameBuilderSubtypes

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Subtype(subtype)

Parameters:subtype (NXOpen.GeometricUtilities.QuadrilateralFrameBuilderSubtypes) –

New in version NX6.0.0.

License requirements: None.

Method Detail

Validate

QuadrilateralFrameBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.