ReduceSurfaceRadiusBuilderFaceSelectionSpecification Enumeration

NXOpen.GeometricUtilities.ReduceSurfaceRadiusBuilder.FaceSelectionSpecification is an alias for NXOpen.GeometricUtilities.ReduceSurfaceRadiusBuilderFaceSelectionSpecification

class NXOpen.GeometricUtilities.ReduceSurfaceRadiusBuilderFaceSelectionSpecification

Bases: object

Specify the face selection type.

There are three types: Select Faces by Radius, Select Faces by Chain and Single Selection.

Enum Members

Enum Member Enum Member Description
Radius
Chain
Select
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.