CurveRangeBuilderAnchorPositionType Enumeration¶
NXOpen.GeometricUtilities.CurveRangeBuilder.AnchorPositionType is an alias for NXOpen.GeometricUtilities.CurveRangeBuilderAnchorPositionType
-
class
NXOpen.GeometricUtilities.
CurveRangeBuilderAnchorPositionType
¶ Bases:
object
Represents the anchor position type
Enum Members
Enum Member Enum Member Description Start Anchor at the start of the curveCenter Anchor at the center of the curveEnd Anchor at the end of the curve-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-