PatternOrientationEnum Enumeration¶
NXOpen.GeometricUtilities.PatternOrientation.Enum is an alias for NXOpen.GeometricUtilities.PatternOrientationEnum
-
class
NXOpen.GeometricUtilities.
PatternOrientationEnum
¶ Bases:
object
pattern orientation options for all pattern types.
Enum Members
Enum Member Enum Member Description Fixed same orientation as the seed.NormalToPath normal to path orientation for Along Type first direction.NormalToVector normal to vector orientation for Along Type first direction.ParallelToVector parallel to vector orientation for Along Type first direction.ThroughAxis through axis orientation for Along Type first direction.FollowPattern follow pattern orientation, for example, circular pattern type.FollowCSYS follow CSYS orientation, for general pattern type, when from/to is CSYS.CSYStoCSYS a relative orientation defined by two CSYSs to transform the seed to an instance location.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-