MirrorPattern Class¶
-
class
NXOpen.GeometricUtilities.
MirrorPattern
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
the Mirror pattern definition.
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ExistingPlane | Returns the Existing Mirror Plane |
NewPlane | Returns or sets the new plane |
PlaneOption | Returns or sets the plane option |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MirrorPatternPlaneOptions Enumeration | the Plane options. |
Property Detail¶
ExistingPlane¶
-
MirrorPattern.
ExistingPlane
¶ Returns the Existing Mirror Plane
-------------------------------------
Getter Method
Signature
ExistingPlane()
Returns: Return type: NXOpen.SelectISurface
New in version NX8.0.0.
License requirements: None.
NewPlane¶
-
MirrorPattern.
NewPlane
¶ Returns or sets the new plane
-------------------------------------
Getter Method
Signature
NewPlane()
Returns: Return type: NXOpen.Plane
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NewPlane(newPlane)
Parameters: newPlane ( NXOpen.Plane
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
PlaneOption¶
-
MirrorPattern.
PlaneOption
¶ Returns or sets the plane option
-------------------------------------
Getter Method
Signature
PlaneOption()
Returns: Return type: NXOpen.GeometricUtilities.MirrorPatternPlaneOptions
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlaneOption(planeOptions)
Parameters: planeOptions ( NXOpen.GeometricUtilities.MirrorPatternPlaneOptions
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
Validate¶
-
MirrorPattern.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.