AlongPathPattern Class

class NXOpen.GeometricUtilities.AlongPathPattern

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

the AlongPath pattern definition.

Allows specification along two section pathes. .. versionadded:: NX7.5.0

Properties

Property Description
Tag Returns the Tag for this object.
UseYDirectionToggle Returns or sets the UseYDirection toggle attribute.
XOnPathSpacing Returns the on path instance spacing along the x path
XPath Returns or sets the x path
XPathOption Returns or sets the x path options
YDirection Returns or sets the y axis, which can be any vector not parallel to the x axis
YDirectionOption Returns or sets the y direction options
YOnPathSpacing Returns the on path instance spacing along the y path
YPath Returns or sets the y path, which can be any continuous section
YPathOption Returns or sets the y path options
YSpacing Returns the instance spacing along the y axis

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

AlongPathPatternPathOptions Enumeration This defines path options
AlongPathPatternYDirectionOptions Enumeration This defines y direction Types

Property Detail

UseYDirectionToggle

AlongPathPattern.UseYDirectionToggle

Returns or sets the UseYDirection toggle attribute.

This function gets the UseYDirection toggle value

-------------------------------------

Getter Method

Signature UseYDirectionToggle()

Returns:
Return type:bool

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature UseYDirectionToggle(toggle)

Parameters:toggle (bool) –

New in version NX7.5.0.

License requirements: None.

XOnPathSpacing

AlongPathPattern.XOnPathSpacing

Returns the on path instance spacing along the x path

-------------------------------------

Getter Method

Signature XOnPathSpacing()

Returns:
Return type:NXOpen.GeometricUtilities.OnPathDistancePatternSpacing

New in version NX7.5.0.

License requirements: None.

XPath

AlongPathPattern.XPath

Returns or sets the x path

-------------------------------------

Getter Method

Signature XPath()

Returns:
Return type:NXOpen.Section

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature XPath(xPath)

Parameters:xPath (NXOpen.Section) –

New in version NX7.5.0.

License requirements: None.

XPathOption

AlongPathPattern.XPathOption

Returns or sets the x path options

-------------------------------------

Getter Method

Signature XPathOption()

Returns:
Return type:NXOpen.GeometricUtilities.AlongPathPatternPathOptions

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature XPathOption(xPathOption)

Parameters:xPathOption (NXOpen.GeometricUtilities.AlongPathPatternPathOptions) –

New in version NX8.0.0.

License requirements: None.

YDirection

AlongPathPattern.YDirection

Returns or sets the y axis, which can be any vector not parallel to the x axis

-------------------------------------

Getter Method

Signature YDirection()

Returns:
Return type:NXOpen.Direction

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature YDirection(yDirection)

Parameters:yDirection (NXOpen.Direction) –

New in version NX7.5.0.

License requirements: None.

YDirectionOption

AlongPathPattern.YDirectionOption

Returns or sets the y direction options

-------------------------------------

Getter Method

Signature YDirectionOption()

Returns:
Return type:NXOpen.GeometricUtilities.AlongPathPatternYDirectionOptions

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature YDirectionOption(yDirectionOption)

Parameters:yDirectionOption (NXOpen.GeometricUtilities.AlongPathPatternYDirectionOptions) –

New in version NX7.5.0.

License requirements: None.

YOnPathSpacing

AlongPathPattern.YOnPathSpacing

Returns the on path instance spacing along the y path

-------------------------------------

Getter Method

Signature YOnPathSpacing()

Returns:
Return type:NXOpen.GeometricUtilities.OnPathDistancePatternSpacing

New in version NX7.5.0.

License requirements: None.

YPath

AlongPathPattern.YPath

Returns or sets the y path, which can be any continuous section

-------------------------------------

Getter Method

Signature YPath()

Returns:
Return type:NXOpen.Section

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature YPath(yPath)

Parameters:yPath (NXOpen.Section) –

New in version NX7.5.0.

License requirements: None.

YPathOption

AlongPathPattern.YPathOption

Returns or sets the y path options

-------------------------------------

Getter Method

Signature YPathOption()

Returns:
Return type:NXOpen.GeometricUtilities.AlongPathPatternPathOptions

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature YPathOption(yPathOption)

Parameters:yPathOption (NXOpen.GeometricUtilities.AlongPathPatternPathOptions) –

New in version NX8.0.0.

License requirements: None.

YSpacing

AlongPathPattern.YSpacing

Returns the instance spacing along the y axis

-------------------------------------

Getter Method

Signature YSpacing()

Returns:
Return type:NXOpen.GeometricUtilities.DistancePatternSpacing

New in version NX7.5.0.

License requirements: None.

Method Detail

Validate

AlongPathPattern.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.