StyledSweepReferenceMethodBuilderReferenceOptions Enumeration

NXOpen.GeometricUtilities.StyledSweepReferenceMethodBuilder.ReferenceOptions is an alias for NXOpen.GeometricUtilities.StyledSweepReferenceMethodBuilderReferenceOptions

class NXOpen.GeometricUtilities.StyledSweepReferenceMethodBuilderReferenceOptions

Bases: object

This enum represents the orientation reference option.

By default, it is set to guide.

Enum Members

Enum Member Enum Member Description
ToGuide
Guide
ToCurve
Curve
ToVector
Vector Direction
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.