EndHoleDataFormOptions Enumeration

NXOpen.GeometricUtilities.EndHoleData.FormOptions is an alias for NXOpen.GeometricUtilities.EndHoleDataFormOptions

class NXOpen.GeometricUtilities.EndHoleDataFormOptions

Bases: object

Represents hole form options.

Enum Members

screw_clearance option should be used “

ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.