EnumTestConstraints Enumeration

NXOpen.GeometricUtilities.EnumTest.Constraints is an alias for NXOpen.GeometricUtilities.EnumTestConstraints

class NXOpen.GeometricUtilities.EnumTestConstraints

Bases: object

constraints are rather smelly

Enum Members

Enum Member Enum Member Description
Coincident
coincident constraints are not coincidental
Parallel
parallel constraints can run serially
Colinear
colinear constraints can’t run parallel
Concentric
concentric constraints are... ah, screw it
EqualRadius
I’m giving up
Fixed
ahhhhh, it’s over
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.