Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.ame |
Provides classes and interfaces for AME.
|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.diagramminglibraryauthor |
Provides classes and interfaces for Diagramming Library Authoring.
|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Class and Description |
---|
AddReusablePartCollection
Represents a collection of AddReusablePart
To obtain an instance of this class, refer to Part Created in NX5.0.0 |
CAMDataManager
Represents an object that manages cam data objects.
|
ToolingManager
Contains the collection objects for creating and iterating over Reuse Library objects.
|
ToolingSession |
Class and Description |
---|
SelectReuseLibraryItemBuilder
Select a part from the reuse library .
|
Class and Description |
---|
CaeReuseLibrary
Represents a
CaeReuseLibrary
To obtain an instance of this class, refer to BaseFEModel Created in NX7.5.2 |
Class and Description |
---|
SelectReuseLibraryItemBuilder
Select a part from the reuse library .
|
Class and Description |
---|
PrebendBuilder
Represents a
PrebendBuilder builder to divide bend faces. |
UniversalUnformBuilder
Represents a
UniversalUnformBuilder builder. |
Class and Description |
---|
SpreadsheetData
Represents the spreadsheet data which could be standalone spreadsheet file
with special format or be the spreadsheet data from part family template part,
the latter format will not have any other data except the name and value in
class
SpreadsheetDataParameter , that means
it might not return any result in some methods such as "GetDefinedAttributesExpressions". |
SpreadsheetDataParameter
Represents parameter in the spreadsheet.
|
Class and Description |
---|
AddReusableFeatureBuilder
Represents a
AddReusableFeatureBuilder To create a new instance of this class, use AddReusableFeatureCollection.createBuilder(nxopen.tooling.AddReusableFeatureCollection.InputData) Default values. |
AddReusableFeatureBuilder.LayerOptionType
Represents the layer option type
|
AddReusableFeatureBuilder.UserExpressionsData
This class holds the data returned from
AddReusableFeatureBuilder.getUserExpressions() |
AddReusableFeatureCollection
Represents a collection of AddReusableFeature
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
AddReusableFeatureCollection.InputData
Defines the input data of AddReusableFeatureBuilder
|
AddReusablePart
Represents a
AddReusablePart
To create a new instance of this class, use AddReusablePartCollection.createBuilder() Default values. |
AddReusablePart.ComponentMode
Represents the component type of the added part
|
AddReusablePart.ModeMethod
Represents adding or editing a reusable component mode method
|
AddReusablePart.PocketBodyMethod
Represents save pocket body information, updating or deleting a pocket body size mode method
|
AddReusablePart.PositionMethod
Represents the position method
|
AssemblyDrawingBuilder
Represents a
AssemblyDrawingBuilder which is
used to create or edit the Assembly Drawing. |
AssemblyDrawingBuilder.AttributeNames
Specifies the attribute name
|
AssemblyDrawingBuilder.AttributeValues
Specifies the attribute value.
|
AssemblyDrawingBuilder.DrawingCreateOrEdit
Specifies the sheet operation.
|
AssemblyDrawingBuilder.DrawingTypes
Specifies the drawing type.
|
AssemblyDrawingBuilder.ModelViewToUseValue
Specifies the model view to use.
|
AssemblyDrawingBuilder.Types
Specifies the filter of assembly.
|
AssemblyDrawingBuilder.ViewOptionValue
Specifies the view options.
|
AssignPatchBuilder
Represents a builder to be used to add sheet bodies as patch surfaces or delete patch surfaces.
|
AssignPatchBuilder.ConvertTypeOption
The option to convert to have copies or no copies for all selected sheets.
|
AssignPatchBuilder.PatchColorData
This class holds the data returned from
AssignPatchBuilder.getPatchColor() |
AssignPatchBuilder.Types
The types for assigning sheets.
|
AssignPatchCollection
Represents a collection of AssignPatch builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
AutoDieCollection
Represents a collection of Die Design Draw Punch
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
AutoDimensionBuilder
Represents a
AutoDimensionBuilder which is
used to create or edit the Auto Dimension. |
AutoDimensionBuilder.MainType
create or edit ordinate dimension
|
AutoDimensionBuilder.TextFontType
text font type
|
AutoDimensionBuilder.TextOrientationType
text orientation type
|
AutoDimensionBuilder.ToleranceType
tolerance type
|
AutoDimensionBuilder.ValuePrecisionType
value precision type
|
BackingPadBuilder
Represents a
BackingPadBuilder which is used to create or delete the Backing Pad. |
BackingPadBuilder.Types
types of backing pad design
|
BendInsertDesignBuilder
Represents a
BendInsertDesignBuilder
Bend Insert Design is to create inset puch or die for bend . |
BendInsertDesignBuilder.BendingDirectionOption
the bending direction.
|
BendInsertDesignBuilder.BendTypeOption
the bend type.
|
BendInsertDesignBuilder.BlankPositions
Specifies the blank position.
|
BendInsertDesignBuilder.InsertTypeOption
the insert type.
|
BendInsertDesignBuilder.ParentOption
the parent node.
|
BendInsertDesignBuilder.Types
the bending operation.
|
BendInsertDesignCollection
Creates a
BendInsertDesignCollection To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
BendOperationBuilder
Represents a
BendOperationBuilder builder. |
BendOperationBuilder.OverbendOptions
The overbend option.
|
BendOperationBuilder.Prebend
The number of children bends of prebend.
|
BendOperationBuilder.Types
unbend operations.
|
BendOperationCollection
Creates a
BendOperationBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.5.0 |
BlankGeneratorBuilder
Represents a
BlankGeneratorBuilder
This class is for Blank Generator Design UI
To create a new instance of this class, use BlankGeneratorCollection.createBlankGeneratorBuilder() Created in NX7.5.0 |
BlankGeneratorBuilder.CreateBlankType
Specify the creation method.
|
BlankGeneratorBuilder.EditBlankType
Specify the edit method.
|
BlankGeneratorBuilder.Types
Specifies the option of blank generator operation type.
|
BlankGeneratorCollection
Creates a
BlankGeneratorBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
BlankLayoutBuilder
Progressive Die Wizard blank layout builder
To create a new instance of this class, use BlankLayoutCollection.createBlankLayoutBuilder() Default values. |
BlankLayoutBuilder.LeftRightSideOption
Specifies the option of left right side type.
|
BlankLayoutBuilder.SideWebOption
Specifies the option of side webs type.
|
BlankLayoutBuilder.SnapSizeOption
Specifies the option of snap size.
|
BlankLayoutBuilder.Types
Specifies the option of blank layout type.
|
BlankLayoutCollection
Creates a
BlankLayoutBuilder To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
BlankNestingBuilder
Blank Nesting Builder of PDW, EDW and Die Engineering.
|
BlankNestingBuilder.LayoutTypeSpecification
Specifies the layout type of blank nesting.
|
BlankNestingCollection
Creates a
BlankNestingBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.5.0 |
BlendCurve3DBuilder
Represents a
BlendCurve3DBuilder builder which implements
blend curves in one side where the corner radius is too small. |
BlendCurve3DBuilder.BlendCurveOptions
The blend curve creation methods: Best Fit, Variable, Vector, Current View
|
BlendCurve3DBuilder.InputCurvesOption
The input curves option to keep, hide or delete input curves
|
BomBuilder
Represents a Tooling::BomBuilder builder
To create a new instance of this class, use BomCollection.createBomBuilder() Default values. |
BomBuilder.Circle
Represents an index to the base circle type of cylinder shape.
|
BomBuilder.Shape
Represents an index to the shape of stock size.
|
BomBuilder.TreeList
Represents an index to components list type.
|
BomCollection
Represents a collection of Bom
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
BomListBuilder
Represents a
BomListBuilder builder. |
BomListBuilder.BomListSortOption
Represents an enumeration indicating whether the sorting needs to be performed in ascending or descending order.
|
BomListBuilder.BomListTypes
Represents an index to components list type.
|
BomListDataProvider
Provides basic data for BOM List.
|
BomListDataProvider.ExportedStatus
Represents the exported status of a cell.
|
BurringInsertBuilder
Progressive Die Wizard builder to design burring punch and die insert
To create a new instance of this class, use BurringInsertCollection.createBurringInsertBuilder() Default values. |
BurringInsertBuilder.BurringDirections
Specifies the burring direction.
|
BurringInsertBuilder.BurringPunchTypes
Specifies the burring punch type.
|
BurringInsertBuilder.CircularOrNonCircularType
Specifies the circular or non-circular type.
|
BurringInsertBuilder.DesignOptions
Specifies the design type.
|
BurringInsertBuilder.ParentTypes
Specifies the parent part type.
|
BurringInsertCollection
Creates a
BurringInsertCollection To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
CalculateAreaBuilder
The CalculateArea builder
To create a new instance of this class, use CalculateAreaCollection.createBuilder() Default values. |
CalculateAreaBuilder.SheetMethodType
Represents the methods to create the projected sheet body.
|
CalculateAreaCollection
Represents a collection of CalculateArea builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
ChangeoverManagementBuilder
Represents a
ChangeoverManagementBuilder to support changeover workflow management. |
ChangeoverManagementBuilder.Types
Specifies the types of changeover management.
|
ChannelAdjustBuilder
The builder class for Channel Adjust which assists you
to adjust the postion and the length of the channel.
|
ChannelAdjustBuilder.AdjustType
the adjust method.
|
ChannelAdjustBuilder.VectorMethod
the vector adjust method.
|
ChannelAdjustCollection
Creates a ChannelAdjust Collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
ChannelFittingBuilder
The builder class for Channel Fitting which assists you
to add cooling fitting.
|
ChannelFittingCollection
Creates a ChannelFitting Collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
ClearanceManagementBuilder
Progressive Die Wizard builder to management clearances.
|
ClearanceManagementBuilder.Selection
Specifies clearance management part.
|
ClearanceManagementBuilder.Type
Specifies type to assign or check clearances
|
ClearanceManagementCollection
Creates a
ClearanceManagementCollection To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
CloneObject
Represents the clone operation in Add Reusable Component Builder.
|
ClonePart
Represents the part inforamtion to be cloned in Add Reusable Component Builder.
|
ColorExpressionsBuilder
Represents a
ColorExpressionsBuilder builder. |
CompDrawingBuilder
Represents a
CompDrawingBuilder which is
used to create or edit the Component Drawing. |
CompDrawingBuilder.ComponentTypeSelection
Specifies the type of components.
|
CompDrawingBuilder.DrawingType
Specifies the drawing type.
|
CompDrawingBuilder.FilterSelection
Specifies the filter of components.
|
CompDrawingBuilder.ProjectionType
Specifies the project type.
|
ConceptPositionBuilder
concept position builder for standard part design
To create a new instance of this class, use ConceptPositionCollection.createConceptPositionBuilder() Created in NX6.0.0 |
ConceptPositionCollection
Represents a collection of ConceptPosition
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
ConcurrentDesignManagementBuilder
Represents a
ConcurrentDesignManagementBuilder to support concurrent design workflow management. |
ConcurrentDesignManagementBuilder.Types
Specifies the types of concurrent design management.
|
ConcurrentDesignManagementBuilder.UpdateTypes
Specifies the types of the update action.
|
CoolingConnectBuilder
The builder class for Cooling connection which assists you
to create channel and connect it to other channels.
|
CoolingConnectCollection
Creates a CoolingConnect Collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
CoolingDefineChannelBuilder
The builder class for Cooling Define Channel which assists you
to create channels directly.
|
CoolingDefineChannelBuilder.ExtensionTypes
The extension types of channel
|
CoolingDefineChannelBuilder.TipEndTypes
The tip end types of channel
|
CoolingDefineChannelBuilder.Types
Types to specify how to assign attributes to the created body.
|
CoolingDefineChannelCollection
Creates a CoolingDefineChannel Collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
CoolingExtendBuilder
The builder class for Channel Extend which assists you
to extend the channel.
|
CoolingExtendBuilder.TipEndTypes
The tip end types of channel
|
CoolingExtendCollection
Creates a CoolingExtend Collection.
|
CoolingFittingData
Represents the cooling fitting data in Add Channel Fitting Builder.
|
CoolingPatternBuilder
The builder class for Cooling pattern which assists you
to create channels with selected curves.
|
CoolingPatternCollection
Creates a CoolingPattern Collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
CopySolidBuilder
Represents a
CopySolidBuilder builder. |
CornerDesignBuilder
Represents a
CornerDesignBuilder ,
Corner Design is to provide tools to make corner. |
CornerDesignBuilder.CornerTypeOpt
the corner types
|
CornerDesignBuilder.SelectFromOpt
the object selection options.
|
CornerDesignBuilder.Types
The corner design type.
|
CornerDesignCollection
Creates a
CornerDesignCollection To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
CostTableDataProvider
Provides basic data for cost feature table data.
|
CreateBoxBuilder
Represents a box creation operation
To create a new instance of this class, use CreateBoxCollection.createBoxBuilder(nxopen.NXObject) Default values. |
CreateBoxBuilder.BoxType
the type for creating box
|
CreateBoxCollection
Creates CreateBoxBuilder collection
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
DefineCamBuilder
Represents a
DefineCamBuilder to create different types of cam objects, which
are used for kinematic motion To create a new instance of this class, use ProgressiveDieManager.createDefineCamBuilder() Default values. |
DefineCamBuilder.PredefinedHydraulicOptions
Specifies the predefined hydraulic motion types
|
DefineCamBuilder.Types
Specifies the cam types
|
DefineLifterBuilder
Represents a
DefineLifterBuilder to create different types of lifter objects, which
are used for kinematic motion. |
DefineLifterBuilder.Types
Specifies the lifter types
|
DefineNeutralFactorBuilder
Represeents a
DefineNeutralFactorBuilder to define
neutral factor according to material and formula in the spreadsheet table. |
DefineNeutralFactorBuilder.FormulaOptions
Specifies the formula used to calculate the neutral factor value
|
DesignTrimToolBuilder
Represents a builder to be used to create Mold Wizard design trim tool.
|
DesignTrimToolCollection
Creates a DesignTrimToolCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
DieBaseBuilder
Represents Progressive Die Wizard and Engineering Die Wizard builder to manage die base.
|
DieBaseBuilder.AlongDirectionOpt
along direction options.
|
DieBaseBuilder.CatalogOpt
catalog options.
|
DieBaseBuilder.DesignToolOption
design tool options.
|
DieBaseBuilder.DieBaseTypeOpt
die bse types options.
|
DieBaseBuilder.ParentNodeOpt
parent node options.
|
DieBaseBuilder.PlatesNumberOpt
plates number options.
|
DieBaseBuilder.SplitMethod
split method.
|
DieBaseBuilder.SplitOption
split options.
|
DieBaseBuilder.Types
die base types.
|
DieBaseCollection
Creates a
DieBaseCollection To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
DieCavityAndSlugHoleBuilder
Represents die cavity and slug hole builder.
|
DieCavityAndSlugHoleBuilder.BottomPlateSlugItems
Specifies the type of bottom plate slug.
|
DieCavityAndSlugHoleBuilder.CavityTypeItems
Specifies the type of cavity.
|
DieCavityAndSlugHoleBuilder.ClearanceOptionItems
Specifies the design option of piercing insert.
|
DieCavityAndSlugHoleBuilder.DieInsertStackType
die insert stack type.
|
DieCavityAndSlugHoleBuilder.DiePlateThreeSlugType
die plate three slug type.
|
DieCavityAndSlugHoleBuilder.DiePlateTwoSlugType
die plate two slug type.
|
DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems
Specifies the type of die shoe slug.
|
DieCavityAndSlugHoleBuilder.InsertPositionItems
Specifies the position of piercing inserts, for EDW only
|
DieCavityAndSlugHoleBuilder.OffsetSideOptionItems
Specifies the offset side of normal pierce insert design.
|
DieDesDrawDieBuilder
Represents the Die Design draw die management builder, which is to create a draw die by selected
sheet body, curve and base plane.
|
DieDesDrawPunchBuilder
Die Design draw punch management builder, create a draw die punch by selected sheet body, curve
and base plane.
|
DieDesignLowerBinderBuilder
Represents a Lower Binder builder
To create a new instance of this class, use AutoDieCollection.createDieDesignLowerBinderBuilder(nxopen.features.Feature) Created in NX9.0.0 |
DieDesignSettingBuilder
Represents a
DieDesignSettingBuilder
This class is for Die Design Setting UI
To create a new instance of this class, use DieDesignSettingCollection.createDieDesignSettingBuilder() Default values. |
DieDesignSettingCollection
Creates a
DieDesignSettingBuilder . |
DieDesignTrimPostBuilder
Represents a Trim Post builder
To create a new instance of this class, use AutoDieCollection.createDieDesignTrimPostBuilder(nxopen.features.Feature) Created in NX9.0.0 |
DieDesPierceInsertBuilder
Represents Die Design Pierce Insert builder.
|
DieDesPierceInsertBuilder.Direction
Represents the thickness direction.
|
DieDesPierceInsertBuilder.HoleShapeTypes
Represents the hole shape type.
|
DieEngDefineProductOrientationBuilder
Die Engineer define product orientation builder.
|
DieEngDefineProductOrientationBuilder.FacetQualityOption
the facet quality option
|
DieEngDefineProductOrientationBuilder.OptimalMethod
the optimal method
|
DieEngDefineProductOrientationBuilder.ViewDraftOptions
view draft options
|
DieEngDieTipBuilder
Die Engineer die tip management builder.
|
DieEngDieTipBuilder.MaterialThicknessType
the material thickness type
|
DieEngFormTaskBuilder
Represents a Form Task builder
To create a new instance of this class, use AutoDieCollection.createDieEngFormTaskBuilder(nxopen.features.Feature) Default values. |
DieEngLineupBuilder
Die Engineer lineup management builder.
|
DieEngProcessUpdateManagerBuilder
Die Engineer process update manager management builder.
|
DieEngProcessUpdateManagerBuilder.Types
the trim task or pierce task.
|
DieEngStampingCarryoverBuilder
Represents a Stamping Carryover builder
To create a new instance of this class, use AutoDieCollection.createDieEngStampingCarryoverBuilder(nxopen.features.BodyFeature) Created in NX10.0.0 |
DieEngStampingOutputBuilder
Represents a Stamping Output builder
To create a new instance of this class, use AutoDieCollection.createDieEngStampingOutputBuilder(nxopen.features.BodyFeature) Default values. |
DieEngStampingOutputBuilder.DisplayProductType
Types of product display.
|
DieEngStampingOutputBuilder.SpringbackMethodType
Types of springback method
|
DieEngTrimAngleCheckBuilder
Represents a Trim Angle Check builder
To create a new instance of this class, use AutoDieCollection.createDieEngTrimAngleCheckBuilder(nxopen.geometricanalysis.AnalysisObject) Default values. |
DieEngTrimAngleCheckBuilder.DirectionOptions
Options to determine the method to specify direction.
|
DieEngTrimTaskBuilder
Die Engineer trim task management builder, create a trim task by selected die tip, trim bounds,
start plane and end plane.
|
DieEngTrimTaskBuilder.TrimTaskCamType
the trim task cam type.
|
DieEngTrimTaskBuilder.TrimTaskMatchCutType
the trim task match cut type.
|
DieInsertBuilder
Represents die insert builder.
|
DieInsertBuilder.BoundingBoxTypeItems
Specifies the bounding box type.
|
DieInsertBuilder.DieInsertTypeItems
Specifies the type of insert.
|
DieInsertBuilder.InsertModeItems
Specifies the insert mode for die.
|
DieInsertBuilder.PositionItems
Specifies the position of piercing inserts, for EDW only
|
DirectUnbendBuilder
The builder contains all inputs for direct unbend.
|
DirectUnbendBuilder.Bendtypes
unbend operations.
|
DirectUnfoldBuilder
The builder contains all inputs for direct unfolding.
|
DirectUnfoldBuilder.Bend
The number of children bends in defining prebend.
|
DirectUnfoldBuilder.BodyList
The name list of bodies in current part.
|
DirectUnfoldBuilder.MatType
The material database defined in PDW.
|
DirectUnfoldBuilder.Types
Specifies the option of direct unfold type
|
DirectUnfoldCollection
Creates a
DirectUnfoldBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
DrawingSheetNameBuilder
Represents a
DrawingSheetNameBuilder To create a new instance of this class, use ToolingDrawingCollection.createDrawingSheetNameBuilder() Created in NX8.5.0 |
EdgePatchBuilder
Represents a builder to be used to create edge patch surfaces.
|
EdgePatchBuilder.BodyColorData
This class holds the data returned from
EdgePatchBuilder.getBodyColor() |
EdgePatchBuilder.PatchStatus
Settings of the patch status types.
|
EdgePatchBuilder.SelectTypes
Settings of the selection types.
|
EdgePatchCollection
Represents a collection of EdgePatch builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
EjectorPostProcessingBuilder
Represents a builder to be used to create Mold Wizard ejector post processing.
|
EjectorPostProcessingBuilder.TrimMethod
The processing type: Trim, Adjust length and Untrim.
|
EjectorPostProcessingBuilder.TrimPartName
The trim part where to find a trim surface as tool to trim ejector pins.
|
EjectorPostProcessingBuilder.TrimSufaceName
The trim surface types.
|
EjectorPostProcessingCollection
Creates a EjectorPostProcessingCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
EjectorTableBuilder
Represens a ejector table builder.
|
EjectorTableBuilder.DrawingType
The types of the ejector drawing.
|
EjectorTableBuilder.EjectorType
The types of ejectors.
|
EjectorTableData
Represents the ejector table data in Ejector Table Builder.
|
ElectrodeBlankBuilder
Design electrode blank builder to create an electrode blank for the selected body.
|
ElectrodeBlankBuilder.BlankMaterial
Represents the blank material option.
|
ElectrodeBlankBuilder.BlankShape
Represents the electrode blank shape option.
|
ElectrodeBlankBuilder.JointObject
Represents the transition type between head bodies and the blank.
|
ElectrodeCheckingBuilder
Electrode Checking builder to check the touch status of all electrode.
|
ElectrodeComponentBuilder
Electrode component builder to install holder and pallet.
|
ElectrodeComponentBuilder.Chuck
Represents the electrode chuck type.
|
ElectrodeCopyBuilder
The ElectrodeCopy builder
To create a new instance of this class, use ElectrodeCopyCollection.createElectrodeCopyBuilder() Default values. |
ElectrodeCopyBuilder.Copy
Represents an index to copy type
|
ElectrodeCopyBuilder.UpdateParameterData
This class holds the data returned from
ElectrodeCopyBuilder.updateParameterData(nxopen.TaggedObject, nxopen.TaggedObject) |
ElectrodeCopyCollection
Represents a collection of ElectrodeCopy builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
ElectrodeDeleteBuilder
Electrode delete component builder to remove blank, pallet and holder from assembly.
|
ElectrodeDeleteBuilder.Types
delete sparking solid from blank or delete blank, pallet or holder directly.
|
ElectrodeDesignCollection
Represents a collection of Electrode Design.
|
ElectrodeInitializationBuilder
Electrode initialize project builder to creates an electrode design assembly.
|
ElectrodeInitializationBuilder.Method
The initialize type: Original, No Working Part, No Machine Set Part and No Template.
|
ElectrodeInitializationBuilder.Type
Clone a member of an electrode assembly, such as top part, machine set part, and working part.
|
EnlargeSurfaceBuilder
Mold Wizard enlarge surface management builder, trims a enlarged surface to a boundary of edges,
curves, datum planes or faces.
|
EnlargeSurfaceBuilder.ColorValueData
This class holds the data returned from
EnlargeSurfaceBuilder.getColorValue() |
EnlargeSurfaceBuilder.KeepDiscardOption
represents the keep discard options for selected region.
|
EnlargeSurfaceCollection
Represents a collection of Enlarge Surface
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
EWDraftingBuilder
Represents the drafting builder which is used to create electrode drafting.
|
EWDraftingBuilder.CNCTemplateOption
the template option of cnc sheet type
|
EWDraftingBuilder.DrawingOption
the drawing type
|
EWDraftingBuilder.EDMTemplateOption
the template option of edm sheet type
|
EWDraftingBuilder.ModeOption
the drafting mode option
|
EWDraftingBuilder.NameOption
the drawing sheet name option
|
EWMultiPositionBuilder
Represents the multiple position builder which is used to get transformed electrode heads together.
|
EWMultiPositionCollection
Creates EWMultiPosition builder collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
FaceAttributeBuilder
Represents a builder to be used to create face attribute.
|
FaceColorManagementBuilder
Tooling builder to assign and edit color of objects
To create a new instance of this class, use FaceColorManagementCollection.createFaceColorManagementBuilder() Default values. |
FaceColorManagementBuilder.HoleTypeEnumValue
the hole type enumeration
|
FaceColorManagementCollection
Creates a
FaceColorManagementBuilder To obtain an instance of this class, refer to ToolingManager Created in NX9.0.0 |
FaceSplitBuilder
Represents a face split operation
To create a new instance of this class, use FaceSplitCollection.createFaceSplitBuilder() Default values. |
FaceSplitBuilder.FaceSplitType
the type for Split Face
|
FaceSplitCollection
Creates Face Split collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
FamilyMoldBuilder
Creates a Mold Wizard Family Mold builder
To create a new instance of this class, use FamilyMoldCollection.createFamilyMoldBuilder() Created in NX6.0.0 |
FamilyMoldCollection
Creates a
FamilyMoldCollection To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
FastenerAssemConfigBuilder
Represents a Fastener Assem Config Collection.
|
FastenerAssemConfigCollection
Represents a collection of FastenerAssy
To obtain an instance of this class, refer to ToolingManager Created in NX5.0.0 |
FastenerAssy
Represents a
FastenerAssy
To create a new instance of this class, use FastenerAssyCollection.createBuilder() Default values. |
FastenerAssy.HoleOperation
Represents the action on the hole menu of the fastener assembly.
|
FastenerAssy.ModeMethod
Represents adding and editing modes for the fastener assembly
|
FastenerAssy.SelectionObjectMethod
Represents selection object type
|
FastenerAssy.SelectionTypeMethod
Represents selection type for position and hole
|
FastenerAssy.StackTypeMethod
Represents screw_array type
|
FastenerAssyCollection
Represents a collection of FastenerAssy
To obtain an instance of this class, refer to ToolingManager Created in NX5.0.0 |
FastenerAssyCustomizationBuilder
Fastener assembly customization builder.
|
FastenerAssyCustomizationCollection
Represents a collection of FastenerAssyCustomizationBuilder
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
FastenerRemoveNodeBuilder
Fastener remove node builder.
|
FastenerRemoveNodeCollection
Represents a collection of FastenerRemoveNodeBuilder
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
FeatureReferenceSetBuilder
Represents a
FeatureReferenceSetBuilder builder. |
FlowAnalysisBuilder
Represents the builder which is used to create flow analysis.
|
FlowDisplayBuilder
Represents the builder which is used to create flow analysis.
|
FlowDisplayBuilder.AnalysisResults
The option of analysis results.
|
ForceCalculationBuilder
Represents a
ForceCalculationBuilder
Force Calculation Design is to calculate force of process
To create a new instance of this class, use ForceCalculationCollection.createForceCalculationBuilder() Default values. |
ForceCalculationBuilder.CalculationTypes
The calculation type.
|
ForceCalculationBuilder.ProcessTypes
The process type.
|
ForceCalculationCollection
Creates a
ForceCalculationBuilder To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
FormingInsertBuilder
Progressive Die Wizard builder to design forming punch and die insert
To create a new instance of this class, use FormingInsertCollection.createFormingInsertBuilder() Default values. |
FormingInsertBuilder.BlankPositions
Specifies the blank position.
|
FormingInsertBuilder.BlankTypes
Specifies the blank type.
|
FormingInsertBuilder.DesignOptions
Specifies the design type.
|
FormingInsertBuilder.ParentTypes
Specifies the parent part type.
|
FormingInsertCollection
Creates a
FormingInsertBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
GeneralInsertBuilder
General Insert Design Builder of PDW and EDW.
|
GeneralInsertBuilder.GenerateMethod
Specify the creation method of insert.
|
GeneralInsertBuilder.ParentOption
Specify the part parent of insert part.
|
GeneralInsertBuilder.Types
Specify the insert operation type.
|
GuidedExtensionBuilder
Builder for creating Guided Extension surface in NX
To create a new instance of this class, use GuidedExtensionManager.createBuilder() Default values. |
GuidedExtensionBuilder.SegmentType
Segment type for segments
|
GuidedExtensionManager
Represents the manager of the GuidedExtension builder
To obtain an instance of this class, refer to ToolingManager |
HemFixerBuilder
Hem Fixer Builder of PDW and EDW.
|
HoleDatumSymbolBuilder
Creates hole datum symbol builder for progressive die.
|
HoleDatumSymbolBuilder.SymbolType
symbol type
|
HoleManufacturingNoteBuilder
Tooling builder for HoleManufacturingNote
To create a new instance of this class, use HoleManufacturingNoteCollection.createHoleManufacturingNoteBuilder() Default values. |
HoleManufacturingNoteBuilder.DefineByViewOrHoles
the view selection or window selection type
|
HoleManufacturingNoteBuilder.HoleIndexType
the hole index type
|
HoleManufacturingNoteCollection
Creates a
HoleManufacturingNoteBuilder To obtain an instance of this class, refer to ToolingManager Created in NX9.0.0 |
HoleReportBuilder
Represents a
HoleReportBuilder
This class is for Hole Report Design UI
To create a new instance of this class, use HoleReportCollection.createHoleReportBuilder() Default values. |
HoleReportBuilder.EnumQuadrantType
Specifies the option of which quadrant is positive
|
HoleReportBuilder.EnumSelectionType
Specifies the option of selection type to create hole table
|
HoleReportBuilder.Types
Specifies the option of hole table type
|
HoleReportCollection
Creates a
HoleReportBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
InitProjBuilder
Represents a
InitProjBuilder
To create a new instance of this class, use InitProjCollection.createInitProjBuilder() Default values. |
InitProjBuilder.ProjTempOption
Represents the project template option of InitProj,
defines the pre-defined project template. this template will be used as the basic assembly structure for this new project
|
InitProjCollection
Represents a collection of InitProj
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
InitProjectBuilder
Mold Wizard initialize project builder
To create a new instance of this class, use InitProjectCollection.createBuilder() Default values. |
InitProjectBuilder.ConfigurationId
the configuration type includes default and orig
|
InitProjectBuilder.MaterialId
the material type includes None and Nylon
|
InitProjectBuilder.UnitId
the unit type includes metric and inch project type
|
InitProjectCollection
Represents a collection of InitProject builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
InsertAuxiliaryBuilder
PDW insert auxiliary builder to design various auxiliaries of insert group
To create a new instance of this class, use InsertAuxiliaryCollection.createInsertAuxiliaryBuilder() Default values. |
InsertAuxiliaryBuilder.CircOperationTypes
Specifies the options of circular array.
|
InsertAuxiliaryBuilder.DesignToolOption
Specifies the design tool option.
|
InsertAuxiliaryBuilder.RampStepsType
Specifies the ramp steps.
|
InsertAuxiliaryBuilder.RectOperationOption
Specifies the rectangular array option.
|
InsertAuxiliaryBuilder.ShankShapeTypes
Specifies the shank shape.
|
InsertAuxiliaryBuilder.Types
Specifies the insert auxiliary type.
|
InsertAuxiliaryBuilder.UseFaceOrSketchToRevolve
Specifies the use face or sketch to revolve.
|
InsertAuxiliaryCollection
Creates a
InsertAuxiliaryBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
InsertEditToolsBuilder
Represents a
InsertEditToolsBuilder which is
used to copy or delete the insert edit. |
InsertEditToolsBuilder.Types
Specifies the insert edit tools type.
|
IntermediateStageBuilder
Represents a
IntermediateStageBuilder builder. |
IntermediateStageBuilder.DesignSequences
The types of design sequences
|
IntermediateStageBuilder.EditOptions
The types of changed intermediate stages
|
IntermediateStageBuilder.Orientations
The types of orientation of intermediate stages
|
IntermediateStageCollection
Creates a
IntermediateStageBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.5.0 |
LayoutBuilder
Represents a Tooling::LayoutBuilder builder
To create a new instance of this class, use MWLayoutCollection.createLayoutBuilder() Default values. |
LayoutBuilder.BalNumber
Represents the number of balance cavity.
|
LayoutBuilder.LayoutSubType
Represents the the sub type of layout.
|
LayoutBuilder.LayoutType
Represents the type of layout.
|
LayoutBuilder.XrefNum
Represents the type of x move refer.
|
LayoutBuilder.YrefNum
Represents the type of y move refer.
|
LayoutManagementBuilder
Layout Management Builder of Engineering Die Wizard
To create a new instance of this class, use LayoutManagementCollection.createLayoutManagementBuilder() Default values. |
LayoutManagementBuilder.StationItems
Specifies the station items
|
LayoutManagementCollection
Creates a
LayoutManagementBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
LayoutRepositionBuilder
Represents a Tooling::LayoutRepositionBuilder builder
To create a new instance of this class, use MWLayoutCollection.createLayoutRepositionBuilder() Default values. |
LayoutRepositionBuilder.Method
Represents the type of layout transform.
|
LayoutRepositionBuilder.Type
Represents the method of layout transform.
|
LsdynaFormAnalysisResultDisplayBuilder
Represents a Ly-Dyna Formability Analysis - Result Display builder
To create a new instance of this class, use AutoDieCollection.createLsdynaFormAnalysisResultDisplayBuilder() Default values. |
LsdynaFormAnalysisResultDisplayBuilder.FormabilityStrainTypeName
Options to set strain type to display for formability analysis result.
|
LsdynaFormAnalysisResultDisplayBuilder.StrainTypeName
Options to set strain type to display for strain analysis result.
|
LsdynaFormAnalysisResultDisplayBuilder.StressTypeName
Options to set stress type to display for stress analysis result.
|
LsdynaGeometryPreparationBuilder
Stamping Die LS-Dyna integration draw geometry preprare builder.
|
LsdynaGeometryPreparationBuilder.BlankOption
the enum of blank option.
|
LsdynaGeometryPreparationBuilder.BlankPosition
the enum of blank position.
|
LsdynaGeometryPreparationBuilder.ContactType
the enum of contact type.
|
LsdynaGeometryPreparationBuilder.DrawBeadType
the enum of draw bead type.
|
LsdynaGeometryPreparationBuilder.DrawType
the enum of draw type.
|
LsdynaGeometryPreparationBuilder.MaterialType
the enum of material type.
|
LsdynaGeometryPreparationBuilder.ProcessActionBinder
the enum of process action binder type.
|
LsdynaGeometryPreparationBuilder.ProcessActionDie
the enum of process action die type.
|
LsdynaGeometryPreparationBuilder.ProcessActionPunch
the enum of process action punch type.
|
LsdynaGeometryPreparationBuilder.ProcessType
the enum of process type.
|
LsdynaGeometryPreparationBuilder.TargetBinder
the enum of target binder type.
|
LsdynaGeometryPreparationBuilder.TargetDie
the enum of target die type.
|
LsdynaGeometryPreparationBuilder.TargetPunch
the enum of target punch type.
|
LsdynaKfileGeneratorBuilder
Represents LS-Dyna K file builder - K file generator builder
To create a new instance of this class, use AutoDieCollection.createLsdynaKfileGeneratorBuilder() Default values. |
LsdynaKfileGeneratorBuilder.MeshDataType
Types of data format.
|
LsdynaKfileGeneratorBuilder.MeshElementType
Types of mesh element type.
|
LsdynaKfileGeneratorBuilder.OperTypes
Types of operation.
|
ManufacturingGeometryBuilder
Represents a builder to be used to create manufacturing geometry.
|
ManufacturingGeometryCollection
Represents a collection of Manufacturing Geometry builder.
|
MoldCsysBuilder
Mold Wizard MoldCsys project builder
To create a new instance of this class, use MoldCsysCollection.createMoldCsysBuilder() Default values. |
MoldCsysBuilder.Wcsposition
Represents the method to computer the WCS positino
|
MoldCsysCollection
Creates a
MoldCsysCollection To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MoldDesignCollection
Represents a collection of Mold Design.
|
MoldFeatureRecognitionBuilder
Represents a
MoldFeatureRecognitionBuilder builder To create a new instance of this class, use MoldwizardManager.createMoldFeatureRecognitionBuilder() Default values. |
MoldFillingBuilder
Builder used to add a gate/runner standard part from fill library, it returns null.
|
MoldFillingBuilder.InstallOption
The installation type of the fill component.
|
MoldFillingBuilder.MoveOption
The modification options of the selected fill component.
|
MoldInsertBuilder
Mold Wizard mold insert management builder
To create a new instance of this class, use MoldInsertCollection.createMoldInsertBuilder() Default values. |
MoldInsertBuilder.BooleanType
design type: unite single workpieces, subtract overall workpieces
|
MoldInsertCollection
Creates a MoldInsertCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MoldProcessBuilder
Represents a Tooling::MoldProcessBuilder builder
To create a new instance of this class, use MoldProcessCollection.createMoldProcessBuilder() Default values. |
MoldProcessCollection
Represents a collection of Mold Process
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MoldwizardManager
Provides create builder methods for Moldwizard.
|
MotionSimulationBuilder
Represents a
MotionSimulationBuilder to support dynamic interference check. |
MotionSimulationBuilder.CamDefinitionType
Specifies the way to define cam, automatically or manually.
|
MotionSimulationBuilder.EjectorMoveOptions
Specifies the ejector move type, after or while
|
MotionSimulationBuilder.MoldbaseStyleType
Specifies the style type of moldbase, two-plate style or three-plate style
|
MotionSimulationBuilder.Types
Specifies the operation options of motion simulation.
|
MotionSimulationCollection
Represents a collection of MotionSimulation.
|
MWCopySheetsBuilder
Builder for copying sheets in the Mold Wizard application
To create a new instance of this class, use MWCopySheetsCollection.createBuilder() Default values. |
MWCopySheetsBuilder.Types
This enum represents the type of sheets to be copied
|
MWCopySheetsCollection
Represents a collection of MWCopySheets builder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
MWDefineRegionsBuilder
The MWDefineRegions builder
To create a new instance of this class, use MWDefineRegionsCollection.createBuilder() Default values. |
MWDefineRegionsBuilder.OrCreateEmptyRegionData
This class holds the data returned from
MWDefineRegionsBuilder.getOrCreateEmptyRegion() |
MWDefineRegionsBuilder.TranslucencyOptionType
This enum represents the translucency is to be performed on the selected or non-selected region faces
|
MWDefineRegionsCollection
Represents a collection of MWDefineRegions builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MWDefineSheetsBuilder
Builder for defining sheets in Mold Wizard
To create a new instance of this class, use MWDefineSheetsCollection.createBuilder() Default values. |
MWDefineSheetsBuilder.DefineStepType
The define steps for defining Cavity and Core using the Split Body method.
|
MWDefineSheetsBuilder.Types
The types for defining Cavity and Core.
|
MWDefineSheetsCollection
Represents a collection of MWDefineSheets builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MWDesignGuideLinesBuilder
The builder for designing guide lines in Mold Wizard.
|
MWDesignGuideLinesBuilder.CreateGuideLineData
This class holds the data returned from
MWDesignGuideLinesBuilder.createGuideLine(nxopen.Curve, nxopen.Point3d, double) |
MWDesignGuideLinesBuilder.DirectionType
The type of direction for the guide line to be created.
|
MWDesignGuideLinesCollection
Represents a collection of MWDesignGuideLines builder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
MWDesignPartingSurfaceBuilder
The builder for designing parting surface in Mold Wizard.
|
MWDesignPartingSurfaceBuilder.ObjectType
The type of parting objects to be edited or placed.
|
MWDesignPartingSurfaceBuilder.PartingSurfaceType
The type of parting surface to be created.
|
MWDesignPartingSurfaceBuilder.TransitionSurfaceType
The type of transition surface to be created.
|
MWDesignPartingSurfaceBuilder.TrimAndExtendFromRegionType
The region type from which to trim and extend when creating parting surface.
|
MWDesignPartingSurfaceCollection
Represents a collection of MWDesignPartingSurface builder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
MWLayoutCollection
Creates Mold Wizard layout collection
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MWMoldedPartValidationBuilder
Represents a builder to be used to perform Molded Part Validation analysis.
|
MWMoldedPartValidationBuilder.AssignToRegion
Options for assigning faces to the Cavity or Core region
|
MWMoldedPartValidationBuilder.CalculateOption
Calculation options
|
MWMoldedPartValidationBuilder.CheckScope
Check scope for information
|
MWMoldedPartValidationBuilder.RangeType
Range type for displaying small corner radius faces
|
MWMoldedPartValidationManager
Represents a manager of the MWMoldedPartValidation builder
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
MWPartingManagerBuilder
Builder for the Parting Manager in the Mold Wizard application
To create a new instance of this class, use MWPartingManagerCollection.createBuilder() Created in NX7.5.0 |
MWPartingManagerBuilder.DataStatus
The status of the parting manager data.
|
MWPartingManagerBuilder.RegisterType
The type of registering UNDO identifier.
|
MWPartingManagerCollection
Represents a collection of MWPartingManager builder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
MWSearchRegionBuilder
The Search Region builder is for defining a region by searching the region faces given a set of seed faces and boundary edges.
|
MWSearchRegionCollection
Represents a collection of MWSearchRegion builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MWTraversePartingLinesBuilder
Builder for creating parting lines by traversing in the Mold Wizard application
To create a new instance of this class, use MWTraversePartingLinesCollection.createBuilder() Created in NX7.5.0 |
MWTraversePartingLinesCollection
Represents a collection of the MWTraversePartingLines builder
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
ObjectAttributeManagementBuilder
Tooling builder to assign and edit attributes of objects
To create a new instance of this class, use ObjectAttributeManagementCollection.createObjectAttributeManagementBuilder() Default values. |
ObjectAttributeManagementBuilder.FilterAccordingToAttributeType
the selection filter type according to attribute
|
ObjectAttributeManagementBuilder.FilterType
the selection filter type
|
ObjectAttributeManagementBuilder.ShowComponentsType
the show type according to attribute
|
ObjectAttributeManagementBuilder.ShowType
show attributes of selected objects or show objects according to attribute
|
ObjectAttributeManagementCollection
Creates a
ObjectAttributeManagementBuilder To obtain an instance of this class, refer to ToolingManager Created in NX9.0.0 |
OffsetCurve3DBuilder
Deprecated.
Deprecated in NX10.0.0. Please use
Offset3DCurveBuilder instead
|
PiercingInsertBuilder
Represents piercing insert builder.
|
PiercingInsertBuilder.AssociationToolType
Specifies the association tool operation option.
|
PiercingInsertBuilder.DieInsertTypeItems
Specifies the type of insert.
|
PiercingInsertBuilder.InsertPosition
Specifies the position of piercing inserts, for EDW only
|
PiercingInsertBuilder.NormalBbpslugType
Specifies the type of bottom plate slug.
|
PiercingInsertBuilder.NormalCavityType
Specifies the type of cavity.
|
PiercingInsertBuilder.NormalClearanceOptionType
Specifies the design option of piercing insert.
|
PiercingInsertBuilder.NormalDsslugType
Specifies the type of die shoe slug.
|
PiercingInsertBuilder.NormalOffsetSideType
Specifies the offset side of normal pierce insert design.
|
PiercingInsertBuilder.NormalUdpparentPartType
Specifies the parent part of user defined punch.
|
PiercingInsertBuilder.PunchPocketTypeItemsBP
Specifies the punch pocket type in backing plate.
|
PiercingInsertBuilder.PunchPocketTypeItemsPP
Specifies the punch pocket type in punch plate.
|
PiercingInsertBuilder.PunchPocketTypeItemsSP
Specifies the punch pocket type in stripper plate.
|
PiercingInsertBuilder.Types
Specifies the option of piercing insert type.
|
PiercingInsertCollection
Creates a
PiercingInsertBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
PiercingInsertMiniToolsBuilder
Represents piercing insert mini tools builder.
|
PiercingInsertMiniToolsBuilder.AssociationToolItems
Specifies the association tool operation option.
|
PocketBuilder
Mold Wizard pocket management builder
To create a new instance of this class, use PocketCollection.createPocketBuilder() Default values. |
PocketBuilder.ModeType
Represents the pocket operation method
|
PocketBuilder.RsetType
Represents the pocket refset types
|
PocketBuilder.ToolType
Represents the select type of tool
|
PocketCollection
Creates a
PocketBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
PrebendBuilder.NumberBendsOption
The option of bend number to divide into
|
ProfileSplitBuilder
The ProfileSplit builder
To create a new instance of this class, use ProfileSplitCollection.createProfileSplitBuilder() Created in NX6.0.0 |
ProfileSplitCollection
Represents a collection of ProfileSplit builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
ProgressiveDieManager
Provides create builder methods for Progressive Die.
|
PunchInsertBuilder
Represents punch insert builder.
|
PunchInsertBuilder.InsertPositionItems
Specifies the position of piercing inserts, for EDW only
|
PunchInsertBuilder.NormalClearanceOptionTypeItems
Specifies the design option of piercing insert.
|
PunchInsertBuilder.NormalOffsetSideTypeItems
Specifies the offset side of normal pierce insert design.
|
PunchInsertBuilder.PunchPocketTypeItemsBackingPlate
Specifies the punch pocket type in backing plate.
|
PunchInsertBuilder.PunchPocketTypeItemsPunchPlate
Specifies the punch pocket type in punch plate.
|
PunchInsertBuilder.PunchPocketTypeItemsStripperPlate
Specifies the punch pocket type in stripper plate.
|
QuickDatumCsysBuilder
Represents a
QuickDatumCsysBuilder builder. |
QuickDatumCsysBuilder.AlignVectors
Represents an index to components list type.
|
QuickQuotationBuilder
Progressive Die Wizard builder to create quick quotation.
|
QuickQuotationBuilder.DesignTypes
Specify the design type.
|
QuickQuotationBuilder.InsertGroupMaterials
Specify the insert group material.
|
QuickQuotationBuilder.ManageTemporaryObjectsTypes
Specify the management type for the temporary objects.
|
QuickQuotationBuilder.ObjectTypes
Specify the concept sheet body type.
|
QuickQuotationBuilder.Types
Specify the operation type.
|
QuickQuotationCollection
Creates a
QuickQuotationBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
ReferenceBlendBuilder
The ReferenceBlend builder
To create a new instance of this class, use ReferenceBlendCollection.createReferenceBlendBuilder() Created in NX7.0.0 |
ReferenceBlendCollection
Creates reference blend collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
ReliefDesignBuilder
Represents a
ReliefDesignBuilder
Relief Design is to cut relief pocket for forming region . |
ReliefDesignBuilder.Method
The relief design creation method.
|
ReliefDesignBuilder.MethodOfDelete
The relief design delete method.
|
ReliefDesignBuilder.Types
The relief design type.
|
ReliefDesignCollection
Creates a
ReliefDesignBuilder To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
RemoveHolesBuilder
Remove Hole is used to patch holes for a solid body.
|
RemoveHolesBuilder.SelectionTypes
select object types, body or face
|
RenameAndExportComponentBuilder
Creates rename and export component builder for progressive die.
|
RenameAndExportComponentBuilder.DefinitionType
definition type
|
RenameAndExportComponentBuilder.LoadOptionType
load option type
|
RenameAndExportComponentBuilder.NameRuleType
tooling naming rule
|
RenameAndExportComponentBuilder.NamingRuleType
naming rule
|
RenameAndExportComponentBuilder.Types
types
|
ReplaceSolidBuilder
Represents a replace solid operation.
|
ReplaceSolidCollection
Creates ReplaceSolidBuilder collection
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
ReusableObject
Represents a
ReusableObject
To create a new instance of this class, use ToolingManager.createReusableObject() Created in NX7.5.2 |
ReusableObjectManager
Represents a collection of ReusableObjects
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
ReusableObjectPasteBuilder
Represents a
ReusableObjectPasteBuilder Use the ReusableObjectManager class to create a ReusableObjectPasteBuilder. |
ReusableObjectPasteBuilder.PasteMethods
Specifies the design option
|
ReusablePocketBuilder
Reusable pocket builder.
|
ReusablePocketBuilder.Hole
Represents hole types.
|
ReusablePocketCollection
Represents a collection of ReusablePocketBuilder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
ReusePositioningObjectBuilder
Represents a
ReusePositioningObjectBuilder Use the ReusableObjectManager class to create a ReusePositioningObjectBuilder. |
ReusePositioningObjectBuilder.CurveExtendToFace
extend to face edges type enum.
|
ReusePositioningObjectBuilder.CurveTrim
trim to each other within section type enum.
|
ReusePositioningObjectBuilder.DialogOptions
the dialog layout options
|
ReusePositioningObjectBuilder.NonStandardPointsData
This class holds the data returned from
ReusePositioningObjectBuilder.getNonStandardPoints() |
ReusePositioningObjectBuilder.SubTypes
the positioning sub types
|
ReusePositioningObjectBuilder.Types
the positioning types
|
RunnerBuilder
Mold Wizard runner management builder, select curves as runner guide, choose section type and edit
section parameters, optional choose boolean type to create runner channel.
|
RunnerBuilder.GuideEndType
Represents the runner guide end type.
|
RunnerBuilder.SectionType
Represents the section type of runner channel.
|
RunnerCollection
Represents a collection of Runner
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
RunSimulationBuilder
Represents a
RunSimulationBuilder to animate the model,
analyze the collision and reference. null is returned To create a new instance of this class, use ProgressiveDieManager.createRunSimulationBuilder() Default values. |
RunSimulationBuilder.CollisionCheckOptions
Specifies the collision check method
|
ScrapDesignBuilder
Represents a scrap design builder
To create a new instance of this class, use ScrapDesignCollection.createScrapDesignBuilder() Default values. |
ScrapDesignBuilder.AddonType
Specifies the add-on type
|
ScrapDesignBuilder.Body
Specifies the operation type of scraps
|
ScrapDesignBuilder.DefScrapType
Specifies the definition type of scraps
|
ScrapDesignBuilder.EditScrapType
Specifies the edit type of scraps
|
ScrapDesignBuilder.OvercutType
Specifies the over cut type, different type has different parameters
|
ScrapDesignBuilder.RemoveType
Specifies the removing type as filter
|
ScrapDesignBuilder.ScrapDefPosition
Specifies the position method of scraps, projecting method is normally used
|
ScrapDesignBuilder.ScrapDefType
Specifies the creation type of scraps
|
ScrapDesignBuilder.TrimNumType
Specifies the step of trimming process, the maximum is five
|
ScrapDesignCollection
Represents a collection of ScrapDesign
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
SectionLineCreationBuilder
Represents a
SectionLineCreationBuilder which is
used to create or edit the section line creation. |
SelectReuseLibraryItemBuilder
Select a part from the reuse library .
|
SelectReuseLibraryListItemBuilder
Select reuse library list item .
|
SelectReuseLibraryListItemBuilderList
Represents a list of objects.
|
SetPressModelBuilder
Represents a
SetPressModelBuilder to set and load the press model. |
SheetMetalFeatureRecognitionBuilder
Represents a
SheetMetalFeatureRecognitionBuilder builder To create a new instance of this class, use MoldwizardManager.createSheetMetalFeatureRecognitionBuilder() Created in NX11.0.1 |
ShimBuilder
Shim Builder of PDW and EDW.
|
ShimBuilder.ParentOption
Specify the parent node.
|
ShimBuilder.SideAttributeValues
Specifies the value of side attribute.
|
ShimBuilder.Types
Specify the shim operation type.
|
ShimInnerProfileSetBuilder
This is a seed block of set list.
|
ShimInnerProfileSetBuilderList
Represents a list of objects.
|
SIZERCollection
Represents a collection of SIZER
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
SIZERExportBuilder
Exports input parameters for motor selection to SIZER drive design to
support the sizing, configuration, and selection of drive components.
|
SIZERExportBuilder.MCDMechanicalData
Defines the mechanical data in MCD mode.
|
SIZERExportBuilder.MechanicalData
Defines the mechanical data in Motion mode.
|
SIZERExportBuilder.RunMode
Represents the run mode.
|
SIZERImportBuilder
Imports results for motor selection from SIZER drive design based on
the sizing, configuration, and selection of drive components.
|
SIZERImportBuilder.PositionMode
Represents the position mode.
|
SlugRetentionBuilder
Represents a
SlugRetentionBuilder which is used to create the Slug Retention. |
SlugRetentionBuilder.Types
the main type
|
SmartScrewUpdateBuilder
Smart Screw Update of MW, PDW and EDW.
|
SmartScrewUpdateBuilder.ParentOption
Specify the parent node.
|
SmartScrewUpdateBuilder.Types
Specify the operation type.
|
SolidPatchBuilder
Represents a builder to be used to create a solid patch.
|
SolidPatchBuilder.SolidPatchType
Settings of the solid patch creation types.
|
SolidPatchCollection
Represents a collection of SolidPatch builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
SpecialFormingBuilder
Creates special forming insert builder for progressive die.
|
SpecialFormingBuilder.BlockType
the block type
|
SpecialFormingBuilder.ParentValue
Specifies the main page type.
|
SpecialFormingBuilder.PunchOrDie
Specifies the main page type.
|
SpecialFormingBuilder.Types
Specifies the main page type.
|
SpecialPiercingInsertBuilder
Creates special piercing insert for progressive die.No entity is returned.
|
SpecialPiercingInsertBuilder.BoundBoxType
Specifies the bounded box type block or cylinder.
|
SpecialPiercingInsertBuilder.InsertPositionTypes
Specifies the position of piercing inserts, for EDW only
|
SpecialPiercingInsertBuilder.NormalBottomBackingPlateSlugType
Specifies the type of bottom plate slug.
|
SpecialPiercingInsertBuilder.NormalCavityType
Specifies the type of cavity.
|
SpecialPiercingInsertBuilder.NormalDieShoeSlugType
Specifies the type of die shoe slug.
|
SpecialPiercingInsertBuilder.NormalOffsetSideType
Specifies the offset side of normal pierce insert design.
|
SpecialPiercingInsertBuilder.ParentPartTypes
Specifies the parent part type.
|
SpecialPiercingInsertBuilder.PunchOrDieTypes
Specifies the parent part type.
|
SpecialPiercingInsertBuilder.StandardOrUserDefinedTypes
Specifies the parent part type.
|
SpecialPiercingInsertBuilder.Types
Specifies the parent part type.
|
SpecifyBaffleBuilder
Represents a builder to be used to create specify baffle.
|
SpecifyBaffleBuilder.AttributeTypes
Types to specify how to assign attributes to the selected body.
|
SpecifyBaffleBuilder.ChannelColorData
This class holds the data returned from
SpecifyBaffleBuilder.getChannelColor() |
SpecifyBaffleCollection
Represents a collection of Specify Baffle builder
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
SpecifyCircuitBuilder
Represents a builder to be used to create specify circuit.
|
SpecifyCircuitCollection
Represents a collection of Specify Circuit builder
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
SpindleSliderBuilder
Represents a
SpindleSliderBuilder to create a spindle slider To create a new instance of this class, use AutoDieCollection.createSpindleSliderBuilder() Created in NX10.0.2 |
SplitInsertBuilder
Creates split insert builder for progressive die.
|
SplitSolidBuilder
Represents a builder to be used to split a solid with geometry tools.
|
SplitSolidBuilder.OperationType
the split operation type: split, trim.
|
SplitSolidBuilder.ToolObjectOption
the split tool selection type: Existing Object, New Plane.
|
SplitSolidCollection
Creates SplitSolid builder collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
SpreadsheetData
Represents the spreadsheet data which could be standalone spreadsheet file
with special format or be the spreadsheet data from part family template part,
the latter format will not have any other data except the name and value in
class
SpreadsheetDataParameter , that means
it might not return any result in some methods such as "GetDefinedAttributesExpressions". |
SpreadsheetData.DefinedAttributesExpressionsData
This class holds the data returned from
SpreadsheetData.getDefinedAttributesExpressions(nxopen.tooling.SpreadsheetData.KeywordType) |
SpreadsheetData.KeywordType
Represents the different attribute or expression section in spreadsheet
|
SpreadsheetData.ParameterStatus
Represents the different spreadsheet parameter status
|
SpreadsheetDataParameter
Represents parameter in the spreadsheet.
|
SpreadsheetDataParameter.Status
Represents the different spreadsheet parameter status
|
StandardPartBuilder
Represents a builder to be used to create Mold Wizard Standard Part.
|
StandardPartBuilder.EditType
Represents the type to edit a standard part.
|
StandardPartBuilder.RefsetName
Represents the reference set of the standard part when it is added to the assembly.
|
StandardPartCollection
Creates a StandardPartCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
StandardPartData
Represents the standard part client data.
|
StandardPartPositionBuilder
Represents a StandardPartPositionBuilder to add or edit a standard part in the selected plane with specified position.
|
StandardPartPositionCollection
Creates a StandardPartPositionCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX8.5.0 |
StockSizeBuilder
Represents a Tooling::StockSizeBuilder builder.
|
StockSizeBuilder.CalculateBoxSizeData
This class holds the data returned from
StockSizeBuilder.calculateBoxSize() |
StockSizeBuilder.Cylinder
Represents the base circle type of cylinder.
|
StockSizeBuilder.RefCsysType
Represents the reference CSYS type.
|
StockSizeBuilder.Shape
Represents the shape of stock size.
|
StockSizeBuilder.Types
Represents the shape of stock size.
|
StockSizeCollection
Represents a collection of StockSize
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
StripLayoutBuilder
Represents a
StripLayoutBuilder
This class is for Strip Layout Design UI
To create a new instance of this class, use StripLayoutCollection.createStripLayoutBuilder() Created in NX6.0.0 |
StripLayoutBuilder.FromStationType
Specifies the option of From Station for layout
|
StripLayoutBuilder.ToStationType
Specifies the option of To Station for layout
|
StripLayoutCollection
Contains the create functions for builders.
|
StripLayoutStationInformationBuilder
Strip Layout Process Description Builder of Tooling.
|
StripLayoutStationInformationBuilder.StationItem
Specifies the station items
|
StripperVentingBuilder
Stripper Venting Builder of PDW and EDW.
|
SubInsertBuilder
The SubInsert builder
To create a new instance of this class, use SubInsertCollection.createSubInsertBuilder() Default values. |
SubInsertBuilder.Shape
Represents the foot shape
|
SubInsertBuilder.Types
Represents the type of parent part
|
SubInsertCollection
Creates SubInsert builder collection
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
ToolingApplication
Wizard type, some of them should be same as in mpdwshare_uf_mold.h
|
ToolingCloneaction
Clone action type
|
ToolingClonemethod
Clone method
|
ToolingCloneparttype
Part file type, .sim, .fem etc.
|
ToolingDrawingCollection
Creates a
CompDrawingBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
TraverseLoopBuilder
The builder class for Traverse Loop component which assists you
to select or traverse a string of adjacent curves or edges.
|
TraverseLoopBuilder.CheckGapData
This class holds the data returned from
TraverseLoopBuilder.checkGap(nxopen.NXObject[]) |
TraverseLoopCollection
Represents a collection of TraverseLoopbuilder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
TrimMoldComponentsBuilder
Represents a builder to be used to create Mold Wizard trim mold components.
|
TrimMoldComponentsBuilder.TargetScope
the target bodies selection scope
|
TrimMoldComponentsBuilder.TrimMethod
the processing type of Trim Mold Components.
|
TrimMoldComponentsBuilder.TrimPartName
the trim part options where a part chosen to work around
|
TrimMoldComponentsBuilder.TrimSurfaceName
trim surface types
|
TrimMoldComponentsCollection
Creates a TrimMoldComponentsCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
TrimRegionBuilder
Mold Wizard trim region management builder, trims a body to a boundary of edges, curves or bodies.
|
TrimRegionBuilder.BoundaryOption
represents the boundary type option, body/curve type or traverse type.
|
TrimRegionBuilder.ColorValueData
This class holds the data returned from
TrimRegionBuilder.getColorValue() |
TrimRegionBuilder.RegionOption
represents the option to keep or discard the selected region.
|
TrimRegionCollection
Represents a collection of Trim Region
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
TrimSolidBuilder
Mold Wizard trim solid management builder, trims bounding box body with region, subtract
bounding box with workpiece or keep region and box.
|
TrimSolidBuilder.TrimSolidAction
represents the action to create trim solid.
|
TrimSolidBuilder.Types
represents the option to select face or sheet body or manufacturing faces to trim the bounding box.
|
TrimSolidCollection
Represents a collection of Trim Solid
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
UndersizeBuilder
Represents a
UndersizeBuilder To create a new instance of this class, use UndersizeCollection.createUndersizeBuilder() Default values. |
UndersizeBuilder.Orbit
Represents the orbit type
|
UndersizeCollection
Creates a undersize builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
UnfoldingSimulationBuilder
Unfolding Simulation Builder of PDW and EDW.
|
UniversalUnformBuilder.BendTypes
The types of bend
|
UnusedFileManagementBuilder
Represents a
UnusedFileManagementBuilder
Unused File Management is to manage the unused files of the project. |
UnusedFileManagementBuilder.FileDirectory
the unused file location.
|
UnusedFileManagementCollection
Creates a
UnusedFileManagementCollection To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
UserDefinedMotionBuilder
Represents a
UserDefinedMotionBuilder to create user defined motion, which
contains linear and rotary motion To create a new instance of this class, use ProgressiveDieManager.createUserDefinedMotionBuilder() Default values. |
UserDefinedMotionBuilder.LinearCurveTypes
Specifies the motion curve types when motion type is Linear
|
UserDefinedMotionBuilder.MotionTypes
Specifies the motion types
|
UserDefinedMotionBuilder.RotaryCurveTypes
Specifies the motion curve types when motion type is Rotary
|
ValidCheckBuilder
This is the JA builder for static interference check
To create a new instance of this class, use ValidCheckCollection.createValidCheckBuilder() Default values. |
ValidCheckBuilder.AnalysisMode
the analysis mode, including solid-based mode and facet-based mode
|
ValidCheckBuilder.CheckingType
the checking type, including true body, false body or both
|
ValidCheckBuilder.SelMode
the selection type, including component and solid body
|
ValidCheckCollection
Represents a collection of ValidCheck
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
WallThicknessCheckerBuilder
Represents a builder to be used to perform wall thickness analysis.
|
WallThicknessCheckerBuilder.CalculateMethod
The calculation method used for the wall thickness analysis.
|
WallThicknessCheckerBuilder.LegendControl
The legend control used in displaying the thickness results.
|
WallThicknessCheckerBuilder.RangeType
The range type for defining the ranges used in displaying the thickness results.
|
WallThicknessCheckerManager
Represents the manager of the WallThicknessChecker builder
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
WireHoleBuilder
Represents a
WireHoleBuilder
This class is for Wire Hole Design UI
To create a new instance of this class, use WireHoleCollection.createWireHoleBuilder() Default values. |
WireHoleBuilder.Types
the plane to create wire hole sketch
|
WireHoleCollection
Creates a
WireHoleBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
WorkflowManagementCollection
Creates a Workflow Management Collection
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
WorkpieceBuilder
Mold Wizard work piece builder
To create a new instance of this class, use WorkpieceCollection.createWorkpieceBuilder() Default values. |
WorkpieceBuilder.MethodType
the unit type includes the work piece define method
|
WorkpieceBuilder.Types
the unit type includes product and combined work piece type
|
WorkpieceBuilder.WorkPieceType
the unit type includes the work piece create method
|
WorkpieceCollection
Creates a Workpiece Collection
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.