Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static PunchInsertBuilder.PunchPocketTypeItemsPunchPlate |
PunchInsertBuilder.PunchPocketTypeItemsPunchPlate.CIRCLE
Punch pocket type in punch plate is circle
|
static PunchInsertBuilder.PunchPocketTypeItemsPunchPlate |
PunchInsertBuilder.PunchPocketTypeItemsPunchPlate.CLEARANCE
Punch pocket type in punch plate is clearance
|
static PunchInsertBuilder.PunchPocketTypeItemsPunchPlate |
PunchInsertBuilder.PunchPocketTypeItemsPunchPlate.FILLET
Punch pocket type in punch plate is fillet
|
static PunchInsertBuilder.PunchPocketTypeItemsPunchPlate |
PunchInsertBuilder.PunchPocketTypeItemsPunchPlate.SUPER_OFFSET
Punch pocket type in punch plate is super offset
|
Modifier and Type | Method and Description |
---|---|
PunchInsertBuilder.PunchPocketTypeItemsPunchPlate |
PunchInsertBuilder.punchPocketTypeInPunchPlate()
Returns the punch pocket type in punch plate.
|
static PunchInsertBuilder.PunchPocketTypeItemsPunchPlate |
PunchInsertBuilder.PunchPocketTypeItemsPunchPlate.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PunchInsertBuilder.PunchPocketTypeItemsPunchPlate |
PunchInsertBuilder.PunchPocketTypeItemsPunchPlate.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PunchInsertBuilder.PunchPocketTypeItemsPunchPlate[] |
PunchInsertBuilder.PunchPocketTypeItemsPunchPlate.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PunchInsertBuilder.setPunchPocketTypeInPunchPlate(PunchInsertBuilder.PunchPocketTypeItemsPunchPlate punchPocketTypeInPunchPlate)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.