Interface | Description |
---|---|
AddReusableFeatureBuilder |
Represents a
AddReusableFeatureBuilder To create a new instance of this class, use AddReusableFeatureCollection.createBuilder(nxopen.tooling.AddReusableFeatureCollection.InputData) Default values. |
AddReusableFeatureCollection |
Represents a collection of AddReusableFeature
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
AddReusablePart |
Represents a
AddReusablePart
To create a new instance of this class, use AddReusablePartCollection.createBuilder() Default values. |
AddReusablePartCollection |
Represents a collection of AddReusablePart
To obtain an instance of this class, refer to Part Created in NX5.0.0 |
AssemblyDrawingBuilder |
Represents a
AssemblyDrawingBuilder which is
used to create or edit the Assembly Drawing. |
AssignPatchBuilder |
Represents a builder to be used to add sheet bodies as patch surfaces or delete patch surfaces.
|
AssignPatchCollection |
Represents a collection of AssignPatch builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
AutoDieCollection |
Represents a collection of Die Design Draw Punch
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
AutoDieGroup |
Represents a group for Auto Stamping Die
To obtain an instance of this class us AutoDieCollection Created in NX8.0.0 |
AutoDimensionBuilder |
Represents a
AutoDimensionBuilder which is
used to create or edit the Auto Dimension. |
BackingPadBuilder |
Represents a
BackingPadBuilder which is used to create or delete the Backing Pad. |
BendInsertDesignBuilder |
Represents a
BendInsertDesignBuilder
Bend Insert Design is to create inset puch or die for bend . |
BendInsertDesignCollection |
Creates a
BendInsertDesignCollection To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
BendOperationBuilder |
Represents a
BendOperationBuilder builder. |
BendOperationCollection |
Creates a
BendOperationBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.5.0 |
BlankGeneratorBuilder |
Represents a
BlankGeneratorBuilder
This class is for Blank Generator Design UI
To create a new instance of this class, use BlankGeneratorCollection.createBlankGeneratorBuilder() Created in NX7.5.0 |
BlankGeneratorCollection |
Creates a
BlankGeneratorBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
BlankLayoutBuilder |
Progressive Die Wizard blank layout builder
To create a new instance of this class, use BlankLayoutCollection.createBlankLayoutBuilder() Default values. |
BlankLayoutCollection |
Creates a
BlankLayoutBuilder To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
BlankNestingBuilder |
Blank Nesting Builder of PDW, EDW and Die Engineering.
|
BlankNestingCollection |
Creates a
BlankNestingBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.5.0 |
BlendCurve3DBuilder |
Represents a
BlendCurve3DBuilder builder which implements
blend curves in one side where the corner radius is too small. |
BomBuilder |
Represents a Tooling::BomBuilder builder
To create a new instance of this class, use BomCollection.createBomBuilder() Default values. |
BomCollection |
Represents a collection of Bom
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
BomListBuilder |
Represents a
BomListBuilder builder. |
BomListDataProvider |
Provides basic data for BOM List.
|
BurringInsertBuilder |
Progressive Die Wizard builder to design burring punch and die insert
To create a new instance of this class, use BurringInsertCollection.createBurringInsertBuilder() Default values. |
BurringInsertCollection |
Creates a
BurringInsertCollection To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
CaeReuseLibrary |
Represents a
CaeReuseLibrary
To obtain an instance of this class, refer to BaseFEModel Created in NX7.5.2 |
CalculateAreaBuilder |
The CalculateArea builder
To create a new instance of this class, use CalculateAreaCollection.createBuilder() Default values. |
CalculateAreaCollection |
Represents a collection of CalculateArea builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
CAMDataManager |
Represents an object that manages cam data objects.
|
ChangeoverManagementBuilder |
Represents a
ChangeoverManagementBuilder to support changeover workflow management. |
ChannelAdjustBuilder |
The builder class for Channel Adjust which assists you
to adjust the postion and the length of the channel.
|
ChannelAdjustCollection |
Creates a ChannelAdjust Collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
ChannelFittingBuilder |
The builder class for Channel Fitting which assists you
to add cooling fitting.
|
ChannelFittingCollection |
Creates a ChannelFitting Collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
ClearanceManagementBuilder |
Progressive Die Wizard builder to management clearances.
|
ClearanceManagementCollection |
Creates a
ClearanceManagementCollection To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
CloneObject |
Represents the clone operation in Add Reusable Component Builder.
|
ClonePart |
Represents the part inforamtion to be cloned in Add Reusable Component Builder.
|
ColorExpressionsBuilder |
Represents a
ColorExpressionsBuilder builder. |
CompDrawingBuilder |
Represents a
CompDrawingBuilder which is
used to create or edit the Component Drawing. |
ConceptPositionBuilder |
concept position builder for standard part design
To create a new instance of this class, use ConceptPositionCollection.createConceptPositionBuilder() Created in NX6.0.0 |
ConceptPositionCollection |
Represents a collection of ConceptPosition
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
ConcurrentDesignManagementBuilder |
Represents a
ConcurrentDesignManagementBuilder to support concurrent design workflow management. |
CoolingConnectBuilder |
The builder class for Cooling connection which assists you
to create channel and connect it to other channels.
|
CoolingConnectCollection |
Creates a CoolingConnect Collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
CoolingDefineChannelBuilder |
The builder class for Cooling Define Channel which assists you
to create channels directly.
|
CoolingDefineChannelCollection |
Creates a CoolingDefineChannel Collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
CoolingExtendBuilder |
The builder class for Channel Extend which assists you
to extend the channel.
|
CoolingExtendCollection |
Creates a CoolingExtend Collection.
|
CoolingFittingData |
Represents the cooling fitting data in Add Channel Fitting Builder.
|
CoolingPatternBuilder |
The builder class for Cooling pattern which assists you
to create channels with selected curves.
|
CoolingPatternCollection |
Creates a CoolingPattern Collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
CopySolidBuilder |
Represents a
CopySolidBuilder builder. |
CornerDesignBuilder |
Represents a
CornerDesignBuilder ,
Corner Design is to provide tools to make corner. |
CornerDesignCollection |
Creates a
CornerDesignCollection To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
CostTableDataProvider |
Provides basic data for cost feature table data.
|
CreateBoxBuilder |
Represents a box creation operation
To create a new instance of this class, use CreateBoxCollection.createBoxBuilder(nxopen.NXObject) Default values. |
CreateBoxCollection |
Creates CreateBoxBuilder collection
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
DefineCamBuilder |
Represents a
DefineCamBuilder to create different types of cam objects, which
are used for kinematic motion To create a new instance of this class, use ProgressiveDieManager.createDefineCamBuilder() Default values. |
DefineLifterBuilder |
Represents a
DefineLifterBuilder to create different types of lifter objects, which
are used for kinematic motion. |
DefineNeutralFactorBuilder |
Represeents a
DefineNeutralFactorBuilder to define
neutral factor according to material and formula in the spreadsheet table. |
DesignTrimToolBuilder |
Represents a builder to be used to create Mold Wizard design trim tool.
|
DesignTrimToolCollection |
Creates a DesignTrimToolCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
DieBaseBuilder |
Represents Progressive Die Wizard and Engineering Die Wizard builder to manage die base.
|
DieBaseCollection |
Creates a
DieBaseCollection To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
DieCavityAndSlugHoleBuilder |
Represents die cavity and slug hole builder.
|
DieDesDrawDieBuilder |
Represents the Die Design draw die management builder, which is to create a draw die by selected
sheet body, curve and base plane.
|
DieDesDrawPunchBuilder |
Die Design draw punch management builder, create a draw die punch by selected sheet body, curve
and base plane.
|
DieDesignLowerBinderBuilder |
Represents a Lower Binder builder
To create a new instance of this class, use AutoDieCollection.createDieDesignLowerBinderBuilder(nxopen.features.Feature) Created in NX9.0.0 |
DieDesignSettingBuilder |
Represents a
DieDesignSettingBuilder
This class is for Die Design Setting UI
To create a new instance of this class, use DieDesignSettingCollection.createDieDesignSettingBuilder() Default values. |
DieDesignSettingCollection |
Creates a
DieDesignSettingBuilder . |
DieDesignTrimPostBuilder |
Represents a Trim Post builder
To create a new instance of this class, use AutoDieCollection.createDieDesignTrimPostBuilder(nxopen.features.Feature) Created in NX9.0.0 |
DieDesPierceInsertBuilder |
Represents Die Design Pierce Insert builder.
|
DieEngDefineProductOrientationBuilder |
Die Engineer define product orientation builder.
|
DieEngDieTipBuilder |
Die Engineer die tip management builder.
|
DieEngFormTaskBuilder |
Represents a Form Task builder
To create a new instance of this class, use AutoDieCollection.createDieEngFormTaskBuilder(nxopen.features.Feature) Default values. |
DieEngLineupBuilder |
Die Engineer lineup management builder.
|
DieEngProcessUpdateManagerBuilder |
Die Engineer process update manager management builder.
|
DieEngStampingCarryoverBuilder |
Represents a Stamping Carryover builder
To create a new instance of this class, use AutoDieCollection.createDieEngStampingCarryoverBuilder(nxopen.features.BodyFeature) Created in NX10.0.0 |
DieEngStampingOutputBuilder |
Represents a Stamping Output builder
To create a new instance of this class, use AutoDieCollection.createDieEngStampingOutputBuilder(nxopen.features.BodyFeature) Default values. |
DieEngTrimAngleCheck |
Represents a die engineering trim angle check analysis object
To create or edit an instance of this class, use DieEngTrimAngleCheckBuilder Created in NX8.5.0 |
DieEngTrimAngleCheckBuilder |
Represents a Trim Angle Check builder
To create a new instance of this class, use AutoDieCollection.createDieEngTrimAngleCheckBuilder(nxopen.geometricanalysis.AnalysisObject) Default values. |
DieEngTrimTaskBuilder |
Die Engineer trim task management builder, create a trim task by selected die tip, trim bounds,
start plane and end plane.
|
DieInsertBuilder |
Represents die insert builder.
|
DirectUnbendBuilder |
The builder contains all inputs for direct unbend.
|
DirectUnfoldBuilder |
The builder contains all inputs for direct unfolding.
|
DirectUnfoldCollection |
Creates a
DirectUnfoldBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
DrawingSheetNameBuilder |
Represents a
DrawingSheetNameBuilder To create a new instance of this class, use ToolingDrawingCollection.createDrawingSheetNameBuilder() Created in NX8.5.0 |
EdgePatchBuilder |
Represents a builder to be used to create edge patch surfaces.
|
EdgePatchCollection |
Represents a collection of EdgePatch builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
EjectorPostProcessingBuilder |
Represents a builder to be used to create Mold Wizard ejector post processing.
|
EjectorPostProcessingCollection |
Creates a EjectorPostProcessingCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
EjectorTableBuilder |
Represens a ejector table builder.
|
EjectorTableData |
Represents the ejector table data in Ejector Table Builder.
|
ElectrodeBlankBuilder |
Design electrode blank builder to create an electrode blank for the selected body.
|
ElectrodeCheckingBuilder |
Electrode Checking builder to check the touch status of all electrode.
|
ElectrodeComponentBuilder |
Electrode component builder to install holder and pallet.
|
ElectrodeCopyBuilder |
The ElectrodeCopy builder
To create a new instance of this class, use ElectrodeCopyCollection.createElectrodeCopyBuilder() Default values. |
ElectrodeCopyCollection |
Represents a collection of ElectrodeCopy builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
ElectrodeDeleteBuilder |
Electrode delete component builder to remove blank, pallet and holder from assembly.
|
ElectrodeDesign |
Represents an Electrode Design.
|
ElectrodeDesignCollection |
Represents a collection of Electrode Design.
|
ElectrodeInitializationBuilder |
Electrode initialize project builder to creates an electrode design assembly.
|
EnlargeSurfaceBuilder |
Mold Wizard enlarge surface management builder, trims a enlarged surface to a boundary of edges,
curves, datum planes or faces.
|
EnlargeSurfaceCollection |
Represents a collection of Enlarge Surface
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
EWDraftingBuilder |
Represents the drafting builder which is used to create electrode drafting.
|
EWMultiPositionBuilder |
Represents the multiple position builder which is used to get transformed electrode heads together.
|
EWMultiPositionCollection |
Creates EWMultiPosition builder collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
FaceAttributeBuilder |
Represents a builder to be used to create face attribute.
|
FaceColorManagementBuilder |
Tooling builder to assign and edit color of objects
To create a new instance of this class, use FaceColorManagementCollection.createFaceColorManagementBuilder() Default values. |
FaceColorManagementCollection |
Creates a
FaceColorManagementBuilder To obtain an instance of this class, refer to ToolingManager Created in NX9.0.0 |
FaceSplitBuilder |
Represents a face split operation
To create a new instance of this class, use FaceSplitCollection.createFaceSplitBuilder() Default values. |
FaceSplitCollection |
Creates Face Split collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
FamilyMoldBuilder |
Creates a Mold Wizard Family Mold builder
To create a new instance of this class, use FamilyMoldCollection.createFamilyMoldBuilder() Created in NX6.0.0 |
FamilyMoldCollection |
Creates a
FamilyMoldCollection To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
FastenerAssemConfigBuilder |
Represents a Fastener Assem Config Collection.
|
FastenerAssemConfigCollection |
Represents a collection of FastenerAssy
To obtain an instance of this class, refer to ToolingManager Created in NX5.0.0 |
FastenerAssy |
Represents a
FastenerAssy
To create a new instance of this class, use FastenerAssyCollection.createBuilder() Default values. |
FastenerAssyCollection |
Represents a collection of FastenerAssy
To obtain an instance of this class, refer to ToolingManager Created in NX5.0.0 |
FastenerAssyCustomizationBuilder |
Fastener assembly customization builder.
|
FastenerAssyCustomizationCollection |
Represents a collection of FastenerAssyCustomizationBuilder
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
FastenerRemoveNodeBuilder |
Fastener remove node builder.
|
FastenerRemoveNodeCollection |
Represents a collection of FastenerRemoveNodeBuilder
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
FeatureReferenceSetBuilder |
Represents a
FeatureReferenceSetBuilder builder. |
FlowAnalysisBuilder |
Represents the builder which is used to create flow analysis.
|
FlowDisplayBuilder |
Represents the builder which is used to create flow analysis.
|
ForceCalculationBuilder |
Represents a
ForceCalculationBuilder
Force Calculation Design is to calculate force of process
To create a new instance of this class, use ForceCalculationCollection.createForceCalculationBuilder() Default values. |
ForceCalculationCollection |
Creates a
ForceCalculationBuilder To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
FormingInsertBuilder |
Progressive Die Wizard builder to design forming punch and die insert
To create a new instance of this class, use FormingInsertCollection.createFormingInsertBuilder() Default values. |
FormingInsertCollection |
Creates a
FormingInsertBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
GeneralInsertBuilder |
General Insert Design Builder of PDW and EDW.
|
GuidedExtensionBuilder |
Builder for creating Guided Extension surface in NX
To create a new instance of this class, use GuidedExtensionManager.createBuilder() Default values. |
GuidedExtensionManager |
Represents the manager of the GuidedExtension builder
To obtain an instance of this class, refer to ToolingManager |
HemFixerBuilder |
Hem Fixer Builder of PDW and EDW.
|
HoleDatumSymbolBuilder |
Creates hole datum symbol builder for progressive die.
|
HoleManufacturingNoteBuilder |
Tooling builder for HoleManufacturingNote
To create a new instance of this class, use HoleManufacturingNoteCollection.createHoleManufacturingNoteBuilder() Default values. |
HoleManufacturingNoteCollection |
Creates a
HoleManufacturingNoteBuilder To obtain an instance of this class, refer to ToolingManager Created in NX9.0.0 |
HoleReportBuilder |
Represents a
HoleReportBuilder
This class is for Hole Report Design UI
To create a new instance of this class, use HoleReportCollection.createHoleReportBuilder() Default values. |
HoleReportCollection |
Creates a
HoleReportBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
InitProjBuilder |
Represents a
InitProjBuilder
To create a new instance of this class, use InitProjCollection.createInitProjBuilder() Default values. |
InitProjCollection |
Represents a collection of InitProj
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
InitProjectBuilder |
Mold Wizard initialize project builder
To create a new instance of this class, use InitProjectCollection.createBuilder() Default values. |
InitProjectCollection |
Represents a collection of InitProject builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
InsertAuxiliaryBuilder |
PDW insert auxiliary builder to design various auxiliaries of insert group
To create a new instance of this class, use InsertAuxiliaryCollection.createInsertAuxiliaryBuilder() Default values. |
InsertAuxiliaryCollection |
Creates a
InsertAuxiliaryBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
InsertEditToolsBuilder |
Represents a
InsertEditToolsBuilder which is
used to copy or delete the insert edit. |
IntermediateStageBuilder |
Represents a
IntermediateStageBuilder builder. |
IntermediateStageCollection |
Creates a
IntermediateStageBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.5.0 |
LayoutBuilder |
Represents a Tooling::LayoutBuilder builder
To create a new instance of this class, use MWLayoutCollection.createLayoutBuilder() Default values. |
LayoutManagementBuilder |
Layout Management Builder of Engineering Die Wizard
To create a new instance of this class, use LayoutManagementCollection.createLayoutManagementBuilder() Default values. |
LayoutManagementCollection |
Creates a
LayoutManagementBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
LayoutRepositionBuilder |
Represents a Tooling::LayoutRepositionBuilder builder
To create a new instance of this class, use MWLayoutCollection.createLayoutRepositionBuilder() Default values. |
LsdynaFormAnalysisResultDisplayBuilder |
Represents a Ly-Dyna Formability Analysis - Result Display builder
To create a new instance of this class, use AutoDieCollection.createLsdynaFormAnalysisResultDisplayBuilder() Default values. |
LsdynaGeometryPreparationBuilder |
Stamping Die LS-Dyna integration draw geometry preprare builder.
|
LsdynaKfileGeneratorBuilder |
Represents LS-Dyna K file builder - K file generator builder
To create a new instance of this class, use AutoDieCollection.createLsdynaKfileGeneratorBuilder() Default values. |
ManufacturingGeometryBuilder |
Represents a builder to be used to create manufacturing geometry.
|
ManufacturingGeometryCollection |
Represents a collection of Manufacturing Geometry builder.
|
MoldCsysBuilder |
Mold Wizard MoldCsys project builder
To create a new instance of this class, use MoldCsysCollection.createMoldCsysBuilder() Default values. |
MoldCsysCollection |
Creates a
MoldCsysCollection To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MoldDesign |
Represents an Mold Design.
|
MoldDesignCollection |
Represents a collection of Mold Design.
|
MoldFeatureRecognitionBuilder |
Represents a
MoldFeatureRecognitionBuilder builder To create a new instance of this class, use MoldwizardManager.createMoldFeatureRecognitionBuilder() Default values. |
MoldFillingBuilder |
Builder used to add a gate/runner standard part from fill library, it returns null.
|
MoldInsertBuilder |
Mold Wizard mold insert management builder
To create a new instance of this class, use MoldInsertCollection.createMoldInsertBuilder() Default values. |
MoldInsertCollection |
Creates a MoldInsertCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MoldProcessBuilder |
Represents a Tooling::MoldProcessBuilder builder
To create a new instance of this class, use MoldProcessCollection.createMoldProcessBuilder() Default values. |
MoldProcessCollection |
Represents a collection of Mold Process
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MoldwizardManager |
Provides create builder methods for Moldwizard.
|
MotionSimulationBuilder |
Represents a
MotionSimulationBuilder to support dynamic interference check. |
MotionSimulationCollection |
Represents a collection of MotionSimulation.
|
MWCopySheetsBuilder |
Builder for copying sheets in the Mold Wizard application
To create a new instance of this class, use MWCopySheetsCollection.createBuilder() Default values. |
MWCopySheetsCollection |
Represents a collection of MWCopySheets builder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
MWDefineRegionsBuilder |
The MWDefineRegions builder
To create a new instance of this class, use MWDefineRegionsCollection.createBuilder() Default values. |
MWDefineRegionsCollection |
Represents a collection of MWDefineRegions builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MWDefineSheetsBuilder |
Builder for defining sheets in Mold Wizard
To create a new instance of this class, use MWDefineSheetsCollection.createBuilder() Default values. |
MWDefineSheetsCollection |
Represents a collection of MWDefineSheets builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MWDesignGuideLinesBuilder |
The builder for designing guide lines in Mold Wizard.
|
MWDesignGuideLinesCollection |
Represents a collection of MWDesignGuideLines builder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
MWDesignPartingSurfaceBuilder |
The builder for designing parting surface in Mold Wizard.
|
MWDesignPartingSurfaceCollection |
Represents a collection of MWDesignPartingSurface builder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
MWLayoutCollection |
Creates Mold Wizard layout collection
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MWMoldedPartValidationBuilder |
Represents a builder to be used to perform Molded Part Validation analysis.
|
MWMoldedPartValidationManager |
Represents a manager of the MWMoldedPartValidation builder
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
MWPartingManagerBuilder |
Builder for the Parting Manager in the Mold Wizard application
To create a new instance of this class, use MWPartingManagerCollection.createBuilder() Created in NX7.5.0 |
MWPartingManagerCollection |
Represents a collection of MWPartingManager builder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
MWSearchRegionBuilder |
The Search Region builder is for defining a region by searching the region faces given a set of seed faces and boundary edges.
|
MWSearchRegionCollection |
Represents a collection of MWSearchRegion builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MWTraversePartingLinesBuilder |
Builder for creating parting lines by traversing in the Mold Wizard application
To create a new instance of this class, use MWTraversePartingLinesCollection.createBuilder() Created in NX7.5.0 |
MWTraversePartingLinesCollection |
Represents a collection of the MWTraversePartingLines builder
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
ObjectAttributeManagementBuilder |
Tooling builder to assign and edit attributes of objects
To create a new instance of this class, use ObjectAttributeManagementCollection.createObjectAttributeManagementBuilder() Default values. |
ObjectAttributeManagementCollection |
Creates a
ObjectAttributeManagementBuilder To obtain an instance of this class, refer to ToolingManager Created in NX9.0.0 |
OffsetCurve3DBuilder | Deprecated
Deprecated in NX10.0.0.
|
PiercingInsertBuilder |
Represents piercing insert builder.
|
PiercingInsertCollection |
Creates a
PiercingInsertBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
PiercingInsertMiniToolsBuilder |
Represents piercing insert mini tools builder.
|
PocketBuilder |
Mold Wizard pocket management builder
To create a new instance of this class, use PocketCollection.createPocketBuilder() Default values. |
PocketCollection |
Creates a
PocketBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
PrebendBuilder |
Represents a
PrebendBuilder builder to divide bend faces. |
ProfileSplitBuilder |
The ProfileSplit builder
To create a new instance of this class, use ProfileSplitCollection.createProfileSplitBuilder() Created in NX6.0.0 |
ProfileSplitCollection |
Represents a collection of ProfileSplit builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
ProgressiveDieManager |
Provides create builder methods for Progressive Die.
|
PunchInsertBuilder |
Represents punch insert builder.
|
QuickDatumCsysBuilder |
Represents a
QuickDatumCsysBuilder builder. |
QuickQuotationBuilder |
Progressive Die Wizard builder to create quick quotation.
|
QuickQuotationCollection |
Creates a
QuickQuotationBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
ReferenceBlendBuilder |
The ReferenceBlend builder
To create a new instance of this class, use ReferenceBlendCollection.createReferenceBlendBuilder() Created in NX7.0.0 |
ReferenceBlendCollection |
Creates reference blend collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
ReliefDesignBuilder |
Represents a
ReliefDesignBuilder
Relief Design is to cut relief pocket for forming region . |
ReliefDesignCollection |
Creates a
ReliefDesignBuilder To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
RemoveHolesBuilder |
Remove Hole is used to patch holes for a solid body.
|
RenameAndExportComponentBuilder |
Creates rename and export component builder for progressive die.
|
ReplaceSolidBuilder |
Represents a replace solid operation.
|
ReplaceSolidCollection |
Creates ReplaceSolidBuilder collection
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
ReusableObject |
Represents a
ReusableObject
To create a new instance of this class, use ToolingManager.createReusableObject() Created in NX7.5.2 |
ReusableObjectManager |
Represents a collection of ReusableObjects
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
ReusableObjectPasteBuilder |
Represents a
ReusableObjectPasteBuilder Use the ReusableObjectManager class to create a ReusableObjectPasteBuilder. |
ReusablePocketBuilder |
Reusable pocket builder.
|
ReusablePocketCollection |
Represents a collection of ReusablePocketBuilder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
ReusePositioningObjectBuilder |
Represents a
ReusePositioningObjectBuilder Use the ReusableObjectManager class to create a ReusePositioningObjectBuilder. |
Runner |
Represents a runner feature
To create or edit an instance of this class, use RunnerBuilder Created in NX11.0.0 |
RunnerBuilder |
Mold Wizard runner management builder, select curves as runner guide, choose section type and edit
section parameters, optional choose boolean type to create runner channel.
|
RunnerCollection |
Represents a collection of Runner
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
RunSimulationBuilder |
Represents a
RunSimulationBuilder to animate the model,
analyze the collision and reference. null is returned To create a new instance of this class, use ProgressiveDieManager.createRunSimulationBuilder() Default values. |
ScrapDesignBuilder |
Represents a scrap design builder
To create a new instance of this class, use ScrapDesignCollection.createScrapDesignBuilder() Default values. |
ScrapDesignCollection |
Represents a collection of ScrapDesign
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
SectionLineCreationBuilder |
Represents a
SectionLineCreationBuilder which is
used to create or edit the section line creation. |
SelectReuseLibraryItemBuilder |
Select a part from the reuse library .
|
SelectReuseLibraryListBuilder |
Select a list of objects from the reuse library .
|
SelectReuseLibraryListItemBuilder |
Select reuse library list item .
|
SelectReuseLibraryListItemBuilderList |
Represents a list of objects.
|
SetPressModelBuilder |
Represents a
SetPressModelBuilder to set and load the press model. |
SheetMetalFeatureRecognitionBuilder |
Represents a
SheetMetalFeatureRecognitionBuilder builder To create a new instance of this class, use MoldwizardManager.createSheetMetalFeatureRecognitionBuilder() Created in NX11.0.1 |
ShimBuilder |
Shim Builder of PDW and EDW.
|
ShimInnerProfileSetBuilder |
This is a seed block of set list.
|
ShimInnerProfileSetBuilderList |
Represents a list of objects.
|
SIZERCollection |
Represents a collection of SIZER
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
SIZERExportBuilder |
Exports input parameters for motor selection to SIZER drive design to
support the sizing, configuration, and selection of drive components.
|
SIZERImportBuilder |
Imports results for motor selection from SIZER drive design based on
the sizing, configuration, and selection of drive components.
|
SlugRetentionBuilder |
Represents a
SlugRetentionBuilder which is used to create the Slug Retention. |
SmartScrewUpdateBuilder |
Smart Screw Update of MW, PDW and EDW.
|
SolidPatchBuilder |
Represents a builder to be used to create a solid patch.
|
SolidPatchCollection |
Represents a collection of SolidPatch builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
SpecialFormingBuilder |
Creates special forming insert builder for progressive die.
|
SpecialPiercingInsertBuilder |
Creates special piercing insert for progressive die.No entity is returned.
|
SpecifyBaffleBuilder |
Represents a builder to be used to create specify baffle.
|
SpecifyBaffleCollection |
Represents a collection of Specify Baffle builder
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
SpecifyCircuitBuilder |
Represents a builder to be used to create specify circuit.
|
SpecifyCircuitCollection |
Represents a collection of Specify Circuit builder
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
SpindleSliderBuilder |
Represents a
SpindleSliderBuilder to create a spindle slider To create a new instance of this class, use AutoDieCollection.createSpindleSliderBuilder() Created in NX10.0.2 |
SplitInsertBuilder |
Creates split insert builder for progressive die.
|
SplitSolidBuilder |
Represents a builder to be used to split a solid with geometry tools.
|
SplitSolidCollection |
Creates SplitSolid builder collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
SpreadsheetData |
Represents the spreadsheet data which could be standalone spreadsheet file
with special format or be the spreadsheet data from part family template part,
the latter format will not have any other data except the name and value in
class
SpreadsheetDataParameter , that means
it might not return any result in some methods such as "GetDefinedAttributesExpressions". |
SpreadsheetDataParameter |
Represents parameter in the spreadsheet.
|
StandardPartBuilder |
Represents a builder to be used to create Mold Wizard Standard Part.
|
StandardPartCollection |
Creates a StandardPartCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
StandardPartData |
Represents the standard part client data.
|
StandardPartPositionBuilder |
Represents a StandardPartPositionBuilder to add or edit a standard part in the selected plane with specified position.
|
StandardPartPositionCollection |
Creates a StandardPartPositionCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX8.5.0 |
StockSizeBuilder |
Represents a Tooling::StockSizeBuilder builder.
|
StockSizeCollection |
Represents a collection of StockSize
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
StripLayoutBuilder |
Represents a
StripLayoutBuilder
This class is for Strip Layout Design UI
To create a new instance of this class, use StripLayoutCollection.createStripLayoutBuilder() Created in NX6.0.0 |
StripLayoutCollection |
Contains the create functions for builders.
|
StripLayoutStationInformationBuilder |
Strip Layout Process Description Builder of Tooling.
|
StripperVentingBuilder |
Stripper Venting Builder of PDW and EDW.
|
SubInsertBuilder |
The SubInsert builder
To create a new instance of this class, use SubInsertCollection.createSubInsertBuilder() Default values. |
SubInsertCollection |
Creates SubInsert builder collection
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
ToolingDrawingCollection |
Creates a
CompDrawingBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
ToolingManager |
Contains the collection objects for creating and iterating over Reuse Library objects.
|
ToolingSession | |
TraverseLoopBuilder |
The builder class for Traverse Loop component which assists you
to select or traverse a string of adjacent curves or edges.
|
TraverseLoopCollection |
Represents a collection of TraverseLoopbuilder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
TrimMoldComponentsBuilder |
Represents a builder to be used to create Mold Wizard trim mold components.
|
TrimMoldComponentsCollection |
Creates a TrimMoldComponentsCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
TrimRegionBuilder |
Mold Wizard trim region management builder, trims a body to a boundary of edges, curves or bodies.
|
TrimRegionCollection |
Represents a collection of Trim Region
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
TrimSolidBuilder |
Mold Wizard trim solid management builder, trims bounding box body with region, subtract
bounding box with workpiece or keep region and box.
|
TrimSolidCollection |
Represents a collection of Trim Solid
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
UndersizeBuilder |
Represents a
UndersizeBuilder To create a new instance of this class, use UndersizeCollection.createUndersizeBuilder() Default values. |
UndersizeCollection |
Creates a undersize builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
UnfoldingSimulationBuilder |
Unfolding Simulation Builder of PDW and EDW.
|
UniversalUnformBuilder |
Represents a
UniversalUnformBuilder builder. |
UnusedFileManagementBuilder |
Represents a
UnusedFileManagementBuilder
Unused File Management is to manage the unused files of the project. |
UnusedFileManagementCollection |
Creates a
UnusedFileManagementCollection To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
UserDefinedMotionBuilder |
Represents a
UserDefinedMotionBuilder to create user defined motion, which
contains linear and rotary motion To create a new instance of this class, use ProgressiveDieManager.createUserDefinedMotionBuilder() Default values. |
ValidCheckBuilder |
This is the JA builder for static interference check
To create a new instance of this class, use ValidCheckCollection.createValidCheckBuilder() Default values. |
ValidCheckCollection |
Represents a collection of ValidCheck
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
WallThicknessCheckerBuilder |
Represents a builder to be used to perform wall thickness analysis.
|
WallThicknessCheckerManager |
Represents the manager of the WallThicknessChecker builder
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
WireHoleBuilder |
Represents a
WireHoleBuilder
This class is for Wire Hole Design UI
To create a new instance of this class, use WireHoleCollection.createWireHoleBuilder() Default values. |
WireHoleCollection |
Creates a
WireHoleBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
WorkflowManagementCollection |
Creates a Workflow Management Collection
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
WorkpieceBuilder |
Mold Wizard work piece builder
To create a new instance of this class, use WorkpieceCollection.createWorkpieceBuilder() Default values. |
WorkpieceCollection |
Creates a Workpiece Collection
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
Class | Description |
---|---|
AddReusableFeatureBuilder.LayerOptionType |
Represents the layer option type
|
AddReusableFeatureBuilder.UserExpressionsData |
This class holds the data returned from
AddReusableFeatureBuilder.getUserExpressions() |
AddReusableFeatureCollection.InputData |
Defines the input data of AddReusableFeatureBuilder
|
AddReusablePart.ComponentMode |
Represents the component type of the added part
|
AddReusablePart.ModeMethod |
Represents adding or editing a reusable component mode method
|
AddReusablePart.PocketBodyMethod |
Represents save pocket body information, updating or deleting a pocket body size mode method
|
AddReusablePart.PositionMethod |
Represents the position method
|
AssemblyDrawingBuilder.AttributeNames |
Specifies the attribute name
|
AssemblyDrawingBuilder.AttributeValues |
Specifies the attribute value.
|
AssemblyDrawingBuilder.DrawingCreateOrEdit |
Specifies the sheet operation.
|
AssemblyDrawingBuilder.DrawingTypes |
Specifies the drawing type.
|
AssemblyDrawingBuilder.ModelViewToUseValue |
Specifies the model view to use.
|
AssemblyDrawingBuilder.Types |
Specifies the filter of assembly.
|
AssemblyDrawingBuilder.ViewOptionValue |
Specifies the view options.
|
AssignPatchBuilder.ConvertTypeOption |
The option to convert to have copies or no copies for all selected sheets.
|
AssignPatchBuilder.PatchColorData |
This class holds the data returned from
AssignPatchBuilder.getPatchColor() |
AssignPatchBuilder.Types |
The types for assigning sheets.
|
AutoDimensionBuilder.MainType |
create or edit ordinate dimension
|
AutoDimensionBuilder.TextFontType |
text font type
|
AutoDimensionBuilder.TextOrientationType |
text orientation type
|
AutoDimensionBuilder.ToleranceType |
tolerance type
|
AutoDimensionBuilder.ValuePrecisionType |
value precision type
|
BackingPadBuilder.Types |
types of backing pad design
|
BendInsertDesignBuilder.BendingDirectionOption |
the bending direction.
|
BendInsertDesignBuilder.BendTypeOption |
the bend type.
|
BendInsertDesignBuilder.BlankPositions |
Specifies the blank position.
|
BendInsertDesignBuilder.InsertTypeOption |
the insert type.
|
BendInsertDesignBuilder.ParentOption |
the parent node.
|
BendInsertDesignBuilder.Types |
the bending operation.
|
BendOperationBuilder.OverbendOptions |
The overbend option.
|
BendOperationBuilder.Prebend |
The number of children bends of prebend.
|
BendOperationBuilder.Types |
unbend operations.
|
BlankGeneratorBuilder.CreateBlankType |
Specify the creation method.
|
BlankGeneratorBuilder.EditBlankType |
Specify the edit method.
|
BlankGeneratorBuilder.Types |
Specifies the option of blank generator operation type.
|
BlankLayoutBuilder.LeftRightSideOption |
Specifies the option of left right side type.
|
BlankLayoutBuilder.SideWebOption |
Specifies the option of side webs type.
|
BlankLayoutBuilder.SnapSizeOption |
Specifies the option of snap size.
|
BlankLayoutBuilder.Types |
Specifies the option of blank layout type.
|
BlankNestingBuilder.LayoutTypeSpecification |
Specifies the layout type of blank nesting.
|
BlendCurve3DBuilder.BlendCurveOptions |
The blend curve creation methods: Best Fit, Variable, Vector, Current View
|
BlendCurve3DBuilder.InputCurvesOption |
The input curves option to keep, hide or delete input curves
|
BomBuilder.Circle |
Represents an index to the base circle type of cylinder shape.
|
BomBuilder.Shape |
Represents an index to the shape of stock size.
|
BomBuilder.TreeList |
Represents an index to components list type.
|
BomListBuilder.BomListSortOption |
Represents an enumeration indicating whether the sorting needs to be performed in ascending or descending order.
|
BomListBuilder.BomListTypes |
Represents an index to components list type.
|
BomListDataProvider.ExportedStatus |
Represents the exported status of a cell.
|
BurringInsertBuilder.BurringDirections |
Specifies the burring direction.
|
BurringInsertBuilder.BurringPunchTypes |
Specifies the burring punch type.
|
BurringInsertBuilder.CircularOrNonCircularType |
Specifies the circular or non-circular type.
|
BurringInsertBuilder.DesignOptions |
Specifies the design type.
|
BurringInsertBuilder.ParentTypes |
Specifies the parent part type.
|
CalculateAreaBuilder.SheetMethodType |
Represents the methods to create the projected sheet body.
|
ChangeoverManagementBuilder.Types |
Specifies the types of changeover management.
|
ChannelAdjustBuilder.AdjustType |
the adjust method.
|
ChannelAdjustBuilder.VectorMethod |
the vector adjust method.
|
ClearanceManagementBuilder.Selection |
Specifies clearance management part.
|
ClearanceManagementBuilder.Type |
Specifies type to assign or check clearances
|
CompDrawingBuilder.ComponentTypeSelection |
Specifies the type of components.
|
CompDrawingBuilder.DrawingType |
Specifies the drawing type.
|
CompDrawingBuilder.FilterSelection |
Specifies the filter of components.
|
CompDrawingBuilder.ProjectionType |
Specifies the project type.
|
ConcurrentDesignManagementBuilder.Types |
Specifies the types of concurrent design management.
|
ConcurrentDesignManagementBuilder.UpdateTypes |
Specifies the types of the update action.
|
CoolingDefineChannelBuilder.ExtensionTypes |
The extension types of channel
|
CoolingDefineChannelBuilder.TipEndTypes |
The tip end types of channel
|
CoolingDefineChannelBuilder.Types |
Types to specify how to assign attributes to the created body.
|
CoolingExtendBuilder.TipEndTypes |
The tip end types of channel
|
CornerDesignBuilder.CornerTypeOpt |
the corner types
|
CornerDesignBuilder.SelectFromOpt |
the object selection options.
|
CornerDesignBuilder.Types |
The corner design type.
|
CreateBoxBuilder.BoxType |
the type for creating box
|
DefineCamBuilder.PredefinedHydraulicOptions |
Specifies the predefined hydraulic motion types
|
DefineCamBuilder.Types |
Specifies the cam types
|
DefineLifterBuilder.Types |
Specifies the lifter types
|
DefineNeutralFactorBuilder.FormulaOptions |
Specifies the formula used to calculate the neutral factor value
|
DieBaseBuilder.AlongDirectionOpt |
along direction options.
|
DieBaseBuilder.CatalogOpt |
catalog options.
|
DieBaseBuilder.DesignToolOption |
design tool options.
|
DieBaseBuilder.DieBaseTypeOpt |
die bse types options.
|
DieBaseBuilder.ParentNodeOpt |
parent node options.
|
DieBaseBuilder.PlatesNumberOpt |
plates number options.
|
DieBaseBuilder.SplitMethod |
split method.
|
DieBaseBuilder.SplitOption |
split options.
|
DieBaseBuilder.Types |
die base types.
|
DieCavityAndSlugHoleBuilder.BottomPlateSlugItems |
Specifies the type of bottom plate slug.
|
DieCavityAndSlugHoleBuilder.CavityTypeItems |
Specifies the type of cavity.
|
DieCavityAndSlugHoleBuilder.ClearanceOptionItems |
Specifies the design option of piercing insert.
|
DieCavityAndSlugHoleBuilder.DieInsertStackType |
die insert stack type.
|
DieCavityAndSlugHoleBuilder.DiePlateThreeSlugType |
die plate three slug type.
|
DieCavityAndSlugHoleBuilder.DiePlateTwoSlugType |
die plate two slug type.
|
DieCavityAndSlugHoleBuilder.DieShoeSlugTypeItems |
Specifies the type of die shoe slug.
|
DieCavityAndSlugHoleBuilder.InsertPositionItems |
Specifies the position of piercing inserts, for EDW only
|
DieCavityAndSlugHoleBuilder.OffsetSideOptionItems |
Specifies the offset side of normal pierce insert design.
|
DieDesPierceInsertBuilder.Direction |
Represents the thickness direction.
|
DieDesPierceInsertBuilder.HoleShapeTypes |
Represents the hole shape type.
|
DieEngDefineProductOrientationBuilder.FacetQualityOption |
the facet quality option
|
DieEngDefineProductOrientationBuilder.OptimalMethod |
the optimal method
|
DieEngDefineProductOrientationBuilder.ViewDraftOptions |
view draft options
|
DieEngDieTipBuilder.MaterialThicknessType |
the material thickness type
|
DieEngProcessUpdateManagerBuilder.Types |
the trim task or pierce task.
|
DieEngStampingOutputBuilder.DisplayProductType |
Types of product display.
|
DieEngStampingOutputBuilder.SpringbackMethodType |
Types of springback method
|
DieEngTrimAngleCheckBuilder.DirectionOptions |
Options to determine the method to specify direction.
|
DieEngTrimTaskBuilder.TrimTaskCamType |
the trim task cam type.
|
DieEngTrimTaskBuilder.TrimTaskMatchCutType |
the trim task match cut type.
|
DieInsertBuilder.BoundingBoxTypeItems |
Specifies the bounding box type.
|
DieInsertBuilder.DieInsertTypeItems |
Specifies the type of insert.
|
DieInsertBuilder.InsertModeItems |
Specifies the insert mode for die.
|
DieInsertBuilder.PositionItems |
Specifies the position of piercing inserts, for EDW only
|
DirectUnbendBuilder.Bendtypes |
unbend operations.
|
DirectUnfoldBuilder.Bend |
The number of children bends in defining prebend.
|
DirectUnfoldBuilder.BodyList |
The name list of bodies in current part.
|
DirectUnfoldBuilder.MatType |
The material database defined in PDW.
|
DirectUnfoldBuilder.Types |
Specifies the option of direct unfold type
|
EdgePatchBuilder.BodyColorData |
This class holds the data returned from
EdgePatchBuilder.getBodyColor() |
EdgePatchBuilder.PatchStatus |
Settings of the patch status types.
|
EdgePatchBuilder.SelectTypes |
Settings of the selection types.
|
EjectorPostProcessingBuilder.TrimMethod |
The processing type: Trim, Adjust length and Untrim.
|
EjectorPostProcessingBuilder.TrimPartName |
The trim part where to find a trim surface as tool to trim ejector pins.
|
EjectorPostProcessingBuilder.TrimSufaceName |
The trim surface types.
|
EjectorTableBuilder.DrawingType |
The types of the ejector drawing.
|
EjectorTableBuilder.EjectorType |
The types of ejectors.
|
ElectrodeBlankBuilder.BlankMaterial |
Represents the blank material option.
|
ElectrodeBlankBuilder.BlankShape |
Represents the electrode blank shape option.
|
ElectrodeBlankBuilder.JointObject |
Represents the transition type between head bodies and the blank.
|
ElectrodeComponentBuilder.Chuck |
Represents the electrode chuck type.
|
ElectrodeCopyBuilder.Copy |
Represents an index to copy type
|
ElectrodeCopyBuilder.UpdateParameterData |
This class holds the data returned from
ElectrodeCopyBuilder.updateParameterData(nxopen.TaggedObject, nxopen.TaggedObject) |
ElectrodeDeleteBuilder.Types |
delete sparking solid from blank or delete blank, pallet or holder directly.
|
ElectrodeInitializationBuilder.Method |
The initialize type: Original, No Working Part, No Machine Set Part and No Template.
|
ElectrodeInitializationBuilder.Type |
Clone a member of an electrode assembly, such as top part, machine set part, and working part.
|
EnlargeSurfaceBuilder.ColorValueData |
This class holds the data returned from
EnlargeSurfaceBuilder.getColorValue() |
EnlargeSurfaceBuilder.KeepDiscardOption |
represents the keep discard options for selected region.
|
EWDraftingBuilder.CNCTemplateOption |
the template option of cnc sheet type
|
EWDraftingBuilder.DrawingOption |
the drawing type
|
EWDraftingBuilder.EDMTemplateOption |
the template option of edm sheet type
|
EWDraftingBuilder.ModeOption |
the drafting mode option
|
EWDraftingBuilder.NameOption |
the drawing sheet name option
|
FaceColorManagementBuilder.HoleTypeEnumValue |
the hole type enumeration
|
FaceSplitBuilder.FaceSplitType |
the type for Split Face
|
FastenerAssy.HoleOperation |
Represents the action on the hole menu of the fastener assembly.
|
FastenerAssy.ModeMethod |
Represents adding and editing modes for the fastener assembly
|
FastenerAssy.SelectionObjectMethod |
Represents selection object type
|
FastenerAssy.SelectionTypeMethod |
Represents selection type for position and hole
|
FastenerAssy.StackTypeMethod |
Represents screw_array type
|
FlowDisplayBuilder.AnalysisResults |
The option of analysis results.
|
ForceCalculationBuilder.CalculationTypes |
The calculation type.
|
ForceCalculationBuilder.ProcessTypes |
The process type.
|
FormingInsertBuilder.BlankPositions |
Specifies the blank position.
|
FormingInsertBuilder.BlankTypes |
Specifies the blank type.
|
FormingInsertBuilder.DesignOptions |
Specifies the design type.
|
FormingInsertBuilder.ParentTypes |
Specifies the parent part type.
|
GeneralInsertBuilder.GenerateMethod |
Specify the creation method of insert.
|
GeneralInsertBuilder.ParentOption |
Specify the part parent of insert part.
|
GeneralInsertBuilder.Types |
Specify the insert operation type.
|
GuidedExtensionBuilder.SegmentType |
Segment type for segments
|
HoleDatumSymbolBuilder.SymbolType |
symbol type
|
HoleManufacturingNoteBuilder.DefineByViewOrHoles |
the view selection or window selection type
|
HoleManufacturingNoteBuilder.HoleIndexType |
the hole index type
|
HoleReportBuilder.EnumQuadrantType |
Specifies the option of which quadrant is positive
|
HoleReportBuilder.EnumSelectionType |
Specifies the option of selection type to create hole table
|
HoleReportBuilder.Types |
Specifies the option of hole table type
|
InitProjBuilder.ProjTempOption |
Represents the project template option of InitProj,
defines the pre-defined project template. this template will be used as the basic assembly structure for this new project
|
InitProjectBuilder.ConfigurationId |
the configuration type includes default and orig
|
InitProjectBuilder.MaterialId |
the material type includes None and Nylon
|
InitProjectBuilder.UnitId |
the unit type includes metric and inch project type
|
InsertAuxiliaryBuilder.CircOperationTypes |
Specifies the options of circular array.
|
InsertAuxiliaryBuilder.DesignToolOption |
Specifies the design tool option.
|
InsertAuxiliaryBuilder.RampStepsType |
Specifies the ramp steps.
|
InsertAuxiliaryBuilder.RectOperationOption |
Specifies the rectangular array option.
|
InsertAuxiliaryBuilder.ShankShapeTypes |
Specifies the shank shape.
|
InsertAuxiliaryBuilder.Types |
Specifies the insert auxiliary type.
|
InsertAuxiliaryBuilder.UseFaceOrSketchToRevolve |
Specifies the use face or sketch to revolve.
|
InsertEditToolsBuilder.Types |
Specifies the insert edit tools type.
|
IntermediateStageBuilder.DesignSequences |
The types of design sequences
|
IntermediateStageBuilder.EditOptions |
The types of changed intermediate stages
|
IntermediateStageBuilder.Orientations |
The types of orientation of intermediate stages
|
LayoutBuilder.BalNumber |
Represents the number of balance cavity.
|
LayoutBuilder.LayoutSubType |
Represents the the sub type of layout.
|
LayoutBuilder.LayoutType |
Represents the type of layout.
|
LayoutBuilder.XrefNum |
Represents the type of x move refer.
|
LayoutBuilder.YrefNum |
Represents the type of y move refer.
|
LayoutManagementBuilder.StationItems |
Specifies the station items
|
LayoutRepositionBuilder.Method |
Represents the type of layout transform.
|
LayoutRepositionBuilder.Type |
Represents the method of layout transform.
|
LsdynaFormAnalysisResultDisplayBuilder.FormabilityStrainTypeName |
Options to set strain type to display for formability analysis result.
|
LsdynaFormAnalysisResultDisplayBuilder.StrainTypeName |
Options to set strain type to display for strain analysis result.
|
LsdynaFormAnalysisResultDisplayBuilder.StressTypeName |
Options to set stress type to display for stress analysis result.
|
LsdynaGeometryPreparationBuilder.BlankOption |
the enum of blank option.
|
LsdynaGeometryPreparationBuilder.BlankPosition |
the enum of blank position.
|
LsdynaGeometryPreparationBuilder.ContactType |
the enum of contact type.
|
LsdynaGeometryPreparationBuilder.DrawBeadType |
the enum of draw bead type.
|
LsdynaGeometryPreparationBuilder.DrawType |
the enum of draw type.
|
LsdynaGeometryPreparationBuilder.MaterialType |
the enum of material type.
|
LsdynaGeometryPreparationBuilder.ProcessActionBinder |
the enum of process action binder type.
|
LsdynaGeometryPreparationBuilder.ProcessActionDie |
the enum of process action die type.
|
LsdynaGeometryPreparationBuilder.ProcessActionPunch |
the enum of process action punch type.
|
LsdynaGeometryPreparationBuilder.ProcessType |
the enum of process type.
|
LsdynaGeometryPreparationBuilder.TargetBinder |
the enum of target binder type.
|
LsdynaGeometryPreparationBuilder.TargetDie |
the enum of target die type.
|
LsdynaGeometryPreparationBuilder.TargetPunch |
the enum of target punch type.
|
LsdynaKfileGeneratorBuilder.MeshDataType |
Types of data format.
|
LsdynaKfileGeneratorBuilder.MeshElementType |
Types of mesh element type.
|
LsdynaKfileGeneratorBuilder.OperTypes |
Types of operation.
|
MoldCsysBuilder.Wcsposition |
Represents the method to computer the WCS positino
|
MoldFillingBuilder.InstallOption |
The installation type of the fill component.
|
MoldFillingBuilder.MoveOption |
The modification options of the selected fill component.
|
MoldInsertBuilder.BooleanType |
design type: unite single workpieces, subtract overall workpieces
|
MotionSimulationBuilder.CamDefinitionType |
Specifies the way to define cam, automatically or manually.
|
MotionSimulationBuilder.EjectorMoveOptions |
Specifies the ejector move type, after or while
|
MotionSimulationBuilder.MoldbaseStyleType |
Specifies the style type of moldbase, two-plate style or three-plate style
|
MotionSimulationBuilder.Types |
Specifies the operation options of motion simulation.
|
MWCopySheetsBuilder.Types |
This enum represents the type of sheets to be copied
|
MWDefineRegionsBuilder.OrCreateEmptyRegionData |
This class holds the data returned from
MWDefineRegionsBuilder.getOrCreateEmptyRegion() |
MWDefineRegionsBuilder.TranslucencyOptionType |
This enum represents the translucency is to be performed on the selected or non-selected region faces
|
MWDefineSheetsBuilder.DefineStepType |
The define steps for defining Cavity and Core using the Split Body method.
|
MWDefineSheetsBuilder.Types |
The types for defining Cavity and Core.
|
MWDesignGuideLinesBuilder.CreateGuideLineData |
This class holds the data returned from
MWDesignGuideLinesBuilder.createGuideLine(nxopen.Curve, nxopen.Point3d, double) |
MWDesignGuideLinesBuilder.DirectionType |
The type of direction for the guide line to be created.
|
MWDesignPartingSurfaceBuilder.ObjectType |
The type of parting objects to be edited or placed.
|
MWDesignPartingSurfaceBuilder.PartingSurfaceType |
The type of parting surface to be created.
|
MWDesignPartingSurfaceBuilder.TransitionSurfaceType |
The type of transition surface to be created.
|
MWDesignPartingSurfaceBuilder.TrimAndExtendFromRegionType |
The region type from which to trim and extend when creating parting surface.
|
MWMoldedPartValidationBuilder.AssignToRegion |
Options for assigning faces to the Cavity or Core region
|
MWMoldedPartValidationBuilder.CalculateOption |
Calculation options
|
MWMoldedPartValidationBuilder.CheckScope |
Check scope for information
|
MWMoldedPartValidationBuilder.RangeType |
Range type for displaying small corner radius faces
|
MWPartingManagerBuilder.DataStatus |
The status of the parting manager data.
|
MWPartingManagerBuilder.RegisterType |
The type of registering UNDO identifier.
|
ObjectAttributeManagementBuilder.FilterAccordingToAttributeType |
the selection filter type according to attribute
|
ObjectAttributeManagementBuilder.FilterType |
the selection filter type
|
ObjectAttributeManagementBuilder.ShowComponentsType |
the show type according to attribute
|
ObjectAttributeManagementBuilder.ShowType |
show attributes of selected objects or show objects according to attribute
|
PiercingInsertBuilder.AssociationToolType |
Specifies the association tool operation option.
|
PiercingInsertBuilder.DieInsertTypeItems |
Specifies the type of insert.
|
PiercingInsertBuilder.InsertPosition |
Specifies the position of piercing inserts, for EDW only
|
PiercingInsertBuilder.NormalBbpslugType |
Specifies the type of bottom plate slug.
|
PiercingInsertBuilder.NormalCavityType |
Specifies the type of cavity.
|
PiercingInsertBuilder.NormalClearanceOptionType |
Specifies the design option of piercing insert.
|
PiercingInsertBuilder.NormalDsslugType |
Specifies the type of die shoe slug.
|
PiercingInsertBuilder.NormalOffsetSideType |
Specifies the offset side of normal pierce insert design.
|
PiercingInsertBuilder.NormalUdpparentPartType |
Specifies the parent part of user defined punch.
|
PiercingInsertBuilder.PunchPocketTypeItemsBP |
Specifies the punch pocket type in backing plate.
|
PiercingInsertBuilder.PunchPocketTypeItemsPP |
Specifies the punch pocket type in punch plate.
|
PiercingInsertBuilder.PunchPocketTypeItemsSP |
Specifies the punch pocket type in stripper plate.
|
PiercingInsertBuilder.Types |
Specifies the option of piercing insert type.
|
PiercingInsertMiniToolsBuilder.AssociationToolItems |
Specifies the association tool operation option.
|
PocketBuilder.ModeType |
Represents the pocket operation method
|
PocketBuilder.RsetType |
Represents the pocket refset types
|
PocketBuilder.ToolType |
Represents the select type of tool
|
PrebendBuilder.NumberBendsOption |
The option of bend number to divide into
|
PunchInsertBuilder.InsertPositionItems |
Specifies the position of piercing inserts, for EDW only
|
PunchInsertBuilder.NormalClearanceOptionTypeItems |
Specifies the design option of piercing insert.
|
PunchInsertBuilder.NormalOffsetSideTypeItems |
Specifies the offset side of normal pierce insert design.
|
PunchInsertBuilder.PunchPocketTypeItemsBackingPlate |
Specifies the punch pocket type in backing plate.
|
PunchInsertBuilder.PunchPocketTypeItemsPunchPlate |
Specifies the punch pocket type in punch plate.
|
PunchInsertBuilder.PunchPocketTypeItemsStripperPlate |
Specifies the punch pocket type in stripper plate.
|
QuickDatumCsysBuilder.AlignVectors |
Represents an index to components list type.
|
QuickQuotationBuilder.DesignTypes |
Specify the design type.
|
QuickQuotationBuilder.InsertGroupMaterials |
Specify the insert group material.
|
QuickQuotationBuilder.ManageTemporaryObjectsTypes |
Specify the management type for the temporary objects.
|
QuickQuotationBuilder.ObjectTypes |
Specify the concept sheet body type.
|
QuickQuotationBuilder.Types |
Specify the operation type.
|
ReliefDesignBuilder.Method |
The relief design creation method.
|
ReliefDesignBuilder.MethodOfDelete |
The relief design delete method.
|
ReliefDesignBuilder.Types |
The relief design type.
|
RemoveHolesBuilder.SelectionTypes |
select object types, body or face
|
RenameAndExportComponentBuilder.DefinitionType |
definition type
|
RenameAndExportComponentBuilder.LoadOptionType |
load option type
|
RenameAndExportComponentBuilder.NameRuleType |
tooling naming rule
|
RenameAndExportComponentBuilder.NamingRuleType |
naming rule
|
RenameAndExportComponentBuilder.Types |
types
|
ReusableObjectPasteBuilder.PasteMethods |
Specifies the design option
|
ReusablePocketBuilder.Hole |
Represents hole types.
|
ReusePositioningObjectBuilder.CurveExtendToFace |
extend to face edges type enum.
|
ReusePositioningObjectBuilder.CurveTrim |
trim to each other within section type enum.
|
ReusePositioningObjectBuilder.DialogOptions |
the dialog layout options
|
ReusePositioningObjectBuilder.NonStandardPointsData |
This class holds the data returned from
ReusePositioningObjectBuilder.getNonStandardPoints() |
ReusePositioningObjectBuilder.SubTypes |
the positioning sub types
|
ReusePositioningObjectBuilder.Types |
the positioning types
|
RunnerBuilder.GuideEndType |
Represents the runner guide end type.
|
RunnerBuilder.SectionType |
Represents the section type of runner channel.
|
RunSimulationBuilder.CollisionCheckOptions |
Specifies the collision check method
|
ScrapDesignBuilder.AddonType |
Specifies the add-on type
|
ScrapDesignBuilder.Body |
Specifies the operation type of scraps
|
ScrapDesignBuilder.DefScrapType |
Specifies the definition type of scraps
|
ScrapDesignBuilder.EditScrapType |
Specifies the edit type of scraps
|
ScrapDesignBuilder.OvercutType |
Specifies the over cut type, different type has different parameters
|
ScrapDesignBuilder.RemoveType |
Specifies the removing type as filter
|
ScrapDesignBuilder.ScrapDefPosition |
Specifies the position method of scraps, projecting method is normally used
|
ScrapDesignBuilder.ScrapDefType |
Specifies the creation type of scraps
|
ScrapDesignBuilder.TrimNumType |
Specifies the step of trimming process, the maximum is five
|
ShimBuilder.ParentOption |
Specify the parent node.
|
ShimBuilder.SideAttributeValues |
Specifies the value of side attribute.
|
ShimBuilder.Types |
Specify the shim operation type.
|
SIZERExportBuilder.MCDMechanicalData |
Defines the mechanical data in MCD mode.
|
SIZERExportBuilder.MechanicalData |
Defines the mechanical data in Motion mode.
|
SIZERExportBuilder.RunMode |
Represents the run mode.
|
SIZERImportBuilder.PositionMode |
Represents the position mode.
|
SlugRetentionBuilder.Types |
the main type
|
SmartScrewUpdateBuilder.ParentOption |
Specify the parent node.
|
SmartScrewUpdateBuilder.Types |
Specify the operation type.
|
SolidPatchBuilder.SolidPatchType |
Settings of the solid patch creation types.
|
SpecialFormingBuilder.BlockType |
the block type
|
SpecialFormingBuilder.ParentValue |
Specifies the main page type.
|
SpecialFormingBuilder.PunchOrDie |
Specifies the main page type.
|
SpecialFormingBuilder.Types |
Specifies the main page type.
|
SpecialPiercingInsertBuilder.BoundBoxType |
Specifies the bounded box type block or cylinder.
|
SpecialPiercingInsertBuilder.InsertPositionTypes |
Specifies the position of piercing inserts, for EDW only
|
SpecialPiercingInsertBuilder.NormalBottomBackingPlateSlugType |
Specifies the type of bottom plate slug.
|
SpecialPiercingInsertBuilder.NormalCavityType |
Specifies the type of cavity.
|
SpecialPiercingInsertBuilder.NormalDieShoeSlugType |
Specifies the type of die shoe slug.
|
SpecialPiercingInsertBuilder.NormalOffsetSideType |
Specifies the offset side of normal pierce insert design.
|
SpecialPiercingInsertBuilder.ParentPartTypes |
Specifies the parent part type.
|
SpecialPiercingInsertBuilder.PunchOrDieTypes |
Specifies the parent part type.
|
SpecialPiercingInsertBuilder.StandardOrUserDefinedTypes |
Specifies the parent part type.
|
SpecialPiercingInsertBuilder.Types |
Specifies the parent part type.
|
SpecifyBaffleBuilder.AttributeTypes |
Types to specify how to assign attributes to the selected body.
|
SpecifyBaffleBuilder.ChannelColorData |
This class holds the data returned from
SpecifyBaffleBuilder.getChannelColor() |
SplitSolidBuilder.OperationType |
the split operation type: split, trim.
|
SplitSolidBuilder.ToolObjectOption |
the split tool selection type: Existing Object, New Plane.
|
SpreadsheetData.DefinedAttributesExpressionsData |
This class holds the data returned from
SpreadsheetData.getDefinedAttributesExpressions(nxopen.tooling.SpreadsheetData.KeywordType) |
SpreadsheetData.KeywordType |
Represents the different attribute or expression section in spreadsheet
|
SpreadsheetData.ParameterStatus |
Represents the different spreadsheet parameter status
|
SpreadsheetDataParameter.Status |
Represents the different spreadsheet parameter status
|
StandardPartBuilder.EditType |
Represents the type to edit a standard part.
|
StandardPartBuilder.RefsetName |
Represents the reference set of the standard part when it is added to the assembly.
|
StockSizeBuilder.CalculateBoxSizeData |
This class holds the data returned from
StockSizeBuilder.calculateBoxSize() |
StockSizeBuilder.Cylinder |
Represents the base circle type of cylinder.
|
StockSizeBuilder.RefCsysType |
Represents the reference CSYS type.
|
StockSizeBuilder.Shape |
Represents the shape of stock size.
|
StockSizeBuilder.Types |
Represents the shape of stock size.
|
StripLayoutBuilder.FromStationType |
Specifies the option of From Station for layout
|
StripLayoutBuilder.ToStationType |
Specifies the option of To Station for layout
|
StripLayoutStationInformationBuilder.StationItem |
Specifies the station items
|
SubInsertBuilder.Shape |
Represents the foot shape
|
SubInsertBuilder.Types |
Represents the type of parent part
|
ToolingApplication |
Wizard type, some of them should be same as in mpdwshare_uf_mold.h
|
ToolingCloneaction |
Clone action type
|
ToolingClonemethod |
Clone method
|
ToolingCloneparttype |
Part file type, .sim, .fem etc.
|
TraverseLoopBuilder.CheckGapData |
This class holds the data returned from
TraverseLoopBuilder.checkGap(nxopen.NXObject[]) |
TrimMoldComponentsBuilder.TargetScope |
the target bodies selection scope
|
TrimMoldComponentsBuilder.TrimMethod |
the processing type of Trim Mold Components.
|
TrimMoldComponentsBuilder.TrimPartName |
the trim part options where a part chosen to work around
|
TrimMoldComponentsBuilder.TrimSurfaceName |
trim surface types
|
TrimRegionBuilder.BoundaryOption |
represents the boundary type option, body/curve type or traverse type.
|
TrimRegionBuilder.ColorValueData |
This class holds the data returned from
TrimRegionBuilder.getColorValue() |
TrimRegionBuilder.RegionOption |
represents the option to keep or discard the selected region.
|
TrimSolidBuilder.TrimSolidAction |
represents the action to create trim solid.
|
TrimSolidBuilder.Types |
represents the option to select face or sheet body or manufacturing faces to trim the bounding box.
|
UndersizeBuilder.Orbit |
Represents the orbit type
|
UniversalUnformBuilder.BendTypes |
The types of bend
|
UnusedFileManagementBuilder.FileDirectory |
the unused file location.
|
UserDefinedMotionBuilder.LinearCurveTypes |
Specifies the motion curve types when motion type is Linear
|
UserDefinedMotionBuilder.MotionTypes |
Specifies the motion types
|
UserDefinedMotionBuilder.RotaryCurveTypes |
Specifies the motion curve types when motion type is Rotary
|
ValidCheckBuilder.AnalysisMode |
the analysis mode, including solid-based mode and facet-based mode
|
ValidCheckBuilder.CheckingType |
the checking type, including true body, false body or both
|
ValidCheckBuilder.SelMode |
the selection type, including component and solid body
|
WallThicknessCheckerBuilder.CalculateMethod |
The calculation method used for the wall thickness analysis.
|
WallThicknessCheckerBuilder.LegendControl |
The legend control used in displaying the thickness results.
|
WallThicknessCheckerBuilder.RangeType |
The range type for defining the ranges used in displaying the thickness results.
|
WireHoleBuilder.Types |
the plane to create wire hole sketch
|
WorkpieceBuilder.MethodType |
the unit type includes the work piece define method
|
WorkpieceBuilder.Types |
the unit type includes product and combined work piece type
|
WorkpieceBuilder.WorkPieceType |
the unit type includes the work piece create method
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.