Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static DefineLifterBuilder.Types |
DefineLifterBuilder.Types.GENERIC_LIFTER
Generic lifter type
|
static DefineLifterBuilder.Types |
DefineLifterBuilder.Types.LIFTERON_LIFTER
Lifter on lifter type
|
Modifier and Type | Method and Description |
---|---|
DefineLifterBuilder.Types |
DefineLifterBuilder.type()
Returns the type
License requirements: None. |
static DefineLifterBuilder.Types |
DefineLifterBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DefineLifterBuilder.Types |
DefineLifterBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DefineLifterBuilder.Types[] |
DefineLifterBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DefineLifterBuilder.setType(DefineLifterBuilder.Types type)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.