Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static DieInsertBuilder.BoundingBoxTypeItems |
DieInsertBuilder.BoundingBoxTypeItems.BLOCK
The bounding box type is Block
|
static DieInsertBuilder.BoundingBoxTypeItems |
DieInsertBuilder.BoundingBoxTypeItems.CYLINDER
The bounding box type is Cylinder
|
Modifier and Type | Method and Description |
---|---|
DieInsertBuilder.BoundingBoxTypeItems |
DieInsertBuilder.boundingBoxType()
Returns the bounding box type
License requirements: None. |
static DieInsertBuilder.BoundingBoxTypeItems |
DieInsertBuilder.BoundingBoxTypeItems.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DieInsertBuilder.BoundingBoxTypeItems |
DieInsertBuilder.BoundingBoxTypeItems.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DieInsertBuilder.BoundingBoxTypeItems[] |
DieInsertBuilder.BoundingBoxTypeItems.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DieInsertBuilder.setBoundingBoxType(DieInsertBuilder.BoundingBoxTypeItems boundingBoxType)
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.