Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static HoleReportBuilder.EnumSelectionType |
HoleReportBuilder.EnumSelectionType.VIEW_SELECTION
Selects view to create hole table
|
static HoleReportBuilder.EnumSelectionType |
HoleReportBuilder.EnumSelectionType.WINDOW_SELECTION
Selects holes in window to create hole table
|
Modifier and Type | Method and Description |
---|---|
HoleReportBuilder.EnumSelectionType |
HoleReportBuilder.selectionType()
Returns the selection type to choose select view or holes in window to create hole report
License requirements: None. |
static HoleReportBuilder.EnumSelectionType |
HoleReportBuilder.EnumSelectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HoleReportBuilder.EnumSelectionType |
HoleReportBuilder.EnumSelectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HoleReportBuilder.EnumSelectionType[] |
HoleReportBuilder.EnumSelectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HoleReportBuilder.setSelectionType(HoleReportBuilder.EnumSelectionType selectionType)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.