Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static InsertAuxiliaryBuilder.UseFaceOrSketchToRevolve |
InsertAuxiliaryBuilder.UseFaceOrSketchToRevolve.FACE |
static InsertAuxiliaryBuilder.UseFaceOrSketchToRevolve |
InsertAuxiliaryBuilder.UseFaceOrSketchToRevolve.SKETCH |
Modifier and Type | Method and Description |
---|---|
InsertAuxiliaryBuilder.UseFaceOrSketchToRevolve |
InsertAuxiliaryBuilder.useFaceOrSketch()
Returns the use face or sketch option
License requirements: None. |
static InsertAuxiliaryBuilder.UseFaceOrSketchToRevolve |
InsertAuxiliaryBuilder.UseFaceOrSketchToRevolve.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InsertAuxiliaryBuilder.UseFaceOrSketchToRevolve |
InsertAuxiliaryBuilder.UseFaceOrSketchToRevolve.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InsertAuxiliaryBuilder.UseFaceOrSketchToRevolve[] |
InsertAuxiliaryBuilder.UseFaceOrSketchToRevolve.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
InsertAuxiliaryBuilder.setUseFaceOrSketch(InsertAuxiliaryBuilder.UseFaceOrSketchToRevolve useFaceOrSketch)
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.